This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[DM8168] About OMXIL VFCC component

Other Parts Discussed in Thread: TVP7002

Hi All

Recently, I'm concerned about with how can i capture the multiplexed video stream (line multiplexed 1080p60fps, 16bit) with VIP0, VIP1.

Firstly, I considered the V4L2 capture. 

But, It looks like support only VIP0 according to TI81XX_Video_Capture_Driver_User_Guide document.

It meas that i can not use VIP1 port to capture 1080p30fps (line multiplexed video stream, 16bit) 

Actually, I'd like to capture the 1080p30fps  2 stream with VIP0 and VIP1  respectively. 

------------------------- page 6 -----------------------------------------

Features
V4L2 capture driver supports following features.
• Supports VIP0 instance of the VPSS.
• Supports TVP7002 standard Linux sub device driver.
• Supports YUV422 interleaved, YUV422 semiplanar, YUV420 semiplanar and RGB888 color formats to memory.
• Supports scaling and cropping for YUV formats (downscaling only)
• Supports 1080P60, 1080P30, 1080I60 and 720P60 input resolutions.
• Supports user pointer buffer mechanism of the V4L2 driver interface.

--------------------------------------------------------------------------------------

Therefore, I'm considering using OMXIL VFCC component to capture it.

Unfortunately, I also find out these sentence from OMX_05_02_00_48_UserGuide.pdf document as below.

I think ... it means that VFCC can not capture the line multiplexed 1080p60fps (16bit) video stream.

Please, Are there anyone who advise me about capturing line multiplexed 1080p60fps (1080p30fps + 1080p30fps) 16bit with OMXIL VFCC ?

Is it possible with VFCC ?

-------------------------- page 23 ----------------------------------

Features supported
· Input Video Source Formats
§ YUV422 8-bit embedded sync mode
§ YUV422 16-bit embedded sync mode
§ YUV422 8-bit 2x/4x pixel multiplxed mode
§ YUV422 8-bit 4x line multiplexed mode


· Output Video formats
§ YUV422 YUYV interleaved format
§ YUV420 Semi-planer format
· In-line video processing features
§ Chroma-down sampling


· Other features
§ multi-port capture on VIP0 & VIP1 (Port A, Port B), with ability to configure.
§ Interlaced as well as progressive capture
§ Non-multiplexed capture upto 1080P60 (1920x1080) resolution

 Multichannel upto 16CH D1 (NTSC/PAL) using 4 VIP ports (VIP0/A, VIP0/B,
VIP1/A, VIP1/B)
§ Per frame info to user like - field ID, captured frame width x height,
timestamp, logical channel ID
§ For YUV input, optional chroma downsampling is supported

----------------------------------------------------------------

Many thanks,

Jiwon