This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM3715/Android 2.3.4 display problem

Other Parts Discussed in Thread: DM3730, ADS7846

Hello everyone!

when I build TI- Android- GingerBread- 2. 3. 4- DevKit- 2. 1

make TARGET_PRODUCT=omap3evm OMAPES=5.x 

I  get a result as the following images shown :

and  this post

http://e2e.ti.com/support/embedded/android/f/509/t/130753.aspx

don't solve my problem ,could anyone tell me what have happened ?thanks 

zsz

  • the debug and logcat info as following :

    Texas Instruments X-Loader 1.51(zsz_UPDATE @ 2012.11.09) (Mar 27 2013 - 14:50:33)
    zsz_UPDATE: mem_type=15
    zsz_UPDATE: GPMC_NAND
    zsz_UPDATE: mem_type=15
    zsz_UPDATE: GPMC_NAND
    zsz_UPDATE: mem_type=15
    zsz_UPDATE: GPMC_NAND
    (zsz_NOTE)Beagle Rev Ax/Bx
    Starting X-loader on MMC
    Reading boot sector

    234532 Bytes Read from MMC
    Starting OS Bootloader from MMC...
    zsz_UPDATE: buf=80041424,CFG_LOADDER=80008000
    zkk dbg,Starting OS Bootloader...
    zkk dbg,buf=80041424,CFG_LOADDER=80008000


    U-Boot 2010.06-rc1 (Apr 15 2013 - 10:32:23)
    (zsz_UPDATE @ 2012.11.09)

    U-Boot code: 80E80000 -> 80EB9424 BSS: -> 80EF89E4

    OMAP34xx/35xx-GP ES2.1, CPU-OPP2 L3-165MHz
    OMAP3 Devkit8500 board + LPDDR/NAND(zsz_NOTE @ 2012.11.09)
    I2C: ready
    --------size of CS0 = 0x08000000
    @--------size of CS1 = 0x08000000
    --------offset of CS1 = 0x08000000
    DRAM: 256 MiB
    NAND: 512 MiB
    *** Warning - bad CRC or NAND, using default environment

    In: serial
    Out: serial
    Err: serial
    arch/arm/lib/board.c=>start_armboot->misc_init_r
    borad/timll/devkit8500/devkit8500.c=>misc_init_r
    zsz_UPDATE: Devkit8500 xM Rev A
    Die ID #22e200029e380000014e51c70101d01e
    zsz_UPDATE: setup_net_chip->CONFIG_DRIVER_DM9000
    LcdSPIInit_240X320_35 begin

    LcdSPIInit_240X320_35 end


    dump regs
    LCD_WIDTH is 140
    LCD_HEIGHT is f0
    DISPC_SIZE_LCD is ef013f
    DISPC_GFX_SIZE is ef013f
    DISPC_GFX_ATTRIBUTES is 113
    DISPC_CONFIG is 208
    DISPC_DIVISOR is 20005

    dump regs end
    CM_CLKSEL_DSS is 8c80c00
    CM_CLLEN_PLL is 10770077
    Net: dm9000
    Hit any key to stop autoboot: 3 2 1 0
    mmc1 is available

    zsz_UPDATE @ do_fat_fsload

    reading boot.scr

    716 bytes read
    Running bootscript from mmc ...
    ## Executing script at 80300000
    ***** RootFS: /dev/mmcblk0p2 *****
    ***** setevn bootargs console=ttyS2,115200n8 androidboot.console=ttyS2 mem=128M root=/dev/mmcblk0p2 rw rootfstype=ext3 rootdelay=1 init=/init ip=off mpurate=1000 omapfb.rotate=3 omapfb.rotate_type=1 vram=8M omapfb.vram=0:8M
    ***** mmc init
    mmc1 is available
    ***** fatload mmc 0 0x80300000 uImage

    zsz_UPDATE @ do_fat_fsload

    reading uImage

    2525732 bytes read
    ***** bootm 0x80300000
    ## Booting kernel from Legacy Image at 80300000 ...
    Image Name: Linux-2.6.32
    Image Type: ARM Linux Kernel Image (uncompressed)
    Data Size: 2525668 Bytes = 2.4 MiB
    Load Address: 80008000
    Entry Point: 80008000
    Verifying Checksum ... OK
    Loading Kernel Image ... OK
    OK

    Starting kernel ...

    zkk dbg, before thekernel
    Uncompressing Linux.............................................................................................................................................................
    (zsz_NOTE)
    done, booting the kernel.
    (zsz_NOTE: Linux kernel begin)
    Linux version 2.6.32 (root@zhusz) (gcc version 4.4.3 (GCC) ) #20 Thu Apr 25 18:55:21 CST 2013
    CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c53c7f
    CPU: VIPT nonaliasing data cache, VIPT nonaliasing instruction cache
    Machine: OMAP3 DEVKIT8500/SED_MT2 Board
    Memory policy: ECC disabled, Data cache writeback
    OMAP3630/DM3730 ES1.0 (l2cache iva sgx neon isp 192mhz_clk )
    SRAM: Mapped pa 0x40200000 to va 0xfe400000 size: 0x100000
    Reserving 8388608 bytes SDRAM for VRAM
    Built 1 zonelists in Zone order, mobility grouping on. Total pages: 32512
    Kernel command line: console=ttyS2,115200n8 androidboot.console=ttyS2 mem=128M root=/dev/mmcblk0p2 rw rootfstype=ext3 rootdelay=1 init=/init ip=off mpurate=1000 omapfb.rotate=3 omapfb.rotate_type=1 vram=8M omapfb.vram=0:8M
    PID hash table entries: 512 (order: -1, 2048 bytes)
    Dentry cache hash table entries: 16384 (order: 4, 65536 bytes)
    Inode-cache hash table entries: 8192 (order: 3, 32768 bytes)
    Memory: 128MB = 128MB total
    Memory: 116080KB available (4360K code, 829K data, 160K init, 0K highmem)
    Hierarchical RCU implementation.
    NR_IRQS:402
    Clocking rate (Crystal/Core/MPU): 26.0/200/600 MHz
    Reprogramming SDRC clock to 200000000 Hz
    dpll3_m2_clk rate change failed: -22
    GPMC revision 5.0
    IRQ: Found an INTC at 0xfa200000 (revision 4.0) with 96 interrupts
    Total of 96 interrupts on 1 active controller
    OMAP GPIO hardware version 2.5
    ------------ads7846_dev_init: OMAP3_DEVKIT8500_TS_GPIO = 27
    OMAP clockevent source: GPTIMER12 at 32768 Hz
    Console: colour dummy device 80x30
    Calibrating delay loop... 476.81 BogoMIPS (lpj=1859584)
    Mount-cache hash table entries: 512
    CPU: Testing write buffer coherency: ok
    regulator: core version 0.5
    NET: Registered protocol family 16

    ********* omap3_devkit8500_init *********
    Found NAND on CS0
    Registering NAND on CS0
    Target VDD1 OPP = 4, VDD2 OPP = 2
    OMAP DMA hardware revision 5.0
    bio: create slab <bio-0> at 0
    SCSI subsystem initialized
    usbcore: registered new interface driver usbfs
    usbcore: registered new interface driver hub
    usbcore: registered new device driver usb
    i2c_omap i2c_omap.1: bus 1 rev4.0 at 2600 kHz
    twl4030: PIH (irq 7) chaining IRQs 368..375
    twl4030: power (irq 373) chaining IRQs 376..383
    twl4030: gpio (irq 368) chaining IRQs 384..401
    regulator: VUSB1V5: 1500 mV normal standby
    regulator: VUSB1V8: 1800 mV normal standby
    regulator: VUSB3V1: 3100 mV normal standby
    twl4030_usb twl4030_usb: Initialized TWL4030 USB module
    regulator: VMMC1: 1850 <--> 3150 mV normal standby
    regulator: VDAC: 1800 mV normal standby
    regulator: VPLL2: 1800 mV normal standby
    regulator: VMMC2: 1850 <--> 3150 mV normal standby
    regulator: VSIM: 1800 <--> 3000 mV normal standby
    i2c_omap i2c_omap.2: bus 2 rev4.0 at 400 kHz
    i2c_omap i2c_omap.3: bus 3 rev4.0 at 100 kHz
    Switching to clocksource 32k_counter
    musb_hdrc: version 6.0, musb-dma, otg (peripheral+host), debug=0
    musb_hdrc: USB OTG mode controller at fa0ab000 using DMA, IRQ 92
    NET: Registered protocol family 2
    IP route cache hash table entries: 1024 (order: 0, 4096 bytes)
    TCP established hash table entries: 4096 (order: 3, 32768 bytes)
    TCP bind hash table entries: 4096 (order: 2, 16384 bytes)
    TCP: Hash tables configured (established 4096 bind 4096)
    TCP reno registered
    UDP hash table entries: 256 (order: 0, 4096 bytes)
    UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
    NET: Registered protocol family 1
    RPC: Registered udp transport module.
    RPC: Registered tcp transport module.
    RPC: Registered tcp NFSv4.1 backchannel transport module.
    omap-iommu omap-iommu.0: isp registered
    NetWinder Floating Point Emulator V0.97 (double precision)
    ashmem: initialized
    VFS: Disk quotas dquot_6.5.2
    Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
    msgmni has been set to 227
    alg: No test for stdrng (krng)
    io scheduler noop registered
    io scheduler deadline registered
    io scheduler cfq registered (default)
    OMAP DSS rev 2.0
    OMAP DISPC rev 3.0
    OMAP VENC rev 2
    **************** devkit8500_panel_drv_init
    LcdSPIInit_240X320_35 begin

    LcdSPIInit_240X320_35 end

    **************** devkit8500_panel_probe
    Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled
    serial8250.0: ttyS0 at MMIO 0x4806a000 (irq = 72) is a ST16654
    serial8250.1: ttyS1 at MMIO 0x4806c000 (irq = 73) is a ST16654
    serial8250.2: ttyS2 at MMIO 0x49020000 (irq = 74) is a ST16654
    console [ttyS2] enabled
    brd: module loaded
    loop: module loaded
    omap2-nand driver initializing
    NAND device: Manufacturer ID: 0xad, Chip ID: 0xbc (Hynix NAND 512MiB 1,8V 16-bit)
    cmdlinepart partition parsing not available
    Creating 5 MTD partitions on "omap2-nand":
    0x000000000000-0x000000080000 : "X-Loader"
    0x000000080000-0x000000260000 : "U-Boot"
    0x000000260000-0x000000280000 : "U-Boot Env"
    0x000000280000-0x000000a80000 : "Kernel"
    0x000000a80000-0x000020000000 : "File System"
    PPP generic driver version 2.4.2
    PPP Deflate Compression module registered
    PPP BSD Compression module registered
    PPP MPPE Compression module registered
    NET: Registered protocol family 24
    PPPoL2TP kernel driver, V1.0
    dm9000 Ethernet Driver, V1.31
    usbcore: registered new interface driver asix
    usbcore: registered new interface driver cdc_ether
    usbcore: registered new interface driver cdc_eem
    usbcore: registered new interface driver dm9601
    usbcore: registered new interface driver smsc95xx
    usbcore: registered new interface driver gl620a
    usbcore: registered new interface driver net1080
    usbcore: registered new interface driver plusb
    usbcore: registered new interface driver rndis_host
    usbcore: registered new interface driver cdc_subset
    usbcore: registered new interface driver zaurus
    usbcore: registered new interface driver MOSCHIP usb-ethernet driver
    ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
    ehci-omap ehci-omap.0: OMAP-EHCI Host Controller
    ehci-omap ehci-omap.0: new USB bus registered, assigned bus number 1
    ehci-omap ehci-omap.0: irq 77, io mem 0x48064800
    ehci-omap ehci-omap.0: USB 2.0 started, EHCI 1.00
    hub 1-0:1.0: USB hub found
    hub 1-0:1.0: 3 ports detected
    Initializing USB Mass Storage driver...
    usbcore: registered new interface driver usb-storage
    USB Mass Storage support registered.
    android init
    android_probe pdata: c04a36bc
    android_bind
    android_usb gadget: android_usb ready
    musb_hdrc musb_hdrc: MUSB HDRC host driver
    musb_hdrc musb_hdrc: new USB bus registered, assigned bus number 2
    hub 2-0:1.0: USB hub found
    hub 2-0:1.0: 1 port detected
    f_adb init
    android_register_function adb
    f_mass_storage init
    android_register_function usb_mass_storage
    adb_bind_config
    mass_storage_bind_config
    android_usb gadget: Number of LUNs=1
    mice: PS/2 mouse device common for all mice
    gpio-keys gpio-keys: failed to request GPIO 29, error -16
    gpio-keys: probe of gpio-keys failed with error -16
    input: TWL4030 Keypad as /devices/platform/i2c_omap.1/i2c-1/1-004a/twl4030_keypad/input/input0
    ----------------------ads7846_probe
    ts->phys = spi2.0/input0
    ts->name = ADS7846 Touchscreen
    ts->model = 7846
    pdata->x_max = 4095
    pdata->y_max = 4095
    ads7846 spi2.0: touchscreen, irq 187
    ads7846 spi2.0: ads7846_read12_ser return 422
    input: ADS7846 Touchscreen as /devices/platform/omap2_mcspi.2/spi2.0/input/input1
    using rtc device, twl_rtc, for alarms
    twl_rtc twl_rtc: rtc core: registered twl_rtc as rtc0
    i2c /dev entries driver
    Linux video capture interface: v2.00
    omap-iommu omap-iommu.0: isp: version 1.1
    usbcore: registered new interface driver uvcvideo
    USB Video Class driver (v0.1.0)
    OMAP Watchdog Timer Rev 0x31: initial timeout 60 sec
    Registered led device: sys_led
    Registered led device: user_ledb
    Registered led device: user_led1
    Registered led device: user_led2
    usbcore: registered new interface driver usbhid
    usbhid: USB HID core driver
    logger: created 64K log 'log_main'
    logger: created 256K log 'log_events'
    logger: created 64K log 'log_radio'
    logger: created 64K log 'log_system'
    Advanced Linux Sound Architecture Driver Version 1.0.21.
    No device for DAI omap-mcbsp-dai-0
    No device for DAI omap-mcbsp-dai-1
    No device for DAI omap-mcbsp-dai-2
    No device for DAI omap-mcbsp-dai-3
    No device for DAI omap-mcbsp-dai-4
    OMAP3 Devkit8500 SoC init
    asoc: twl4030 <-> omap-mcbsp-dai-0 mapping ok
    ALSA device list:
    #0: omap3devkit8500 (twl4030)
    TCP cubic registered
    NET: Registered protocol family 17
    NET: Registered protocol family 15
    Power Management for TI OMAP3.
    Unable to set L3 frequency (400000000)
    Switched to new clocking rate (Crystal/Core/MPU): 26.0/200/1000 MHz
    IVA2 clocking rate: 800 MHz
    SmartReflex driver initialized
    VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3
    ----------------------omapfb_probe
    ***********************register_framebuffer
    Console: switching to colour frame buffer device 30x40
    -------------------DISPC_CONTROL=18008
    ----------------------dispc_set_tft_data_lines: 1
    ----------------------dispc_set_tft_data_lines: 24
    _dispc_set_pol_freq: onoff 0 rf 0 ieo 0 ipc 0 ihs 1 ivs 1 acbi 0 acb 0
    lck_div = 2, pck_div = 3
    **************** devkit8500_panel_enable: x_res = 320, y_res = 240

    ********* omap3_devkit8500_enable_lcd *********

    ********* TWL4030_MODULE_LED: 11
    regulator_init_complete: incomplete constraints, leaving VDVI on
    regulator_init_complete: incomplete constraints, leaving VDAC on
    twl_rtc twl_rtc: setting system clock to 2000-01-01 00:39:00 UTC (946687140)
    omapdss DPI error: display already enabled
    omap_vout omap_vout: 'lcd' Display already enabled
    omapdss DPI error: display already enabled
    omap_vout omap_vout: 'lcd' Display already enabled
    omap_vout omap_vout: Buffer Size = 3686400
    omap_vout omap_vout: : registered and initialized video device 0
    omap_vout omap_vout: Buffer Size = 3686400
    omap_vout omap_vout: : registered and initialized video device 1
    Waiting 1sec before mounting root device...
    mmc0: host does not support reading read-only switch. assuming write-enable.
    mmc0: new high speed SD card at address e624
    mmcblk0: mmc0:e624 SU02G 1.84 GiB
    mmcblk0: p1 p2 p3
    kjournald starting. Commit interval 5 seconds
    EXT3-fs (mmcblk0p2): using internal journal
    EXT3-fs (mmcblk0p2): recovery complete
    EXT3-fs (mmcblk0p2): mounted filesystem with writeback data mode
    VFS: Mounted root (ext3 filesystem) on device 179:2.
    Freeing init memory: 160K
    Warning: unable to open an initial console.
    init: cannot find '/system/bin/wifi/rc.wifi', disabling 'wl12xx'
    init: cannot find '/system/etc/install-recovery.sh', disabling 'flash_recovery'
    # enabling adb
    adb_open
    omaplfb: Device 0: Framebuffer physical address: 0x8066a000
    omaplfb: Device 0: Framebuffer virtual address: 0xc9000000
    omaplfb: Device 0: Framebuffer size: 8388608
    omaplfb: Device 0: Framebuffer virtual width: 240
    omaplfb: Device 0: Framebuffer virtual height: 640
    omaplfb: Device 0: Framebuffer width: 240
    omaplfb: Device 0: Framebuffer height: 320
    omaplfb: Device 0: Framebuffer stride: 960
    omaplfb: Device 0: LCM of stride and page size: 61440
    omaplfb: bits_per_pixel = 32
    omaplfb: red.length = 8
    omaplfb: green.length = 8
    omaplfb: blue.length = 8
    omaplfb: red.offset = 16
    omaplfb: green.offset = 8
    omaplfb: blue.offset = 0
    omaplfb: red.msb_right = 0
    omaplfb: psPVRFBInfo->ePixelFormat = 20
    omaplfb: Device 0: Maximum number of swap chain buffers: 27
    omaplfb: Device 0: PVR Device ID: 1
    warning: `zygote' uses 32-bit capabilities (legacy support in use)
    select 1094 (d.process.acore), adj 7, size 5767, to kill
    send sigkill to 1094 (d.process.acore), adj 7, size 5767
    select 1132 (com.android.mms), adj 8, size 4568, to kill
    select 1142 (d.process.media), adj 9, size 4541, to kill
    send sigkill to 1142 (d.process.media), adj 9, size 4541
    select 1132 (com.android.mms), adj 8, size 4517, to kill
    send sigkill to 1132 (com.android.mms), adj 8, size 4517
    select 1162 (droid.deskclock), adj 8, size 4360, to kill
    send sigkill to 1162 (droid.deskclock), adj 8, size 4360
    select 1196 (droid.bluetooth), adj 7, size 4552, to kill
    send sigkill to 1196 (droid.bluetooth), adj 7, size 4552
    select 1205 (m.android.email), adj 7, size 4904, to kill
    send sigkill to 1205 (m.android.email), adj 7, size 4904
    select 1224 (d.process.media), adj 8, size 4820, to kill
    select 1252 (m.android.music), adj 9, size 4269, to kill
    send sigkill to 1252 (m.android.music), adj 9, size 4269

    # logcat
    --------- beginning of /dev/log/main
    I/DEBUG ( 889): debuggerd: Apr 24 2013 21:02:07
    --------- beginning of /dev/log/system
    I/Vold ( 887): Vold 2.1 (the revenge) firing up
    D/Vold ( 887): usb_configuration switch is not enabled in the kernel
    I/Netd ( 888): Netd 1.0 starting
    D/Vold ( 887): Volume sdcard state changing -1 (Initializing) -> 0 (No-Media)
    D/Vold ( 887): Volume sdcard state changing 0 (No-Media) -> 2 (Pending)
    D/Vold ( 887): Volume sdcard state changing 2 (Pending) -> 1 (Idle-Unmounted)
    D/AndroidRuntime( 891):
    D/AndroidRuntime( 891): >>>>>> AndroidRuntime START com.android.internal.os.ZygoteInit <<<<<<
    D/AndroidRuntime( 891): CheckJNI is ON
    D/dalvikvm( 891): creating instr width table
    I/ ( 892): ServiceManager: 0xad50
    E/ALSALib ( 892): external/alsa-lib/src/control/control.c:909:(snd_ctl_open_noupdate) Invalid CTL AndroidPlayback
    W/AudioHardwareALSA( 892): Unable to attach mixer to device AndroidPlayback: No such file or directory
    E/ALSALib ( 892): external/alsa-lib/src/control/control.c:909:(snd_ctl_open_noupdate) Invalid CTL AndroidCapture
    W/AudioHardwareALSA( 892): Unable to attach mixer to device AndroidCapture: No such file or directory
    D/TIALSAModule( 892): TI ALSA module opened
    D/TIALSAModule( 892): Initializing devices for TI ALSA module
    I/CameraService( 892): CameraService started (pid=892)
    D/AudioHardwareALSA( 892): openOutputStream called for devices: 0x00000002
    D/TIALSAModule( 892): open called for devices 00000002 in mode 0...
    I/TIALSAModule( 892): Initialized ALSA PLAYBACK device default
    I/AudioFlinger( 892): AudioFlinger's thread 0x388d8 ready to run
    D/TIALSAModule( 892): route called for devices 00000002 in mode 0...
    E/AudioHardwareALSA( 892): CALLING STANDBY
    I/SamplingProfilerIntegration( 891): Profiler is disabled.
    I/Zygote ( 891): Preloading classes...
    D/dalvikvm( 891): GC_EXPLICIT freed 47K, 78% free 233K/1024K, external 0K/0K, paused 2ms
    D/dalvikvm( 891): GC_EXPLICIT freed 1K, 73% free 283K/1024K, external 0K/0K, paused 2ms
    D/dalvikvm( 891): GC_EXPLICIT freed 20K, 70% free 316K/1024K, external 0K/0K, paused 2ms
    I/bluetooth_ScoSocket.cpp( 891): Entry name = MY-CAR ScoTypes = 0x7f
    I/bluetooth_ScoSocket.cpp( 891): Entry name = Motorola HF850 ScoTypes = 0x7
    D/dalvikvm( 891): GC_EXPLICIT freed 17K, 66% free 354K/1024K, external 0K/0K, paused 2ms
    D/dalvikvm( 891): GC_EXPLICIT freed 26K, 63% free 382K/1024K, external 0K/0K, paused 3ms
    D/dalvikvm( 891): GC_EXPLICIT freed 21K, 57% free 441K/1024K, external 0K/0K, paused 2ms
    W/MediaProfiles( 891): could not find media config xml file
    D/dalvikvm( 891): GC_EXPLICIT freed 98K, 47% free 543K/1024K, external 0K/0K, paused 3ms
    D/dalvikvm( 891): GC_EXPLICIT freed 271K, 24% free 882K/1155K, external 0K/0K, paused 7ms
    D/dalvikvm( 891): GC_EXPLICIT freed 21K, 20% free 930K/1155K, external 0K/0K, paused 6ms
    D/RenderScript_jni( 891): RenderScript JNI library not found!
    D/dalvikvm( 891): GC_EXPLICIT freed 24K, 21% free 970K/1219K, external 0K/0K, paused 7ms
    D/dalvikvm( 891): GC_EXPLICIT freed 24K, 6% free 1276K/1347K, external 0K/0K, paused 9ms
    D/dalvikvm( 891): GC_EXPLICIT freed 24K, 4% free 1306K/1347K, external 0K/0K, paused 10ms
    D/dalvikvm( 891): GC_EXPLICIT freed 28K, 6% free 1331K/1411K, external 0K/0K, paused 10ms
    D/dalvikvm( 891): GC_EXPLICIT freed 14K, 3% free 1371K/1411K, external 0K/0K, paused 10ms
    W/Zygote ( 891): Class not found for preloading: android.widget.TextView$SelectionModifierCursorController$1
    D/dalvikvm( 891): GC_EXPLICIT freed 28K, 6% free 1397K/1475K, external 0K/0K, paused 10ms
    D/dalvikvm( 891): GC_EXPLICIT freed 31K, 3% free 1436K/1475K, external 0K/0K, paused 10ms
    D/dalvikvm( 891): GC_EXPLICIT freed 38K, 6% free 1453K/1539K, external 0K/0K, paused 11ms
    D/dalvikvm( 891): GC_EXPLICIT freed 41K, 5% free 1468K/1539K, external 0K/0K, paused 11ms
    D/dalvikvm( 891): GC_EXPLICIT freed 55K, 8% free 1481K/1603K, external 0K/0K, paused 11ms
    D/dalvikvm( 891): GC_FOR_MALLOC freed 2890K, 57% free 2232K/5123K, external 0K/0K, paused 33ms
    D/dalvikvm( 891): GC_EXPLICIT freed 2438K, 52% free 2485K/5123K, external 0K/0K, paused 29ms
    D/dalvikvm( 891): GC_EXPLICIT freed 128K, 51% free 2545K/5123K, external 0K/0K, paused 21ms
    D/dalvikvm( 891): GC_EXPLICIT freed 73K, 50% free 2571K/5123K, external 0K/0K, paused 22ms
    D/dalvikvm( 891): GC_EXPLICIT freed 36K, 50% free 2588K/5123K, external 0K/0K, paused 21ms
    D/dalvikvm( 891): GC_EXPLICIT freed 31K, 50% free 2611K/5123K, external 0K/0K, paused 21ms
    D/dalvikvm( 891): GC_EXPLICIT freed 38K, 49% free 2634K/5123K, external 0K/0K, paused 21ms
    I/Zygote ( 891): ...preloaded 1829 classes in 2914ms.
    D/dalvikvm( 891): GC_EXPLICIT freed 18K, 49% free 2631K/5123K, external 0K/0K, paused 22ms
    I/Zygote ( 891): Preloading resources...
    D/dalvikvm( 891): GC_EXTERNAL_ALLOC freed <1K, 49% free 2633K/5123K, external 0K/0K, paused 21ms
    D/dalvikvm( 891): GC_EXPLICIT freed 15K, 48% free 2672K/5123K, external 414K/521K, paused 32ms
    D/dalvikvm( 891): GC_EXTERNAL_ALLOC freed 7K, 48% free 2682K/5123K, external 516K/521K, paused 21ms
    I/Zygote ( 891): ...preloaded 51 resources in 542ms.
    I/Zygote ( 891): ...preloaded 15 resources in 14ms.
    D/dalvikvm( 891): GC_EXPLICIT freed 14K, 48% free 2706K/5123K, external 716K/1038K, paused 22ms
    D/dalvikvm( 891): GC_EXPLICIT freed 8K, 48% free 2698K/5123K, external 716K/1038K, paused 22ms
    D/dalvikvm( 891): GC_EXPLICIT freed 1K, 48% free 2697K/5123K, external 716K/1038K, paused 22ms
    I/dalvikvm( 891): System server process 968 has been created
    I/Zygote ( 891): Accepting command socket connections
    E/BatteryService( 968): Could not open /sys/class/power_supply
    I/sysproc ( 968): Entered system_init()
    I/sysproc ( 968): ServiceManager: 0x8d6e0
    I/SurfaceFlinger( 968): SurfaceFlinger is starting
    I/SurfaceFlinger( 968): SurfaceFlinger's main thread ready to run. Initializing graphics H/W...
    D/libEGL ( 968): loaded /system/lib/egl/libGLES_android.so
    D/libEGL ( 968): loaded /system/lib/egl/libEGL_POWERVR_SGX530_125.so
    D/libEGL ( 968): loaded /system/lib/egl/libGLESv1_CM_POWERVR_SGX530_125.so
    D/libEGL ( 968): loaded /system/lib/egl/libGLESv2_POWERVR_SGX530_125.so
    W/SurfaceFlinger( 968): ro.sf.lcd_density not defined, using 160 dpi by default.
    E/libEGL ( 968): eglSetSwapRectangleANDROID:1844 error 3008 (EGL_BAD_DISPLAY)
    I/SurfaceFlinger( 968): EGL informations:
    I/SurfaceFlinger( 968): # of configs : 36
    I/SurfaceFlinger( 968): vendor : Android
    I/SurfaceFlinger( 968): version : 1.4 Android META-EGL
    I/SurfaceFlinger( 968): extensions: EGL_KHR_image EGL_KHR_image_base EGL_KHR_image_pixmap EGL_ANDROID_image_native_buffer EGL_ANDROID_swap_rectangle
    I/SurfaceFlinger( 968): Client API: OpenGL ES
    I/SurfaceFlinger( 968): EGLSurface: 8-8-8-8, config=0x1
    I/SurfaceFlinger( 968): OpenGL informations:
    I/SurfaceFlinger( 968): vendor : Imagination Technologies
    I/SurfaceFlinger( 968): renderer : PowerVR SGX 530
    I/SurfaceFlinger( 968): version : OpenGL ES-CM 1.1
    I/SurfaceFlinger( 968): extensions: GL_OES_byte_coordinates GL_OES_fixed_point GL_OES_single_precision GL_OES_matrix_get GL_OES_read_format GL_OES_compressed_paletted_texture GL_OES_point_sprite GL_OES_point_size_array GL_OES_matrix_palette GL_OES_draw_texture GL_OES_query_matrix GL_OES_texture_env_crossbar GL_OES_texture_mirrored_repeat GL_OES_texture_cube_map GL_OES_blend_subtract GL_OES_blend_func_separate GL_OES_blend_equation_separate GL_OES_stencil_wrap GL_OES_extended_matrix_palette GL_OES_framebuffer_object GL_OES_rgb8_rgba8 GL_OES_depth24 GL_OES_stencil8 GL_OES_compressed_ETC1_RGB8_texture GL_OES_mapbuffer GL_OES_EGL_image GL_EXT_multi_draw_arrays GL_OES_required_internalformat GL_IMG_read_format GL_IMG_texture_compression_pvrtc GL_IMG_texture_format_BGRA8888 GL_EXT_texture_format_BGRA8888 GL_IMG_texture_stream GL_OES_egl_sync GL_IMG_vertex_array_object
    I/SurfaceFlinger( 968): GL_MAX_TEXTURE_SIZE = 2048
    I/SurfaceFlinger( 968): GL_MAX_VIEWPORT_DIMS = 2048
    I/SurfaceFlinger( 968): flags = 00010000
    D/SensorService( 968): nuSensorService starting...
    E/SensorService( 968): couldn't load sensors module (No such file or directory)
    I/sysproc ( 968): System server: starting Android runtime.
    I/sysproc ( 968): System server: starting Android services.
    I/sysproc ( 968): System server: entering thread pool.
    I/SystemServer( 968): Entered the Android system server!
    I/SystemServer( 968): Entropy Service
    I/SurfaceFlinger( 968): SurfaceFlinger::createNormalSurface format=4
    I/SurfaceFlinger( 968): SurfaceFlinger::createNormalSurface format=4,w=240,h=320,flags=0
    I/SystemServer( 968): Power Manager
    D/libEGL ( 983): loaded /system/lib/egl/libGLES_android.so
    D/libEGL ( 983): loaded /system/lib/egl/libEGL_POWERVR_SGX530_125.so
    D/libEGL ( 983): loaded /system/lib/egl/libGLESv1_CM_POWERVR_SGX530_125.so
    I/SystemServer( 968): Activity Manager
    D/libEGL ( 983): loaded /system/lib/egl/libGLESv2_POWERVR_SGX530_125.so
    W/zipro ( 983): Unable to open zip '/data/local/bootanimation.zip': No such file or directory
    E/SurfaceFlinger( 968): eglSwapBuffers: EGL error 0x3008 (EGL_BAD_DISPLAY)
    W/zipro ( 983): Unable to open zip '/system/media/bootanimation.zip': No such file or directory
    I/ActivityManager( 968): Memory class: 16
    W/UsageStats( 968): Usage stats version changed; dropping
    I/SystemServer( 968): Telephony Registry
    I/SystemServer( 968): Package Manager
    I/installd( 894): new connection
    I/Installer( 968): connecting...
    D/dalvikvm( 968): GC_CONCURRENT freed 181K, 47% free 3034K/5639K, external 716K/1038K, paused 2ms+3ms
    W/PackageManager( 968): Running ENG build: no pre-dexopt!
    D/dalvikvm( 968): GC_CONCURRENT freed 260K, 46% free 3240K/5959K, external 716K/1038K, paused 2ms+3ms
    W/PackageParser( 968): No actions in intent filter at /system/app/Bluetooth.apk Binary XML file line #124
    D/dalvikvm( 968): GC_CONCURRENT freed 220K, 44% free 3453K/6151K, external 716K/1038K, paused 2ms+3ms
    D/PackageManager( 968): No files in app dir /vendor/app
    I/PackageManager( 968): Time to scan packages: 2.216 seconds
    W/PackageManager( 968): Unknown permission com.google.android.gm.permission.WRITE_GMAIL in package com.android.settings
    W/PackageManager( 968): Unknown permission com.google.android.gm.permission.READ_GMAIL in package com.android.settings
    W/PackageManager( 968): Unknown permission com.google.android.googleapps.permission.GOOGLE_AUTH in package com.android.settings
    W/PackageManager( 968): Unknown permission com.google.android.googleapps.permission.GOOGLE_AUTH in package com.android.providers.contacts
    W/PackageManager( 968): Unknown permission com.google.android.googleapps.permission.GOOGLE_AUTH.cp in package com.android.providers.contacts
    W/PackageManager( 968): Unknown permission com.google.android.googleapps.permission.GOOGLE_AUTH.mail in package com.android.contacts
    W/PackageManager( 968): Unknown permission android.permission.ADD_SYSTEM_SERVICE in package com.android.phone
    W/PackageManager( 968): Unknown permission com.google.android.googleapps.permission.GOOGLE_AUTH in package com.android.providers.calendar
    W/PackageManager( 968): Unknown permission com.google.android.googleapps.permission.GOOGLE_AUTH.cl in package com.android.providers.calendar
    W/PackageManager( 968): Unknown permission com.google.android.googleapps.permission.ACCESS_GOOGLE_PASSWORD in package com.android.development
    W/PackageManager( 968): Unknown permission com.google.android.googleapps.permission.GOOGLE_AUTH in package com.android.development
    W/PackageManager( 968): Unknown permission com.google.android.googleapps.permission.GOOGLE_AUTH.ALL_SERVICES in package com.android.development
    W/PackageManager( 968): Unknown permission com.google.android.googleapps.permission.GOOGLE_AUTH.YouTubeUser in package com.android.development
    W/PackageManager( 968): Unknown permission com.google.android.googleapps.permission.GOOGLE_AUTH.mail in package com.android.calendar
    W/PackageManager( 968): Not granting permission android.permission.SEND_DOWNLOAD_COMPLETED_INTENTS to package com.android.browser (protectionLevel=2 flags=0x9be45)
    W/PackageManager( 968): Unknown permission android.permission.READ_OWNER_DATA in package com.android.email
    W/PackageManager( 968): Not granting permission android.permission.DEVICE_POWER to package com.android.deskclock (protectionLevel=2 flags=0x8be45)
    D/dalvikvm( 968): GC_EXPLICIT freed 286K, 45% free 3506K/6279K, external 716K/1038K, paused 33ms
    I/SystemServer( 968): Account Manager
    I/SystemServer( 968): Content Manager
    I/SystemServer( 968): System Content Providers
    I/ActivityThread( 968): Pub settings: com.android.providers.settings.SettingsProvider
    I/SystemServer( 968): Battery Service
    D/SettingsProvider( 968): cache for settings table 'secure' rows=25; fullycached=true
    I/SystemServer( 968): Lights Service
    I/SystemServer( 968): Vibrator Service
    D/SettingsProvider( 968): cache for settings table 'system' rows=49; fullycached=true
    I/SystemServer( 968): Alarm Manager
    I/SystemServer( 968): Init Watchdog
    I/SystemServer( 968): Window Manager
    I/InputManager( 968): Initializing input manager
    I/InputManager( 968): Starting input manager
    I/SystemServer( 968): Bluetooth Service
    E/EventHub( 968): could not get driver version for /dev/input/mice, Not a typewriter
    I/EventHub( 968): New device: path=/dev/input/event1 name=ADS7846 Touchscreen id=0x10000 (of 0x1) index=1 fd=82 classes=0x4
    E/EventHub( 968): could not get driver version for /dev/input/mouse0, Not a typewriter
    I/EventHub( 968): New keyboard: device->id=0x10001 devname='TWL4030 Keypad' propName='hw.keyboards.65537.devname' keylayout='/system/usr/keylayout/TWL4030_Keypad.kl'
    I/EventHub( 968): New device: path=/dev/input/event0 name=TWL4030 Keypad id=0x10001 (of 0x2) index=2 fd=84 classes=0x1
    I/InputReader( 968): Device added: id=0x0, name=TWL4030 Keypad, sources=00000101
    I/InputReader( 968): Device added: id=0x10000, name=ADS7846 Touchscreen, sources=00001002
    I/InputManager-Callbacks( 968): No input device calibration properties found for device TWL4030 Keypad.
    I/InputManager-Callbacks( 968): No input device calibration properties found for device ADS7846 Touchscreen.
    I/BluetoothProfileState( 968): Message:Entering Stable State
    I/BluetoothProfileState( 968): Message:Entering Stable State
    I/SystemServer( 968): Device Policy
    I/SystemServer( 968): Status Bar
    I/SystemServer( 968): Clipboard Service
    I/SystemServer( 968): Input Method Service
    I/InputManagerService( 968): Enabled input methods: com.android.inputmethod.latin/.LatinIME
    I/SystemServer( 968): NetStat Service
    I/SystemServer( 968): NetworkManagement Service
    I/SystemServer( 968): Connectivity Service
    I/WifiService( 968): WifiService starting up with Wi-Fi disabled
    D/NetworkManagmentService( 968): Registering observer
    I/SystemServer( 968): Throttle Service
    I/SystemServer( 968): Accessibility Manager
    I/SystemServer( 968): Mount Service
    I/SystemServer( 968): Notification Manager
    I/SystemServer( 968): Device Storage Monitor
    I/SystemServer( 968): Location Manager
    I/PackageManager( 968): Updating external media status from unmounted to unmounted
    D/VoldCmdListener( 887): volume list
    I/SystemServer( 968): Search Service
    D/VoldCmdListener( 887): share status ums
    I/SystemServer( 968): DropBox Service
    I/SystemServer( 968): Wallpaper Service
    I/SystemServer( 968): Audio Service
    D/dalvikvm( 968): GC_CONCURRENT freed 196K, 42% free 3777K/6471K, external 716K/1038K, paused 2ms+4ms
    W/AudioPolicyManagerALSA( 892): setPhoneState() setting same state 0
    I/SystemServer( 968): Headset Observer
    W/HeadsetObserver( 968): This kernel does not have wired headset support
    I/SystemServer( 968): HDMI Observer
    I/SystemServer( 968): Dock Observer
    W/DockObserver( 968): This kernel does not have dock station support
    I/SystemServer( 968): USB Service
    W/UsbDeviceSettingsManager( 968): settings file not found
    I/UsbService( 968): This kernel does not have USB configuration switch support
    I/SystemServer( 968): UI Mode Manager Service
    I/SystemServer( 968): Backup Service
    V/BackupManagerService( 968): No ancestral data
    I/BackupManagerService( 968): Found stale backup journal, scheduling
    I/BackupManagerService( 968): android
    I/BackupManagerService( 968): com.android.inputmethod.latin
    I/BackupManagerService( 968): com.android.browser
    I/BackupManagerService( 968): com.android.providers.userdictionary
    I/BackupManagerService( 968): com.android.providers.settings
    I/BackupManagerService( 968): Backup enabled => false
    I/SystemServer( 968): AppWidget Service
    I/SystemServer( 968): Recognition Service
    I/SystemServer( 968): DiskStats Service
    I/WindowManager( 968): SAFE MODE not enabled
    D/dalvikvm( 968): JIT started for system_server
    E/lights ( 968): write_int failed to open /sys/class/leds/keyboard-backlight/brightness
    D/PowerManagerService( 968): system ready!
    I/lights ( 968): write_int failed to open /sys/class/backlight/omap3evm-bklight/brightness
    I/ActivityManager( 968): System now ready
    I/SystemServer( 968): Making services ready
    I/StatusBarManagerService( 968): Starting service: ComponentInfo{com.android.systemui/com.android.systemui.statusbar.StatusBarService}
    I/Zygote ( 968): Process: zygote socket opened
    I/SurfaceFlinger( 968): SurfaceFlinger::createNormalSurface format=-2
    I/SurfaceFlinger( 968): SurfaceFlinger::createNormalSurface format=1,w=12,h=20,flags=0
    I/ActivityManager( 968): Start proc com.android.systemui for service com.android.systemui/.statusbar.StatusBarService: pid=1036 uid=1000 gids={3002, 3001, 3003}
    I/ActivityManager( 968): Config changed: { scale=1.0 imsi=0/0 loc=md_US touch=3 keys=1/1/2 nav=1/1 orien=1 layout=17 uiMode=0 seq=2}
    I/ActivityManager( 968): Config changed: { scale=1.0 imsi=0/0 loc=md_US touch=3 keys=1/1/2 nav=1/1 orien=1 layout=17 uiMode=17 seq=3}
    W/RecognitionManagerService( 968): no available voice recognition services found
    I/ActivityManager( 968): Start proc com.android.inputmethod.latin for service com.android.inputmethod.latin/.LatinIME: pid=1050 uid=10017 gids={}
    W/ActivityManager( 968): Unable to start service Intent { act=@0 }: not found
    W/ActivityManager( 968): Unable to start service Intent { act=@0 }: not found
    D/NetworkManagmentService( 968): Registering observer
    E/ThrottleService( 968): Could not open GPS configuration file /etc/gps.conf
    I/ActivityManager( 968): Start proc com.android.phone for added application com.android.phone: pid=1060 uid=1001 gids={3002, 3001, 3003, 1015}
    I/ActivityManager( 968): Starting: Intent { act=android.intent.action.MAIN cat=[android.intent.category.HOME] flg=0x10000000 cmp=com.android.launcher/com.android.launcher2.Launcher } from pid 0
    D/dalvikvm( 968): GREF has increased to 201
    I/ActivityManager( 968): Start proc com.android.launcher for activity com.android.launcher/com.android.launcher2.Launcher: pid=1062 uid=10029 gids={}
    I/SystemServer( 968): Enabled StrictMode for system server main thread.
    D/dalvikvm( 1036): GC_CONCURRENT freed 350K, 51% free 2786K/5575K, external 716K/1038K, paused 2ms+2ms
    D/dalvikvm( 1050): GC_CONCURRENT freed 393K, 51% free 2809K/5639K, external 716K/1038K, paused 2ms+3ms
    I//system/bin/tc( 888): Cannot find device "rmnet0"
    I/logwrapper( 888): /system/bin/tc terminated by exit(1)
    I//system/bin/tc( 888): Cannot find device "rmnet0"
    I/logwrapper( 888): /system/bin/tc terminated by exit(1)
    I//system/bin/tc( 888): Cannot find device "ifb0"
    I/logwrapper( 888): /system/bin/tc terminated by exit(1)
    D/dalvikvm( 968): GC_EXTERNAL_ALLOC freed 216K, 41% free 3908K/6599K, external 1035K/1038K, paused 49ms
    I/ActivityManager( 968): Start proc android.process.acore for content provider com.android.providers.userdictionary/.UserDictionaryProvider: pid=1094 uid=10006 gids={3003, 1015}
    I/StatusBarManagerService( 968): registerStatusBar bar=com.android.internal.statusbar.IStatusBar$Stub$Proxy@40567758
    D/dalvikvm( 1060): GC_CONCURRENT freed 403K, 51% free 2812K/5639K, external 716K/1038K, paused 2ms+24ms
    I/ActivityThread( 1060): Pub mms: com.android.providers.telephony.MmsProvider
    I/ActivityThread( 1060): Pub sms: com.android.providers.telephony.SmsProvider
    I/ActivityThread( 1060): Pub telephony: com.android.providers.telephony.TelephonyProvider
    I/ActivityThread( 1060): Pub icc: com.android.phone.IccProvider
    I/ActivityThread( 1060): Pub mms-sms: com.android.providers.telephony.MmsSmsProvider
    D/VoldCmdListener( 887): share status ums
    D/StorageNotification( 1036): Startup with UMS connection false (media state unmounted)
    D/dalvikvm( 1050): GC_EXTERNAL_ALLOC freed 68K, 49% free 2890K/5639K, external 1020K/1038K, paused 49ms
    I/StorageNotification( 1036): UMS connection changed to false (media state unmounted)
    I/ActivityThread( 1062): Pub com.android.launcher2.settings: com.android.launcher2.LauncherProvider
    D/dalvikvm( 1062): GC_CONCURRENT freed 401K, 51% free 2797K/5639K, external 716K/1038K, paused 20ms+2ms
    I/ActivityThread( 1094): Pub com.android.social: com.android.providers.contacts.SocialProvider
    I/ActivityThread( 1094): Pub applications: com.android.providers.applications.ApplicationsProvider
    D/dalvikvm( 1094): GC_CONCURRENT freed 393K, 51% free 2781K/5639K, external 716K/1038K, paused 2ms+2ms
    D/dalvikvm( 968): GC_CONCURRENT freed 257K, 41% free 4032K/6727K, external 1297K/1567K, paused 3ms+3ms
    D/CallManager( 1060): registerPhone(GSM Handler{405175c8})
    I/ActivityThread( 1094): Pub contacts;com.android.contacts: com.android.providers.contacts.ContactsProvider2
    W/AudioPolicyManagerALSA( 892): AudioPolicyManagerALSA::getStrategyForStream() Stub Called...
    W/AudioPolicyManagerALSA( 892): redirecting AudioPolicyManagerALSA::getStrategy()
    W/ActivityManager( 968): Unable to start service Intent { act=com.android.ussd.IExtendedNetworkService }: not found
    I/TelephonyRegistry( 968): notifyServiceState: 1 home null null null Unknown CSS not supported -1 -1RoamInd: -1DefRoamInd: -1EmergOnly: false
    I/TelephonyRegistry( 968): notifyDataConnection: state=0 isDataConnectivityPossible=false reason=radioTurnedOff interfaceName=null networkType=0
    I/TelephonyRegistry( 968): notifyDataConnection: state=0 isDataConnectivityPossible=false reason=gprsDetached interfaceName=null networkType=0
    D/BT HSHFP( 1060): Starting BluetoothHeadsetService
    I/SurfaceFlinger( 968): SurfaceFlinger::createNormalSurface format=2
    I/SurfaceFlinger( 968): SurfaceFlinger::createNormalSurface format=1,w=1,h=1,flags=0
    D/dalvikvm( 1062): GC_EXTERNAL_ALLOC freed 46K, 50% free 2843K/5639K, external 1032K/1038K, paused 70ms
    I/ActivityThread( 1094): Pub call_log: com.android.providers.contacts.CallLogProvider
    I/ActivityThread( 1094): Pub user_dictionary: com.android.providers.userdictionary.UserDictionaryProvider
    I/SurfaceFlinger( 968): SurfaceFlinger::createNormalSurface format=-2
    I/SurfaceFlinger( 968): SurfaceFlinger::createNormalSurface format=1,w=1,h=1,flags=0
    I/ActivityManager( 968): Displayed com.android.launcher/com.android.launcher2.Launcher: +1s936ms
    D/dalvikvm( 1062): GC_EXTERNAL_ALLOC freed 57K, 49% free 2910K/5639K, external 1561K/1572K, paused 48ms
    I/SurfaceFlinger( 968): SurfaceFlinger::createNormalSurface format=-3
    I/SurfaceFlinger( 968): SurfaceFlinger::createNormalSurface format=1,w=240,h=320,flags=0
    D/dalvikvm( 968): GC_EXTERNAL_ALLOC freed 313K, 41% free 4096K/6855K, external 1468K/1567K, paused 89ms
    I/SurfaceFlinger( 968): SurfaceFlinger::createNormalSurface format=-3
    I/SurfaceFlinger( 968): SurfaceFlinger::createNormalSurface format=1,w=240,h=1,flags=0
    D/OtaStartupReceiver( 1060): Not a CDMA phone, no need to process OTA
    D/PowerManagerService( 968): bootCompleted
    D/VoldCmdListener( 887): volume mount /mnt/sdcard
    I/SearchManagerService( 968): Building list of searchable activities
    I/RecoverySystem( 968): No recovery log file
    I/Vold ( 887): /dev/block/vold/179:3 being considered for volume sdcard
    D/Vold ( 887): Volume sdcard state changing 1 (Idle-Unmounted) -> 3 (Checking)
    I/StorageNotification( 1036): Media {/mnt/sdcard} state changed from {unmounted} -> {checking}
    I/ActivityManager( 968): Start proc com.android.mms for broadcast com.android.mms/.transaction.MmsSystemEventReceiver: pid=1132 uid=10005 gids={3003, 1015}
    I/SurfaceFlinger( 968): SurfaceFlinger::createNormalSurface format=4
    I/SurfaceFlinger( 968): SurfaceFlinger::createNormalSurface format=4,w=1,h=1,flags=0
    I/SurfaceFlinger( 968): Boot is finished (7742 ms)
    W/logwrapper( 1135): Unable to background process (No such file or directory)
    I//system/bin/fsck_msdos( 887): ** /dev/block/vold/179:3
    I//system/bin/fsck_msdos( 887): ** Phase 1 - Read and Compare FATs
    I//system/bin/fsck_msdos( 887): Attempting to allocate 872 KB for FAT
    I//system/bin/fsck_msdos( 887): Attempting to allocate 872 KB for FAT
    I/ActivityThread( 1132): Pub com.android.mms.SuggestionsProvider: com.android.mms.SuggestionsProvider
    D/dalvikvm( 1132): GC_CONCURRENT freed 403K, 51% free 2792K/5639K, external 716K/1038K, paused 3ms+2ms
    I/ActivityManager( 968): Start proc android.process.media for content provider com.android.providers.downloads/.DownloadProvider: pid=1142 uid=10007 gids={1015, 2001, 3003}
    I/ActivityManager( 968): Process android.process.acore (pid 1094) has died.
    I/ActivityManager( 968): Low Memory: No more background processes.
    I//system/bin/fsck_msdos( 887): ** Phase 2 - Check Cluster Chains
    I//system/bin/fsck_msdos( 887): ** Phase 3 - Checking Directories
    I//system/bin/fsck_msdos( 887): ** Phase 4 - Checking for Lost Files
    I//system/bin/fsck_msdos( 887): 52 files, 840580 free (210145 clusters)
    I/Vold ( 887): Filesystem check completed OK
    I/Vold ( 887): Device /dev/block/vold/179:3, target /mnt/sdcard mounted @ /mnt/secure/staging
    D/Vold ( 887): Volume sdcard state changing 3 (Checking) -> 4 (Mounted)
    I/PackageManager( 968): Updating external media status from unmounted to mounted
    I/ActivityThread( 1142): Pub media: com.android.providers.media.MediaProvider
    I/StorageNotification( 1036): Media {/mnt/sdcard} state changed from {checking} -> {mounted}
    D/VoldCmdListener( 887): asec list
    D/dalvikvm( 968): GREF has increased to 301
    I/ActivityManager( 968): Start proc com.android.deskclock for broadcast com.android.deskclock/.AlarmInitReceiver: pid=1162 uid=10010 gids={}
    V/MediaProvider( 1142): Attached volume: internal
    I/PackageManager( 968): No secure containers on sdcard
    W/PackageManager( 968): Unknown permission com.google.android.gm.permission.WRITE_GMAIL in package com.android.settings
    W/PackageManager( 968): Unknown permission com.google.android.gm.permission.READ_GMAIL in package com.android.settings
    W/PackageManager( 968): Unknown permission com.google.android.googleapps.permission.GOOGLE_AUTH in package com.android.settings
    W/PackageManager( 968): Unknown permission com.google.android.googleapps.permission.GOOGLE_AUTH in package com.android.providers.contacts
    W/PackageManager( 968): Unknown permission com.google.android.googleapps.permission.GOOGLE_AUTH.cp in package com.android.providers.contacts
    W/PackageManager( 968): Unknown permission com.google.android.googleapps.permission.GOOGLE_AUTH.mail in package com.android.contacts
    W/PackageManager( 968): Unknown permission android.permission.ADD_SYSTEM_SERVICE in package com.android.phone
    W/PackageManager( 968): Unknown permission com.google.android.googleapps.permission.GOOGLE_AUTH in package com.android.providers.calendar
    W/PackageManager( 968): Unknown permission com.google.android.googleapps.permission.GOOGLE_AUTH.cl in package com.android.providers.calendar
    W/PackageManager( 968): Unknown permission com.google.android.googleapps.permission.ACCESS_GOOGLE_PASSWORD in package com.android.development
    W/PackageManager( 968): Unknown permission com.google.android.googleapps.permission.GOOGLE_AUTH in package com.android.development
    W/PackageManager( 968): Unknown permission com.google.android.googleapps.permission.GOOGLE_AUTH.ALL_SERVICES in package com.android.development
    W/PackageManager( 968): Unknown permission com.google.android.googleapps.permission.GOOGLE_AUTH.YouTubeUser in package com.android.development
    W/PackageManager( 968): Unknown permission com.google.android.googleapps.permission.GOOGLE_AUTH.mail in package com.android.calendar
    W/PackageManager( 968): Not granting permission android.permission.SEND_DOWNLOAD_COMPLETED_INTENTS to package com.android.browser (protectionLevel=2 flags=0x9be45)
    D/dalvikvm( 1142): GC_CONCURRENT freed 411K, 51% free 2790K/5639K, external 716K/1038K, paused 2ms+35ms
    V/MediaProvider( 1142): /mnt/sdcard volume ID: -570179281
    D/dalvikvm( 1062): GC_EXTERNAL_ALLOC freed 113K, 48% free 2965K/5639K, external 2090K/2091K, paused 121ms
    D/dalvikvm( 1060): GC_CONCURRENT freed 206K, 48% free 3011K/5703K, external 716K/1038K, paused 2ms+3ms
    V/MediaProvider( 1142): Attached volume: external
    I/ActivityThread( 1142): Pub downloads: com.android.providers.downloads.DownloadProvider
    W/PackageManager( 968): Unknown permission android.permission.READ_OWNER_DATA in package com.android.email
    W/PackageManager( 968): Not granting permission android.permission.DEVICE_POWER to package com.android.deskclock (protectionLevel=2 flags=0x8be45)
    D/dalvikvm( 1062): GC_EXPLICIT freed 40K, 49% free 2930K/5639K, external 1982K/2467K, paused 58ms
    I/ActivityThread( 1142): Pub drm: com.android.providers.drm.DrmProvider
    D/dalvikvm( 968): GC_CONCURRENT freed 445K, 42% free 4171K/7111K, external 1565K/2765K, paused 3ms+12ms
    I/ActivityThread( 1162): Pub com.android.deskclock: com.android.deskclock.AlarmProvider
    D/dalvikvm( 1162): GC_CONCURRENT freed 327K, 51% free 2772K/5575K, external 716K/1038K, paused 2ms+2ms
    I/ActivityManager( 968): Start proc com.android.providers.calendar for broadcast com.android.providers.calendar/.CalendarReceiver: pid=1177 uid=10020 gids={3003}
    D/dalvikvm( 891): GC_EXPLICIT freed 10K, 50% free 2708K/5379K, external 716K/1038K, paused 54ms
    D/dalvikvm( 891): GC_EXPLICIT freed <1K, 50% free 2708K/5379K, external 716K/1038K, paused 37ms
    D/dalvikvm( 891): GC_EXPLICIT freed <1K, 50% free 2708K/5379K, external 716K/1038K, paused 39ms
    I/ActivityThread( 1177): Pub com.android.calendar: com.android.providers.calendar.CalendarProvider2
    D/dalvikvm( 1177): GC_CONCURRENT freed 387K, 51% free 2768K/5639K, external 716K/1038K, paused 2ms+2ms
    I/ActivityManager( 968): Start proc com.android.bluetooth for broadcast com.android.bluetooth/.opp.BluetoothOppReceiver: pid=1196 uid=10022 gids={3003, 3002, 3001, 1015}
    I/ActivityManager( 968): Process android.process.media (pid 1142) has died.
    D/Calendar( 1177): missed alarms found: 0
    I/ActivityThread( 1196): Pub com.android.bluetooth.opp: com.android.bluetooth.opp.BluetoothOppProvider
    I/ActivityManager( 968): Start proc com.android.email for broadcast com.android.email/.service.EmailBroadcastReceiver: pid=1205 uid=10023 gids={3003, 1015}
    I/ActivityManager( 968): Process com.android.mms (pid 1132) has died.
    I/ActivityThread( 1205): Pub com.android.email.provider: com.android.email.provider.EmailProvider
    I/ActivityThread( 1205): Pub com.android.email.attachmentprovider: com.android.email.provider.AttachmentProvider
    I/ActivityThread( 1205): Pub com.android.exchange.provider: com.android.exchange.provider.ExchangeProvider
    I/ActivityManager( 968): Start proc android.process.media for broadcast com.android.providers.downloads/.DownloadReceiver: pid=1224 uid=10007 gids={1015, 2001, 3003}
    I/ActivityManager( 968): Process com.android.deskclock (pid 1162) has died.
    D/EAS SyncManager( 1205): !!! EAS SyncManager, onCreate
    I/ActivityThread( 1224): Pub media: com.android.providers.media.MediaProvider
    V/MediaProvider( 1224): Attached volume: internal
    V/MediaProvider( 1224): /mnt/sdcard volume ID: -570179281
    D/dalvikvm( 1205): GC_FOR_MALLOC freed 496K, 51% free 2910K/5831K, external 716K/1038K, paused 35ms
    V/MediaProvider( 1224): Attached volume: external
    I/ActivityThread( 1224): Pub downloads: com.android.providers.downloads.DownloadProvider
    I/ActivityThread( 1224): Pub drm: com.android.providers.drm.DrmProvider
    D/Eas Debug( 1205): Logging:
    D/Email ( 1205): BOOT_COMPLETED
    I/ActivityManager( 968): Start proc com.android.quicksearchbox for broadcast com.android.quicksearchbox/.SearchWidgetProvider: pid=1239 uid=10012 gids={3003}
    I/ActivityManager( 968): Process com.android.bluetooth (pid 1196) has died.
    I/ActivityManager( 968): Low Memory: No more background processes.
    D/EAS SyncManager( 1205): !!! EAS SyncManager, onDestroy
    D/MediaScannerService( 1224): start scanning volume internal
    D/EAS SyncManager( 1205): !!! EAS SyncManager, onCreate
    D/EAS SyncManager( 1205): !!! EAS SyncManager, onStartCommand
    D/dalvikvm( 1205): GC_CONCURRENT freed 108K, 50% free 2932K/5831K, external 716K/1038K, paused 2ms+7ms
    D/EAS SyncManager( 1205): !!! EAS SyncManager, stopping self
    D/EAS SyncManager( 1205): !!! EAS SyncManager, onDestroy
    I/ActivityThread( 1239): Pub com.android.quicksearchbox.google: com.android.quicksearchbox.google.GoogleSuggestionProvider
    I/ActivityThread( 1239): Pub com.android.quicksearchbox.shortcuts: com.android.quicksearchbox.ShortcutsProvider
    I/ActivityManager( 968): Start proc com.android.music for broadcast com.android.music/.MediaAppWidgetProvider: pid=1252 uid=10013 gids={3003, 1015}
    I/ActivityManager( 968): Process com.android.email (pid 1205) has died.
    D/dalvikvm( 1224): GC_CONCURRENT freed 520K, 51% free 2832K/5767K, external 716K/1038K, paused 2ms+2ms
    D/MediaScanner( 1224): prescan time: 319ms
    D/MediaScanner( 1224): scan time: 59ms
    D/MediaScanner( 1224): postscan time: 0ms
    D/MediaScanner( 1224): total time: 378ms
    D/MediaScannerService( 1224): done scanning volume internal
    I/ActivityManager( 968): Start proc com.cooliris.media for broadcast com.cooliris.media/com.cooliris.cache.BootReceiver: pid=1263 uid=10028 gids={1015, 3003}
    I/ActivityThread( 1263): Pub com.cooliris.picasa.contentprovider: com.cooliris.picasa.PicasaContentProvider
    I/ActivityManager( 968): Process com.android.music (pid 1252) has died.
    D/dalvikvm( 1263): GC_CONCURRENT freed 608K, 53% free 2797K/5831K, external 716K/1038K, paused 2ms+6ms
    I/BootReceiver( 1263): Got intent with action android.intent.action.MEDIA_MOUNTED
    I/BootReceiver( 1263): Got intent with action android.intent.action.MEDIA_SCANNER_FINISHED
    D/MediaScannerService( 1224): start scanning volume external
    D/MediaScanner( 1224): prescan time: 37ms
    D/MediaScanner( 1224): scan time: 14ms
    D/MediaScanner( 1224): postscan time: 0ms
    D/MediaScanner( 1224): total time: 51ms
    I/BootReceiver( 1263): Got intent with action android.intent.action.MEDIA_SCANNER_FINISHED
    D/MediaScannerService( 1224): done scanning volume external
    I/InputReader( 968): Device reconfigured: id=0x10000, name=ADS7846 Touchscreen, display size is now 240x320
    I/InputManager-Callbacks( 968): No virtual keys found for device ADS7846 Touchscreen.
    D/dalvikvm( 968): GC_CONCURRENT freed 751K, 45% free 4118K/7367K, external 1565K/2765K, paused 6ms+4ms

  • Looks like SGX is not started. Can you make sure whether the SGX services started?

    Regards,

    Arun

  • Hi Arun Joseph,

    thanks for your reply!

    look at the logcat:

    ..

    D/libEGL ( 968): loaded /system/lib/egl/libGLES_android.so
    D/libEGL ( 968): loaded /system/lib/egl/libEGL_POWERVR_SGX530_125.so
    D/libEGL ( 968): loaded /system/lib/egl/libGLESv1_CM_POWERVR_SGX530_125.so
    D/libEGL ( 968): loaded /system/lib/egl/libGLESv2_POWERVR_SGX530_125.so
    W/SurfaceFlinger( 968): ro.sf.lcd_density not defined, using 160 dpi by default.
    E/libEGL ( 968): eglSetSwapRectangleANDROID:1844 error 3008 (EGL_BAD_DISPLAY)
    I/SurfaceFlinger( 968): EGL informations:
    I/SurfaceFlinger( 968): # of configs : 36
    I/SurfaceFlinger( 968): vendor : Android
    I/SurfaceFlinger( 968): version : 1.4 Android META-EGL
    I/SurfaceFlinger( 968): extensions: EGL_KHR_image EGL_KHR_image_base EGL_KHR_image_pixmap EGL_ANDROID_image_native_buffer EGL_ANDROID_swap_rectangle 
    I/SurfaceFlinger( 968): Client API: OpenGL ES
    I/SurfaceFlinger( 968): EGLSurface: 8-8-8-8, config=0x1
    I/SurfaceFlinger( 968): OpenGL informations:
    I/SurfaceFlinger( 968): vendor : Imagination Technologies
    I/SurfaceFlinger( 968): renderer : PowerVR SGX 530
    I/SurfaceFlinger( 968): version : OpenGL ES-CM 1.1
    I/SurfaceFlinger( 968): extensions: GL_OES_byte_coordinates GL_OES_fixed_point GL_OES_single_precision GL_OES_matrix_get GL_OES_read_format GL_OES_compressed_paletted_texture GL_OES_point_sprite

    ...


    Doesn't this meaning the SGX services had started ?

    If not ,and how to start SGX?

    And from another post,

    http://e2e.ti.com/support/embedded/android/f/509/p/111385/485431.aspx 

    Pankaj Bharadiya said the SGX clock should be 200MHz ,but my sgx_fck/rate is 100000000,

    and patch as following didn't work 

    diff --git a/arch/arm/mach-omap2/clock34xx_data.c b/arch/arm/mach-omap2/clock34xx_data.c
    index e3c752f..89e2f61 100644
    --- a/arch/arm/mach-omap2/clock34xx_data.c
    13 +++ b/arch/arm/mach-omap2/clock34xx_data.c
    @@ -3325,8 +3325,8 @@ static struct omap_clk omap3xxx_clks[] = {
    CLK(NULL, "gfx_l3_ick", &gfx_l3_ick, CK_3430ES1),
    CLK(NULL, "gfx_cg1_ck", &gfx_cg1_ck, CK_3430ES1),
    CLK(NULL, "gfx_cg2_ck", &gfx_cg2_ck, CK_3430ES1),
    - CLK(NULL, "sgx_fck", &sgx_fck, CK_3430ES2 | CK_3517),
    - CLK(NULL, "sgx_ick", &sgx_ick, CK_3430ES2 | CK_3517),
    + CLK(NULL, "sgx_fck", &sgx_fck, CK_3430ES2 | CK_3517 | CK_36XX),
    + CLK(NULL, "sgx_ick", &sgx_ick, CK_3430ES2 | CK_3517 | CK_36XX),
    CLK(NULL, "d2d_26m_fck", &d2d_26m_fck, CK_3430ES1),
    CLK(NULL, "modem_fck", &modem_fck, CK_343X),
    CLK(NULL, "sad2d_ick", &sad2d_ick, CK_343X),
    --

  • HI,

    Looks like somehow SGX drivers are not loaded or SGX initialization is not happened.  Can you check the following things?

    1. Check lsmod to see omaplfb.ko and pvrsvrkm.ko loaded
    2. See all the steps in rc.pvr service from init.rc are executed
    3. You have a file gralloc.omap3.so at /system/lib/hw/

    Regards,

    Arun

  • hi 

    can you please check below link for your Referance

    http://e2e.ti.com/support/embedded/android/f/509/p/156457/592233.aspx#592233

    Thanks 

    Bhagavath

  • Arun Joseph said:

    HI,

    Looks like somehow SGX drivers are not loaded or SGX initialization is not happened.  Can you check the following things?

    1. Check lsmod to see omaplfb.ko and pvrsvrkm.ko loaded
    2. See all the steps in rc.pvr service from init.rc are executed
    3. You have a file gralloc.omap3.so at /system/lib/hw/

    Regards,

    Arun

    1. yes, they both loaded

    2. In init.rc:

       service pvr /system/bin/sgx/rc.pvr start

      which is load_pvr:

    load_pvr()
    {

    insmod /system/bin/sgx/pvrsrvkm.ko
    insmod /system/bin/sgx/omaplfb.ko
    sleep 1
    chmod 0666 /dev/pvrsrvkm
    pvrsrvinit
    echo "Loaded PowerVR consumer services."
    return 0;
    }

    but I could not see "Loaded PowerVR consumer services." in debug info

    3. there is gralloc.omap3.so at /system/lib/hw/

  • Bhagavath Ram said:

    hi 

    can you please check below link for your Referance

    http://e2e.ti.com/support/embedded/android/f/509/p/156457/592233.aspx#592233

    Thanks 

    Bhagavath

    HI

    but that didn't work

  • I used DDMS tools to capture screen ,but I get nothing ,as follow:


  • but when changed the FileSystem to android2.3.4 the screen capture was fine,and screenshot as follows:


  • It was the DSS interface CONTROL_PADCONF problem.