This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Should MMC lines have internal pullups enabled if there are external pullup resistors in the circuit



I have a board that has 10K pullup resistors on the lines to the micro SD card.  Should I enable or disable the CPU internal pullups in this situation?