This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SRIO_LoopbackTestProject

Hi,

I'm testing SRIO_LoopbackTestProject at C6678EVM. (CCS 5.2.1 with mcsdk 2_01_02_05)

I removed Application managed test code section, (This is for simplicity because I only need Driver managed code. Anyway, whether I remove it or not, the following result is always same.) and compiled and load and tested successfully at debug mode.

Now, when I press Suspend, Restart, Resume is sequence, it always fail at read test. SRIO_sockSend() seems to works well, but following SRIO_sockRecv() always blocked or receive 0 byte(at non-blocking). Even if I restart CCS and reload the at debugger, it still not works. The only solution is turn off the EVM power and turn it on again.

So, in brief, it seems SRIO_LoopbackTestProject works just once after power on.

Is this normal situation ? How can I repeat the test without touching power switch ?

Regards,

Stellar