Hi,
We are evaluating the TI DM3730 for a major project and have acquired a batch of Beagle boards (xM Rec C) in order to do so. We wish to use a TI PSP as we will be moving to a TI EVM later.
Is AM35x-OMAP35x-PSP 04.02.00.07 the correct PSP for this board? We have built the x-loader and kernel etc using the instructions provided with this PSP and get no response when booting them.
For example the x-loader is built using config:
make CROSS_COMPILE=arm-none-linux-gnueabi- ARCH=arm omap3beagle_config
and then signed and renamed to MLO (as required by the BBxM). This file is then placed on the boot partition of the uSD card and the card powers up with zero response. I have tried using the PSP kernel with a working (Angstrom) x-loader and u-boot but it also fails to run after loading. Any ideas?
Many thanks,
Dave