Hi,all.
Maybe it's a question of audio if it doesn't match this forums, Tiers you can move it. :-)
Sorry for poor english.
We meet a speech decode problem.
When we decode the 1.g711 cmd: ./decode -s 1.g711, then Failed to set buffer size (0) , got (32) on plughw:0,0(Success). happened in dmai. And after 8 times sample decode, the progress will stop with this error came: @11,670,003us: [+7 T:0x408c9490] ti.sdo.dmai - [Sound] Failed to write to plughw:0,0 (Unknown error 4294967291-->it's an input/output error when we use stderror) .then speech thread will output: Error: Failed to write audio buffer, and stop this thread.
The dvsdk is 2_10_01_18 and linux kernel is 2.6.18, we use DM365 with aic3101. The whole log we attached. Any other information you need, feel free to ask me.
Advanced Linux Sound Architecture Driver Version 1.0.12rc1 (Thu Jun 22 13:55:50 2006 UTC).
ASoC version 0.13.1
AIC3X Audio Codec 0.2
asoc: aic3x <-> davinci-i2s mapping ok
ALSA device list:
#0: DaVinci DM365 EVM (aic3x)
http://e2e.ti.com/cfs-file.ashx/__key/communityserver-discussions-components-files/100/6433.log.log
brs
jingwei