This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Problem with DM6437 encdec codes...



Hi, I'm new to development boards as well as to this TI's Da Vinci Board of DM6437. As far as the Capture/Preview mode is concerned for video input routed to video output port is concerned it's working fine.

But with the Encoder/Decoder code is concerned, I've having a problem. The code is compiled and gets loaded on the board but no video output is shown on TV device. As far as the STDOUT is concerned, it shows messages: \

Decoder frame 0 Processing failed.   Error: 0xfffff and another error code.

Furthermore, on generated files, it says:         video_encdeccfg.s62 & video_encdeccfg_c.c  (Files not found).

And when i include the GEL file, evmdm6437.gel then the program doesn't runs after being loaded.

Kindly help me, if there's any possible solution available.

Thanks!