Hello,
I'm facing the same problem again after upgrading to JB 4.1.2. And i'm using the same USB driver as provided with ICS. I get the same error "The specified file does not contain information about the hardware". Please help.
I added the following lines into the android_winusb.inf
[Google.NTx86]
;TI EVM-SK
%SingleAdbInterface% = USB_Install, USB\VID_18D1&PID_9018
%CompositeAdbInterface% = USB_Install, USB\VID_18D1&PID_9018&MT_01
I also changed the 9018 to D002 which worked the last time with ICS and was suggested to me in the following post.
http://e2e.ti.com/support/embedded/android/f/509/p/252496/884036.aspx#884036