All
I have a problem about DDR3 RW .
1: Connect A8, Load PG2.1_DM814X_20Mhz_Si.gel.gel and Carry out follow gel scripts.
PG 2.x DM814X --> ALL_ADPLL_CLOCKS_ENABLE_API
PG 2.x DM814X --> DDR3_EMIF0_EMIF1_Config_Full_leveling
2: Write the RW Code like this:
UINT32* test=(UINT32*)0x80000000;
for ( j = 0 ; j < 1024 ; j++ )
{
test[j]=0xffffffff;
}
3 after running the code,I see the result at Memory Broswer
We can see that ,not all datas are FFFFFFFF,It looks like some memory cann't be wrote
I wana konw the reason of this problem.I will give more information if need.
Thanks for your reply very much !