Hi,
i m developing on SK AM335x , i m running linux (SDK 05.05.01.00) .. what i want to do is to toggle a pin .. i have a Userspace Application and a Kernel Module working on SPi..
so first i want to toggle a Pin in a Kernel Module
i want to use one of the user leds LED1-3 above the Power on Button beacause they are not blinking and the OS is not using them.. there must be a driver somewhere to use this Leds ?!?!?
i ve no plan what to do beacause i dont find any kernel Source ( gpio Driver or somthing ) accesing the Hardware .. so what can i do ?
Edit:
somewhere i found
gpio_set_value(NFC_PWRUP_GPIO, 0);
gpio_set_value(NFC_PWRUP_GPIO, 1);
i guess this toggles a pin ?!?! ... but what are the PinNummbers for the User Leds ?? Is there a list of all Pin Nummbers of the Microcontroller ?!?
IF YOU HAVE AN IDEA HOW TO TOGGLE ANY OTHER PIN IT WOULD ALSO BE OK .... LIKE (J8 / I2CHeader ) !?!?
thanx a lot
best regards
aly