This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

NDK shutdown/ reboot does not restore interface

After NDK stack is successfully brought up, used, and then shutdown (or reboot), subsequent attempts to bring the NDK stack back up from software fail, and  can only recover with a System Reset (or power cycle). 

This has been observed on stack version 2_21_02_43 and 2_21_01_38

 

Steps to reproduce:

  1. Using a C6678 EVM, load and run the client_cvmc6678l project (DHCP mode was used)
  2. After the NDK stack comes up and receives an IP address, connect via telnet
  3. Issue 'shutdown' command (or 'reboot')
  4. Observe NDK stack shutdown (or reboot) messages in CCS
  5. Do a pause, restart, and run

NDK stack initialization after a shutdown will look something like this:

<...> 

Ethernet subsystem successfully initialized
Ethernet eventId : 48 and vectId (Interrupt) : 7
Verify_Init: Expected 16 entry count for gTxFreeQHnd queue 736, found 31 entries
Verify_Init: Expected 0 entry count for Queue number = 899, found 1 entries
Verify_Init: Expected 0 entry count for Queue number = 4095, found 2 entries
Warning:Queue handler Verification failed
Registration of the EMAC Successful, waiting for link up ..

Service Status: DHCPC    : Enabled  :          : 000
Service Status: Telnet   : Enabled  :          : 000
Service Status: HTTP     : Enabled  :          : 000
Service Status: DHCPC    : Enabled  : Running  : 000

00000.000 PBM_free: Invalid Packet
00000.000 PBM_enq: Invalid Packet

 

Above procedure repeated with reboot:

<...>

Ethernet subsystem successfully initialized
Error allocating Tx free descriptors
Tx setup failed
Error: Unable to register the EMAC
NIMUIOCTL Failed with error code: -22 

<after a delay of ~60 seconds>

Service Status: DHCPC    : Failed   :          : 000
Service Status: Telnet   : Enabled  :          : 000
Service Status: HTTP     : Enabled  :          : 000

  • Hi Michael,

    I suspect that there is a Hwi after the NC_NetStop() is called which is causing the control back to NC_NetStart() and since it does not have valid arguments now fails to perform Network initialization and NDK stack doesn't come clean.

    I would like to know the functionality of the below lines, part of the helloworld.cfg file :

    /*
     * Enable Event Groups here and registering of ISR for specific GEM INTC is done
     * using EventCombiner_dispatchPlug() and Hwi_eventMap() APIs
     */

    Ecm.eventGroupHwiNum[0] = 7;
    Ecm.eventGroupHwiNum[1] = 8;
    Ecm.eventGroupHwiNum[2] = 9;
    Ecm.eventGroupHwiNum[3] = 10;

    Is there anything that can be inferred from this?

  • Hi Michael,

    Michael Erdahl said:
    • Issue 'shutdown' command (or 'reboot')
    • Observe NDK stack shutdown (or reboot) messages in CCS
    • Do a pause, restart, and run

    I'm curious why you are doing a pause/restart/run at this point?  Are you only doing that for the 'shutdown' case?

    What happens if you do a reboot *without* doing the pause/restart/run?  Does the stack come back up?  Are you able to ping it and telnet back in?

    ----

    Here's some data points:

    I also tried some experiments with reboot and shutdown.  I did the following for both the Concerto (M3) and Freon (C674X):

    • ndk_2_22_03_20
    • bios_6_34_04_22
    • xdctools_3_24_06_63
    • Concerto EMAC driver:
      • TI-RTOS 1.10.00.11 (eng build)
    • Freon EMAC driver:
      • nsp_1_10_01_08_eng
    1. run the app
    2. ping the target - success
    3. telnet into the NDK - success
    4. issue a reboot command - telnet connection is lost and stack reboots - success
    5. ping the target - success
    6. telnet into the NDK - success

    I also tried:

    1. run the app
    2. ping the target - success
    3. telnet into the NDK - success
    4. issue a reboot command - telnet connection is lost and stack reboots - success
    5. pause/restart/run
    6. I'm still able to ping and telnet the target

    I also tried:

    1. run the app
    2. ping the target - success
    3. telnet into the NDK - success
    4. issue a shutdown command - telnet connection is lost and stack shuts down - success
    5. ping the target, no response - success
    6. pause/restart/run
    7. stack comes back
    8. I'm able to ping and telnet the target

    For these two boards, the behavior seems correct.  One difference, however is that my test apps are using static IP addresses.

    Steve

  • Steve,

    Thanks for the reply and your tests. 

    Steven Connell said:

    I'm curious why you are doing a pause/restart/run at this point?  Are you only doing that for the 'shutdown' case?

    Sorry I was not clear enough on this point: I was only doing the pause/reset/run in the shutdown case. 

    I ran the reboot test in both static and dhcp modes, both failed to restart the network interface.  I've instrumented my NDK/ NIMU stack and the problem currently resides in the QMSS/ CPPI configuration- I cannot get any free descriptors the second time around. 

  • Michael,

    Michael Erdahl said:
    I ran the reboot test in both static and dhcp modes, both failed to restart the network interface. 

    Good data point.  This tells us that it's not related to the DHCP client.

    Michael Erdahl said:
    I've instrumented my NDK/ NIMU stack and the problem currently resides in the QMSS/ CPPI configuration- I cannot get any free descriptors the second time around. 

    Another good data point.  I believe the QMSS/CPPI is part of the 6678 EMAC driver.  Given this, and that the problem does not happen on Concerto or Freon, I'd say that the issue you're running into is in the 6678 driver.

    If so, I won't be able to help much with that.  We need to get some help from someone on the MCSDK team who knows the 6678 driver.

    Steve

  • Hi Steve & Michael,

    After running my NDK application which is nothing but modified NDK helloworld for C6678, when I terminate the debug session the PC becomes unstable and a list of log messages appear on the screen after which I would have to restart the PC. This issue occurs not always but sometimes.

    What could be the possible reason for such a behaviour ?

    OS : Ubuntu 12.04

    CCS version : 5.3