This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM642 NDK web sever

TI give a  demo of  creating a web server :

//
// Main Thread
//
// We changed our CDB file to point call this private init
// function. Here we initialize our board and read in our
// MAC address.
//
void dm642_init()
{

    // Init cache mode manually
    CSL_init(); 
    CACHE_clean(CACHE_L2ALL, 0, 0);
    CACHE_setL2Mode(CACHE_128KCACHE);
    CACHE_enableCaching(CACHE_EMIFA_CE00);
    CACHE_enableCaching(CACHE_EMIFA_CE01);

 
 bMacAddr[0]='D'; bMacAddr[1]=4;
 bMacAddr[2]='A'; bMacAddr[3]=1;
 bMacAddr[4]='Z'; bMacAddr[5]=1;

 memcpy(IP_MAC,bMacAddr,6);

}

every time start the system, the code run.

TI gives DM642 a MAC adress of "D:4:A:1:Z:1",can  we  change  this  MAC address?

if  we can , how  we  can  change this?