This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Minimum frame rate in H.264 encoder?

We are using the IPNC RDK 3.5.0 on a DM8127.  When I try to set a frame rate less than 1 fps to the H.264 encoder, the handle->fxns->ividenc.control() call in enclink_h264_control() consistently fails with an XDM_UNSUPPORTEDPARAM return code.  Specifically, I'm setting params->videnc2DynamicParams.refFrameRate and params->videnc2DynamicParams.targetFrameRate both to 500 (that is, 0.5 fps) in the handle->fxns->ividenc.control() call.

Are frame rates less than 1 fps not supported?  Is this a hard limit?  Thanks!