This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

How to configure the UART work in 384K bits/s Baudrate on AM335x

Hi Champ,

   My customer needs the UART work in 384K bits/s Baudrate on AM335x, which is the requirement from one sensor communication.

   According to the TRM, 19.3.8 Protocol Formatting, UART 16x mode (≤230.4 Kbits/s), UART16x ≤460Kbits/s if MDR3[1] is set.

   According to the description for MOD3, when MOD3[1] is set, the FREQ_SEL is necessary to do the configuration as well.

   For the FREQ_SEL, it is configured for the sample per bit, but I didn't find any description for the "sample per bit" here.

   So could you help to supply on what is the sample here?

Yaoming

Thanks!