Hello,
This is not a great problem, but I would be very grateful if you can help me.
I am working with EVM_Sample code with EVM5515. This code is the program loaded in the EVM5515, when we bought it. When I power On the board, a menu is shown in the Display. It says SW:12 LED Blink On; SW11:LED Blink Off... . However, I want to add more options in this menu and I found that in function Get_sar_key (in sar.c) the value of switches do not match with the switches that appears in the LCD.
Moreover, the text in the LCD is correct because when I push this switches they do what it is supposed to do.
I said that it is not a great problem, because I can try to push all buttons but maybe you can help me.
thanks