In the many hours days weeks of reading this forum and assorted documentation I have seen lots of talk about using different imaging paths (for example "ISIF-->RSZ-->DDR") in the DM36x for different purposes, but I have not found any really clear information on how you actually set the path up from within the source code.
By lots of grepping of the source code and tinkering I have video capture working, but it would be really good to have some idea of all the code we should or should not be altering to configure the imager correctly. There doesn't seem to be one single place where an overall configuration file or header is stored, and all of the code is free from comments.
Our setup is Appro IPNC DM368-MT5 4.0.x, input is BT.1120 YUV422, either 720p60 or 1080p30, so all other resolutions must be generated by resizing. We do not need any corrections (LDC, AEWB, NR, etc.), simply to capture full res + resize to one or two smaller streams.
Can any of you gurus out there give either a link to the explanation that I've missed, or a summary of how to set up a couple of example paths/pipes/whatever they are properly called?