we are using IMGDEC1_process on dm365 with JPEG codec 01.00.00.10 recently and it works fine but once i got the error from cmem:
Unable to handle kernel paging request at virtual address 9d6f9d8a
we are now using a loop-queue to index the buff info. the full log is as follow:
[0m[37;40m10:43:36|trace CMediaFileList::onTimerOnEventNotify::event notify [mTime : Thu Apr 25 10:43:36 2013 =========================== TRACE START =================================== Tid:413, Exception type : SIGSEGV [0m[33;40m10:43:36|warn Src/./RtspClient.cpp:685 rtsp connect exception! [0m[33;40m10:43:36|warn Src/./RtspClient.cpp:688 return -1 [0m[31;40m10:43:36|error send failed! Connection reset by peer [0m[31;40m10:43:36|error CStreamSender socket exception! fd: 38 [0m[33;40m10:43:36|warn Src/./StateMachine.cpp:181:execute exception occured! [0m[33;40m10:43:36|warn Src/./MachineKeeper.cpp:64 [0m[33;40m10:43:36|warn Src/./RtspClient.cpp:~CRtspClient client:0x1be2cc0 PC:[0x00034e48] (0x00034dc0--0x00034e63) stack_sig_hook + [0x88] Unable to handle kernel paging request at virtual address 9d6f9d8a PC:[0x401a77c0] (0x00034dc0--0x00034e63) __defaupgd = c203c000 lt_rt_sa_restore[9d6f9d8a] *pgd=00000000r_v2 + [0x0] PC:[0x00099428] (0 x00034dc0--0x000Internal error: Oops: 1 [#1] Modules linked in: mmc_drv mmc_blk mmc_core davinci_fm2018 davinci_evm_tlv320 snd_soc_davinci davinci_i2s_mcbsp aout tlv320aic23 dm365_ad h3ak myvdec vpfek pwm vpbek touch_panel_ctrl i2ckey evdev getjif mymemcpy irqk edmak dm365mmap cmemk davinci_emac gpio CPU: 0 PC is at HeapMem_free+0x40/0xb4 [cmemk] LR is at 0x1000 pc : [<bf00f184>] lr : [<00001000>] Tainted: GF sp : c3477d5c ip : 9d6f9d8a fp : c3477d6c r10: 00000000 r9 : 00000001 r8 : c2025828 r7 : bf013d60 r6 : 00000000 r5 : c2025828 r4 : bf013d40 r3 : 00000001 r2 : 00000128 r1 : c7a4b000 r0 : 9d6f9d8a Flags: Nzcv IRQs on FIQs on Mode SVC_32 Segment user Control: 5317F Table: 8203C000 DAC: 00000015 Process VideoDaemon (pid: 397, stack limit = 0xc3476258) Stack: (0xc3477d5c to 0xc3478000) 7d40: c2025820 7d60: c3477dbc c3477d70 bf00fca4 bf00f154 00000000 00000000 bf013d58 c0c7fb20 7d80: bf013d60 c20257e0 00000000 00000000 c00b59a0 00000008 c0c7fb20 c098a120 7da0: c0b62618 c04b4ea0 00000000 00000000 c3477dec c3477dc0 c0096738 bf00fb28 7dc0: 00000000 c0dd2bc0 c0dd2bf4 c0c7fb20 00000000 c04aba40 c04aba48 00000000 7de0: c3477dfc c3477df0 c0096a00 c0096694 c3477e1c c3477e00 c0092fa8 c00969dc 7e00: c3476000 00001fff c04aba40 00000018 c3477e4c c3477e20 c004bb64 c0092f40 7e20: c3477e4c c04aba40 c0527680 c0ab9070 00000000 0000000b 00000000 c3477f50 7e40: c3477e6c c3477e50 c004d16c c004bae0 c3477e6c 001f24c8 c3477ea0 c3476000 7e60: c3477e84 c3477e70 c004da04 c004cf2c 00000000 00000009 c3477ebc c3477e88 7e80: c00588f0 c004d958 c3477fb0 c0527860 c0054d58 c3476000 00000000 c3477fb0 7ea0: c0034208 c0034208 c3476000 00000000 c3477f9c c3477ec0 c0036dd8 c0058520 7ec0: c3476000 00000001 c0527860 c3477ed8 00000009 00000000 00000000 00000000 7ee0: 00000000 0000000a c3477f14 c3477ef8 c0064078 c3477f88 00000000 0000000a 7f00: bee2ed08 bee2ed08 00000008 00000000 c3477f20 c0063b14 0fb21b40 000013f0 7f20: c149df21 00000000 00000000 00000000 2215fe7d 000013f8 c0063c24 c034dc38 7f40: 00000000 00000002 c3477f48 c3477f48 c0527680 c0059610 00000008 1263e33d 7f60: c3477f88 bee2ed08 00000000 000000a2 c0034208 40024e00 00000000 00000000 7f80: 000000a2 c0034208 c3476000 00000000 c3477fac c3477fa0 c0037258 c0036d90 7fa0: 00000000 c3477fb0 c00340ac c003723c fffffdfc bee2ed08 4001f5a4 00000002 7fc0: 40024e00 00000000 00000000 000000a2 00000000 00000000 40025000 bee2ed1c 7fe0: 00000000 bee2ecf8 400664f4 40067634 80000010 bee2ed10 03f60001 03f70000 Backtrace: [<bf00f144>] (HeapMem_free+0x0/0xb4 [cmemk]) from [<bf00fca4>] (release+0x18c/0x270 [cmemk]) r4 = C2025820 [<bf00fb18>] (release+0x0/0x270 [cmemk]) from [<c0096738>] (__fput+0xb4/0x214) [<c0096684>] (__fput+0x0/0x214) from [<c0096a00>] (fput+0x34/0x38) r8 = 00000000 r7 = C04ABA48 r6 = C04ABA40 r5 = 00000000 r4 = C0C7FB20 [<c00969cc>] (fput+0x0/0x38) from [<c0092fa8>] (filp_close+0x78/0x84) [<c0092f30>] (filp_close+0x0/0x84) from [<c004bb64>] (put_files_struct+0x94/0xe8) r6 = 00000018 r5 = C04ABA40 r4 = 00001FFF [<c004bad0>] (put_files_struct+0x0/0xe8) from [<c004d16c>] (do_exit+0x250/0xa2c) [<c004cf1c>] (do_exit+0x0/0xa2c) from [<c004da04>] (sys_exit_group+0x0/0x1c) [<c004d948>] (do_group_exit+0x0/0xbc) from [<c00588f0>] (get_signal_to_deliver+0x3e0/0x42c) r4 = 00000009 [<c0058510>] (get_signal_to_deliver+0x0/0x42c) from [<c0036dd8>] (do_signal+0x58/0x4ac) [<c0036d80>] (do_signal+0x0/0x4ac) from [<c0037258>] (do_notify_resume+0x2c/0x30) [<c003722c>] (do_notify_resume+0x0/0x30) from [<c00340ac>] (work_pending+0x1c/0x20) Code: 1062e003 e1a0c004 ea000001 e1a0c000 (e5900000) 34e63) JPEGDEC_TI_updateState + [0x18] PC:[0x00084b5c] (0x00034e84--0x00130e0f) IMGDEC1_process + [0x23c] PC:[0x0007f678] (0x00034e84--0x00130e0f) decode_jpeg + [0x1a4] PC:[0x00000004] (0x00034e84--0x00130e0f) Unknown <1>Fixing recursive fault but reboot is needed!
[0m[36;40m10:43:37|[libInfra] debug ThreadBody Enter name = [ringTimer], id = 551, prior = N64, stack = 0x473d6e24
any idea why it just failed once but all goes fine.
Thanks in advance.
Regards, Mike.