All,
A customer has generated a .cfg file for a C6748 using AISgen and they're having issues with their DDR2 memory locking up. I've attached the .cfg file, and I'm curious if anyone might be able to point out some obvious issues, but also, are there any known issues with AISgen? The reason why I ask is because the cfg file does show for some of the registers that it's writing 1's to reserved bits. While this might not be too much of an issue in itself, with the lack of experience I have with AISgen, I'm wondering if there are known bugs.
DDR2: Micron MT47H64M16R-3:H
DSP: 375MHz C6748 (DSP core = 364.8MHz, DDR2 = 148.8MHz), 19.2MHz external oscillator being used
Regards,
Reagan