This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AIF2 usage for data transfer between TMS320C6670 and Xilinx FPGA

Hi I wish to make a connection between 6670 DSP (with respect to each of 4 cores) and FPGA (supporting SERDES link and CPRI protocol).

The operartions to be implemented are read and write.

In my case, previously SRIO was used for this interface but now SRIO is to be used for inter DSP communication. Hence SRIO cannot be used.

I am left with option of using AIF2 peripheral, but unable to decide on which feature/mode I can use for my use case.

After going through the available literature and sample code on AIF2, I believe generic packet mode for CPRI is the most suitable option.

But, I wish to use it for 1.4MHz LTE Rate and see that there is a specific option available in AIF2. But, I am not sure if I can use LTE mode for inter device communication. Can anyone please suggest if LTE mode can be used in my scenario?

 

Also, please suggest on what basis can I select a core for transmission/reception of messages? (IN SRIO, I was able to distinguish the core number with the help of LSU registers)

 

Is there any sample/reference code available for the DSP-FPGA communication using LTE feature for AIF2?

 

Is there any sample/reference material (other than User guide and LLD) available for the same?

 

Also, please suggest what components of AIF2 are covered by loopback mode supported by AIF2? (For SRIO, we had Digital and SERDES loopback modes, but for AIF2, I read only internal loopback mode is available. So, wish to know how it maps to loopback modes available in SRIO?)

 

In anticipation of response for all/some of the above queries

Thanks

Regards

Anuj Agarwal

  • Hi,

    If you are thinking about using Generic packet mode, that means you are trying to transfer various size of packet with flexible packing and the data is not IQ data.

    I was confused why you want to transfer LTE 1.4 MHz type of IQ data, even though you want to use Generic packet mode.

    Generic packet mode is very flexible and use the whole link BW flexibly for whatever the packet size is. packet is only differentiate by SOP and EOP signal which is created by delimiter. we have 4b5b encoding and NULL delimiter for that purpose.

    I attached an example of CPRI generic packet mode. LLD also has this. AIF2 LLD also has this code 

    /****************************************************************************\
     *           Copyright (C) 2009 Texas Instruments Incorporated.             *
     *                           All Rights Reserved                            *
     *                                                                          *
     * GENERAL DISCLAIMER                                                       *
     * -------------------------------------------------------------------      *
     * All software and related documentation is provided "AS IS" and without   *
     * warranty or support of any kind and Texas Instruments expressly disclaims*
     * all other warranties, express or implied, including, but not limited to, *
     * the implied warranties of merchantability and fitness for a particular   *
     * purpose.  Under no circumstances shall Texas Instruments be liable for   *
     * any incidental, special or consequential damages that result from the    *
     * use or inability to use the software or related documentation, even if   *
     * Texas Instruments has been advised of the liability.                     *
     ****************************************************************************
     *                                                                          *
     * Written by :                                                             *
     *            Albert Bae                                                    *
     *            Texas Instruments                                             *
     *            15 Nov, 2010                                                 *
     *                                                                          *
     ***************************************************************************/
    #include <stdio.h>
    #include <stdlib.h>
    #include <string.h>
    #include <c6x.h>
    #include <ti/csl/src/intc/csl_intc.h>
    
    #include "Aif2_config.h"
    #include "psc_util.h"
    
    /* Define queues for common FDQs */
    #define HOST_TX_COMPLETE_Q     2000
    #define HOST_RX_FDQ            2001
    
    /* These are for the AIF test */
    #define HOST_RX_Q              900
    #define HOST_TX_Q              512
    
    //Users should use 16 bytes aligned data for Aif2 and pkt dma test
    #pragma DATA_ALIGN (host_region, 16)
    Uint8   host_region[64 * 32];//32 64 byte descriptors
    #pragma DATA_ALIGN (buffers, 16)
    Uint8   buffers[32 * 256];
    Uint32  tmp0[8], tmp1[8];
    
    /* Intc variable declarartion */
    CSL_IntcObj    intcObj;
    CSL_IntcHandle   hIntc;
    CSL_IntcEventHandlerRecord  EventHandler[8];
    CSL_IntcGlobalEnableState state;
    
    /* Global structures and variables  */
    CSL_Aif2Obj Aif2Obj;// Aif2 CSL object
    CSL_Aif2Handle hAif2;// Aif2 handle 
    Bool ctrlArg; // Ctrl Argument;
    
    CSL_Aif2Context Aif2Context;//Aif2 context
    CSL_Aif2Param  aif2Param;//AIF2 module specific parameters
    CSL_Status status; // CSL status
       
    CSL_Aif2Setup               aif2Setup;//Aif2 HW setup
    CSL_Aif2LinkSetup           linkSetup;// Setup for links 
    CSL_Aif2GlobalSetup         globalSetup;// global config for AIF2 
    CSL_Aif2CommonSetup         commonSetup; // Setup for common params
       
    CSL_Aif2SdCommonSetup       SdCommonSetup;//SERDES common setup
    CSL_Aif2PdCommonSetup       PdCommonSetup;//PD common setup
    CSL_Aif2PeCommonSetup       PeCommonSetup;//PE common setup
    CSL_Aif2IngrDbSetup         IngrDbSetup;// Ingress data buffer setup 
    CSL_Aif2EgrDbSetup          EgrDbSetup;// Egress data buffer setup 
    CSL_Aif2AdCommonSetup       AdCommonSetup;// Aif2 DMA common setup 
    CSL_Aif2AtCommonSetup       AtCommonSetup; // Aif2 Timer common  setup 
    CSL_Aif2AtEventSetup        AtEventSetup; // Aif2 Timer external and internal event  setup 
    CSL_Aif2AtCountObj          PhyTimerTc;// AT Phy Terminal Count setup
    CSL_Aif2AtCountObj          RadTimerTc;// AT Rad Terminal Count setup
    CSL_Aif2AtCountObj          PhyTimerInit;// AT Phy Init value setup
    CSL_Aif2AtCountObj          RadTimerInit;// AT Rad Init value setup
       
    CSL_Aif2CommonLinkSetup     ComLinkSetup; // Aif2 link common setup 
    CSL_Aif2SdLinkSetup         SdLinkSetup; //SERDES link setup
    CSL_Aif2RmLinkSetup         RmLinkSetup; //RM link setup
    CSL_Aif2TmLinkSetup         TmLinkSetup; //TM link setup
    CSL_Aif2PdLinkSetup         PdLinkSetup; //PD link setup
    CSL_Aif2PeLinkSetup         PeLinkSetup; //PE link setup
    CSL_Aif2RtLinkSetup         RtLinkSetup; //RT link setup
    CSL_Aif2AtLinkSetup         AtLinkSetup; // Aif2 timer link setup (Pi, Delta, PE signal) 
    
    volatile unsigned int int4_result;
    
    interrupt void int4_isr(){
        int i;
        if(int4_result == 1){
          for(i=0;i<8;i++)push_queue(HOST_TX_Q, 1, 0, tmp0[i]);	
        }
        int4_result++;
    
    }
    
    void Intc_config(void)
    {
       CSL_IntcParam    vectId;
       CSL_IntcContext  context;
       //!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!//
       //! GEM0 Intc Configuration              !//
       //!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!//
       /* Setup the global Interrupt */
       context.numEvtEntries = 8;    
       context.eventhandlerRecord = EventHandler; 
       CSL_intcInit(&context);
       /* Enable NMIs  */
       CSL_intcGlobalNmiEnable();
       /* Enable Global Interrupts  */
       CSL_intcGlobalEnable(&state);
       
       /* VectorID for the Global Edma Event  */
       vectId = CSL_INTC_VECTID_4;
       
       /* Opening a handle for the Fsync->EDMA Interrupt Event */                                      
       hIntc   = CSL_intcOpen(&intcObj,
                               AIF2_EVENT7_INTSEL_MAP, // Event 7
                               &vectId,
                               NULL);
       //Hook the ISRs
       CSL_intcHookIsr(vectId,  &int4_isr);
       // Clear the Interrupt    
       CSL_intcHwControl(hIntc, CSL_INTC_CMD_EVTCLEAR,  NULL);
       //Enable the Event & the interrupt 
       CSL_intcHwControl(hIntc, CSL_INTC_CMD_EVTENABLE,  NULL);
     
    }
    
    void MNavigator_config(void)
    {
        Uint32  flow_a, flow_d, flow_e;
        Uint16  idx;
        MNAV_HostPacketDescriptor *host_pkt;
    
       /* Setup Memory Region 0 for 32 * 64B host descriptors. Our
        * host descriptors will be 64 bytes and it is dividable by 16  */
    
       set_memory_region(0, (Uint32) host_region, 0, 0x00030000);
    
       /*****************************************************************
        * Configure Linking RAM 0 for the descriptor regions.
        */
       set_link_ram(0, QM_LRAM_REGION, 0x3fff); //internal link ram
    
       /* Initialize descriptor regions and buffers */
       memset(host_region, 0, 64 * 32);
       memset(buffers, 0xFF, 256 * 32);
    
        /* Push Host Descriptors to Tx Completion Queue */
        for (idx = 0; idx < 16; idx ++)
        {
          host_pkt = (MNAV_HostPacketDescriptor *)(host_region + (idx * 64));
          host_pkt->type_id = MNAV_DESC_TYPE_HOST;
          host_pkt->pkt_return_qmgr = 0;
          host_pkt->pkt_return_qnum = HOST_TX_COMPLETE_Q;
          host_pkt->return_policy = 1;
          host_pkt->orig_buff0_len = 256;
          host_pkt->orig_buff0_ptr = (Uint32)(buffers + (idx * 256));
          host_pkt->buffer_len = 0;
          host_pkt->buffer_ptr = host_pkt->orig_buff0_ptr;
          host_pkt->next_desc_ptr = NULL;
    
          push_queue(HOST_TX_COMPLETE_Q, 1, 0, (Uint32)(host_pkt));
        }
    
        /* Push Host Descriptors to Rx FDQ */
        for (idx = 16; idx < 32; idx ++)
        {
          host_pkt = (MNAV_HostPacketDescriptor *)(host_region + (idx * 64));
          host_pkt->type_id = MNAV_DESC_TYPE_HOST;
    
          /* Set non-Rx overwrite fields */
          host_pkt->orig_buff0_len = 256;
          host_pkt->orig_buff0_ptr = (Uint32)(buffers + (idx * 256));
          host_pkt->next_desc_ptr = NULL; //don't link Host buffers in Rx FDQ
    
          push_queue(HOST_RX_FDQ, 1, 0, (Uint32)(host_pkt));
        }
    
       /*****************************************************************
        * Configure Rx channel flows
        */
        //Create flow configuration 0 for the Monolithic packets
        flow_a = 0x02000000 | HOST_RX_Q;
        flow_d = (HOST_RX_FDQ << 16) + HOST_RX_FDQ;
        flow_e = flow_d;
        config_rx_flow(AIF_PKTDMA_RX_FLOW_REGION, 0,
                       flow_a, 0, 0, flow_d, flow_e, 0, 0, 0);
    
       /*****************************************************************
        * Enable Tx and Rx channels.
        */
        enable_disable_loopback(0);//disable PktDMA loopback for normal data transfer
        enable_tx_chan(AIF_PKTDMA_TX_CHAN_REGION, 0, 0x80000000);//channel 0
        enable_rx_chan(AIF_PKTDMA_RX_CHAN_REGION, 0, 0x80000000);//channel 0
    }
    
    void Aif2_MNAV_Cpri_config(void)
    {
       int i;
       /************ Initialize Aif2 structures to avoid unwanted configuration ************************************************/ 
       memset(&globalSetup, 0, sizeof(globalSetup));
       memset(&linkSetup, 0, sizeof(linkSetup));
       memset(&commonSetup, 0, sizeof(commonSetup));
       
       memset(&SdCommonSetup, 0, sizeof(SdCommonSetup));
       memset(&PdCommonSetup, 0, sizeof(PdCommonSetup));
       memset(&PeCommonSetup, 0, sizeof(PeCommonSetup));
       memset(&IngrDbSetup, 0, sizeof(IngrDbSetup));
       memset(&EgrDbSetup, 0, sizeof(EgrDbSetup));
       memset(&AdCommonSetup, 0, sizeof(AdCommonSetup));
       memset(&AtCommonSetup, 0, sizeof(AtCommonSetup));
       memset(&AtEventSetup, 0, sizeof(AtEventSetup));
       memset(&PhyTimerInit, 0, sizeof(PhyTimerInit));
       memset(&RadTimerInit, 0, sizeof(RadTimerInit));
       memset(&PhyTimerTc, 0, sizeof(PhyTimerTc));
       memset(&RadTimerTc, 0, sizeof(RadTimerTc));
       
       memset(&ComLinkSetup, 0, sizeof(ComLinkSetup));
       memset(&SdLinkSetup, 0, sizeof(SdLinkSetup));
       memset(&RmLinkSetup, 0, sizeof(RmLinkSetup));
       memset(&TmLinkSetup, 0, sizeof(TmLinkSetup));
       memset(&PdLinkSetup, 0, sizeof(PdLinkSetup));
       memset(&PeLinkSetup, 0, sizeof(PeLinkSetup));
       memset(&RtLinkSetup, 0, sizeof(RtLinkSetup));
       memset(&AtLinkSetup, 0, sizeof(AtLinkSetup));
        
       // Initialize CSL library, this step is required 
       CSL_aif2Init(&Aif2Context);
       
       // Open Aif2 and get handle 
       hAif2 = CSL_aif2Open(&Aif2Obj, CSL_AIF, &aif2Param, &status);
    
       if ((hAif2 == NULL) || (status != CSL_SOK)) 
       {
          printf ("\nError opening CSL_AIF2");
          exit(1);
       }
       
       /************** populating AIF2 major setup structures ***************************************************/
       aif2Setup.globalSetup = &globalSetup;
       aif2Setup.commonSetup = &commonSetup;
       aif2Setup.linkSetup[CSL_AIF2_LINK_0] = &linkSetup;//assign only one link setup for link 0
     
       // populate global config fields
       globalSetup.ActiveLink[CSL_AIF2_LINK_0] = TRUE;//Activate link 0 for this test
       globalSetup.frameMode = CSL_AIF2_FRAME_MODE_NORMAL; 
      
       //populate common config fields
       commonSetup.pSdCommonSetup = &SdCommonSetup;
       commonSetup.pPdCommonSetup = &PdCommonSetup;
       commonSetup.pPeCommonSetup = &PeCommonSetup;
       commonSetup.pIngrDbSetup   = &IngrDbSetup;
       commonSetup.pEgrDbSetup    = &EgrDbSetup;
       commonSetup.pAdCommonSetup = &AdCommonSetup;
       commonSetup.pAtCommonSetup = &AtCommonSetup;
       commonSetup.pAtEventSetup  = &AtEventSetup; 
       
       /****Link Setup (Do this setup repeatedly with different link setup structure if user wants to use multiple links) ***/
       //populate link config fields for link 0
       linkSetup.linkIndex     = CSL_AIF2_LINK_0; 
       linkSetup.pComLinkSetup = &ComLinkSetup;
       linkSetup.pSdLinkSetup  = &SdLinkSetup;
       linkSetup.pRmLinkSetup  = &RmLinkSetup;
       linkSetup.pTmLinkSetup  = &TmLinkSetup;
       linkSetup.pPdLinkSetup  = &PdLinkSetup;
       linkSetup.pPeLinkSetup  = &PeLinkSetup;
       linkSetup.pRtLinkSetup  = &RtLinkSetup;
       linkSetup.pAtLinkSetup  = &AtLinkSetup;
       
       //Link Common setup
       ComLinkSetup.linkProtocol = CSL_AIF2_LINK_PROTOCOL_CPRI;
       ComLinkSetup.linkRate = CSL_AIF2_LINK_RATE_4x;
       ComLinkSetup.IngrDataWidth = CSL_AIF2_DATA_WIDTH_15_BIT;
       ComLinkSetup.EgrDataWidth = CSL_AIF2_DATA_WIDTH_15_BIT;
       
       //SD link setup
       SdLinkSetup.rxAlign = CSL_AIF2_SD_RX_COMMA_ALIGNMENT_ENABLE;
       SdLinkSetup.rxLos = CSL_AIF2_SD_RX_LOS_ENABLE;
       SdLinkSetup.rxCdrAlgorithm = CSL_AIF2_SD_RX_CDR_FIRST_ORDER_THRESH_17;
       SdLinkSetup.rxInvertPolarity = CSL_AIF2_SD_RX_NORMAL_POLARITY;
       SdLinkSetup.rxTermination = CSL_AIF2_SD_RX_TERM_COMMON_POINT_0_7 ;//for AC coupled application
       SdLinkSetup.rxEqualizerConfig = CSL_AIF2_SD_RX_EQ_ADAPTIVE;//Equalizer On
       SdLinkSetup.bRxEqHold = FALSE;//fixed value
       SdLinkSetup.bRxOffsetComp = TRUE;//fixed value
       SdLinkSetup.bEnableTxSyncMater = TRUE; //fixed value
       SdLinkSetup.txInvertPolarity = CSL_AIF2_SD_TX_PAIR_NORMAL_POLARITY;
       SdLinkSetup.txOutputSwing = CSL_AIF2_SD_TX_OUTPUT_SWING_14;
       SdLinkSetup.txPrecursorTapWeight = CSL_AIF2_SD_TX_PRE_TAP_WEIGHT_2;// -5%
       SdLinkSetup.txPostcursorTapWeight = CSL_AIF2_SD_TX_POST_TAP_WEIGHT_24;// -20%
       SdLinkSetup.bTxFirFilterUpdate = TRUE;//FIR filter update on
       
       //TM link setup
       TmLinkSetup.bEnableTmLink = TRUE;
       TmLinkSetup.bEnableRmLos = FALSE;
       TmLinkSetup.SeedValue = 0x1;
       TmLinkSetup.bEnableScrambler = FALSE;
       TmLinkSetup.pCpriTmSetup.L1InbandEn = 0;//disable 9 bits mask
       TmLinkSetup.pCpriTmSetup.RmLinkLosError = CSL_AIF2_LINK_0;//select link 0 as source RM link
       TmLinkSetup.pCpriTmSetup.RmLinkLofError = CSL_AIF2_LINK_0;//select link 0 as source RM link
       TmLinkSetup.pCpriTmSetup.RmLinkLosRx = CSL_AIF2_LINK_0;//select link 0 as source RM link
       TmLinkSetup.pCpriTmSetup.RmLinkLofRx = CSL_AIF2_LINK_0;//select link 0 as source RM link
       TmLinkSetup.pCpriTmSetup.RmLinkRaiRx = CSL_AIF2_LINK_0;//select link 0 as source RM link
       TmLinkSetup.pCpriTmSetup.TxStartup = 0;
       TmLinkSetup.pCpriTmSetup.TxPointerP = 20;
       TmLinkSetup.pCpriTmSetup.TxProtocolVer = 1;
       
       //RM link setup
       RmLinkSetup.bEnableRmLink = TRUE;
       RmLinkSetup.RmFifoThold = CSL_AIF2_RM_FIFO_THOLD_IMMEDIATELY;
       RmLinkSetup.RmErrorSuppress = CSL_AIF2_RM_ERROR_ALLOW;
       RmLinkSetup.bEnableSdAutoAlign = FALSE;
       RmLinkSetup.bEnableScrambler = FALSE;
       RmLinkSetup.bEnableLcvUnsync = FALSE;
       RmLinkSetup.bEnableLcvControl = FALSE;
       RmLinkSetup.bEnableWatchDog = FALSE;
       RmLinkSetup.WatchDogWrap = 0xFF;//set watch dog wrap value
       RmLinkSetup.bEnableClockQuality = FALSE;
       RmLinkSetup.ClockMonitorWrap = 0;
       RmLinkSetup.losDetThreshold = RM_LOS_DET_THOLD;
       RmLinkSetup.SyncThreshold = RM_SYNC_THOLD;
       RmLinkSetup.FrameSyncThreshold = RM_SYNC_THOLD;
       RmLinkSetup.UnsyncThreshold = RM_UNSYNC_THOLD;
       RmLinkSetup.FrameUnsyncThreshold = RM_UNSYNC_THOLD;
       
       //RT link setup
       RtLinkSetup.CiSelect =  CSL_AIF2_LINK_0;
       RtLinkSetup.bEnableEmptyMsg = TRUE;
       RtLinkSetup.RtConfig = CSL_AIF2_RT_MODE_TRANSMIT;// takes PE input only
       
       //PD link setup
       PdLinkSetup.bEnablePdLink = TRUE;
       PdLinkSetup.CpriEnetStrip = 0;//disable ethernet strip for control channel
       PdLinkSetup.Crc8Poly = CRC8_POLY;
       PdLinkSetup.Crc8Seed = CRC8_SEED;
       PdLinkSetup.CpriCwNullDelimitor = 0xFB;//K 27.7 charactor
       PdLinkSetup.CpriCwPktDelimitor[0] = CSL_AIF2_CW_DELIM_4B5B;
       PdLinkSetup.PdCpriCrcType[0] = CSL_AIF2_CRC_16BIT;
       PdLinkSetup.bEnableCpriCrc[0] = FALSE;//enable CPRI CRC for control channel 0
       PdLinkSetup.PdPackDmaCh[0] = 0;//Set DB channel 0 as a dma ch for control channel 0   
       PdLinkSetup.bEnablePack[0] = TRUE;//enable CPRI control channel 0 packing
       
       PdLinkSetup.PdCpriDualBitMap.DbmX = 0;// set X-1
       PdLinkSetup.PdCpriDualBitMap.DbmXBubble = 0;//2 bubbles of 1 AxC sample
       PdLinkSetup.PdCpriDualBitMap.Dbm1Mult = 0;//set n-1
       PdLinkSetup.PdCpriDualBitMap.Dbm1Size = 0;//set n-1
       PdLinkSetup.PdCpriDualBitMap.Dbm1Map[0] = 0x0;
       PdLinkSetup.PdCpriDualBitMap.Dbm2Size = 0;
       PdLinkSetup.PdCpriDualBitMap.Dbm2Map[0] = 0x0;
       PdLinkSetup.CpriDmaCh[0]= 0; //match DbmX channel 0 to DB channel 0 
       PdLinkSetup.bEnableCpriX[0]= TRUE; //enable CPRI X channel 0
       PdLinkSetup.bEnableCpriPkt[0]= TRUE;//use Pkt data for X channel 0
       PdLinkSetup.Cpri8WordOffset[0]= 0;//Word level CPRI data offset for X channel 0
       
       //PE link setup
       PeLinkSetup.bEnablePeLink = TRUE;
       PeLinkSetup.PeCppiDioSel = CSL_AIF2_CPPI;
       PeLinkSetup.TddAxc = FALSE;
       PeLinkSetup.PeDelay = DB_PE_DELAY_CPRI;//0 sys_clks delay between DB and PE
       PeLinkSetup.Crc8Poly = CRC8_POLY;
       PeLinkSetup.Crc8Seed = CRC8_SEED;
       PeLinkSetup.PeCpriDualBitMap.DbmX = 0;//set X-1
       PeLinkSetup.PeCpriDualBitMap.DbmXBubble = 0;//2 bubbles of 1 AxC sample
       PeLinkSetup.PeCpriDualBitMap.Dbm1Mult = 0;//set n-1
       PeLinkSetup.PeCpriDualBitMap.Dbm1Size = 0;//set n-1
       PeLinkSetup.PeCpriDualBitMap.Dbm1Map[0] = 0x0;
       PeLinkSetup.PeCpriDualBitMap.Dbm2Size = 0;
       PeLinkSetup.PeCpriDualBitMap.Dbm2Map[0] = 0x0;
       PeLinkSetup.CpriAxCPack = CSL_AIF2_CPRI_15BIT_SAMPLE;
       PeLinkSetup.CpriCwNullDelimitor = 0xFB;//K 27.7 character
       PeLinkSetup.CpriCwPktDelimitor[0] = CSL_AIF2_CW_DELIM_4B5B;
       PeLinkSetup.PePackDmaCh[0] = 0;//match DB channel 0 to control channel 0
       PeLinkSetup.bEnablePack[0] = TRUE;
       
       //AT link setup
       AtLinkSetup.PE1Offset = 300;
       AtLinkSetup.PE2Offset = 310;
       AtLinkSetup.DeltaOffset = 370;// Packet DMA delay + pe1 + pe2 = 300 + 10 + 60 (min Delta)
       AtLinkSetup.PiMin = 370;
       AtLinkSetup.PiMax = 390;
       AtLinkSetup.IsNegativeDelta = FALSE;//positive delta
       
       /************** Common Setup ********************************************************************************/
       //SD common setup
       SdCommonSetup.bEnablePllB8 = TRUE;
       SdCommonSetup.CLKBYP_B8 = CSL_AIF2_PLL_CLOCK_NO_BYPASS;
       SdCommonSetup.LB_B8 = CSL_AIF2_PLL_LOOP_BAND_MID;//High BW is also fine
       SdCommonSetup.VoltRangeB8 = CSL_AIF2_PLL_VOLTAGE_LOW;//fixed factor
       SdCommonSetup.SleepPllB8 = CSL_AIF2_PLL_AWAKE;
       SdCommonSetup.pllMpyFactorB8 = CSL_AIF2_PLL_MUL_FACTOR_20X;//for CPRI when reference clock is 122.88 Mhz
       SdCommonSetup.SysClockSelect = CSL_AIF2_SD_BYTECLOCK_FROM_B8;
       SdCommonSetup.DisableLinkClock[0] = FALSE;//enable link0 clock
       
       //PD common setup
       PdCommonSetup.PdCppiDioSel = CSL_AIF2_CPPI;//AxC data uses CPPI for DMA machine
       PdCommonSetup.PdChConfig[0].bChannelEn = TRUE;//Channel enable for channel 0
       PdCommonSetup.PdChConfig[0].DataFormat = CSL_AIF2_LINK_DATA_TYPE_NORMAL;//Data format for channel 0
       PdCommonSetup.PdChConfig1[0].DataFormat = CSL_AIF2_GSM_DATA_OTHER;//Non GSM data
       PdCommonSetup.PdChConfig1[0].TddEnable = 0xFFFF;//PD TDD, enables all symbols(FDD) for channel 0 
       PdCommonSetup.TddEnable1[0] = 0xFFFFFFFF;//enables all symbols(FDD)
       PdCommonSetup.TddEnable2[0] = 0xFFFFFFFF;//enables all symbols(FDD)
       PdCommonSetup.TddEnable3[0] = 0xFFFFFFFF;//enables all symbols(FDD)
       PdCommonSetup.TddEnable4[0] = 0xFFFFFFFF;//enables all symbols(FDD)
       
       //PE common setup
       PeCommonSetup.PeTokenPhase = 0;
       PeCommonSetup.EnetHeaderSelect = 0;//bit order for Ethernet preamble and SOF 
       
       PeCommonSetup.bEnableCh[0] = TRUE;//Enable PE channel for channel 0
       PeCommonSetup.PeDmaCh0[0].bCrcEn = FALSE;//disable CRC for channel 0
       PeCommonSetup.PeDmaCh0[0].RtControl = CSL_AIF2_PE_RT_INSERT;//use PE insert option for channel 0
       PeCommonSetup.PeDmaCh0[0].CrcType = CSL_AIF2_CRC_16BIT;//CRC type for channel 0
       PeCommonSetup.PeDmaCh0[0].isEthernet = FALSE;//AxC data 
       PeCommonSetup.PeDmaCh0[0].CrcObsaiHeader = FALSE;//calculate OBSAI header CRC
       PeCommonSetup.PeInFifo[0].SyncSymbol = 0;//sync symbol offset for channel 0
       PeCommonSetup.PeInFifo[0].MFifoWmark = 2;//Message FIFO water mark for channel 0
       PeCommonSetup.PeInFifo[0].MFifoFullLevel = 3;//Message FIFO full level for channel 0
       
       PeCommonSetup.ChIndex0[0] = 0; //channel 0
       PeCommonSetup.bEnableChIndex0[0] = TRUE;//Route egress channel 0 to CPRI link 0
       PeCommonSetup.CpriPktEn0[0] = TRUE; //use channel 0 for Pkt
    
       //Ingress DB setup
       IngrDbSetup.bEnableIngrDb = TRUE; //Enable Ingress DB
       IngrDbSetup.bEnableChannel[0] = TRUE; //Enable Ingress DB channel 0
       IngrDbSetup.IngrDbChannel[0].BaseAddress = AIF2_DB_BASE_ADDR_I_FIFO_0; //Set DB FIFO base address for channel 0
       IngrDbSetup.IngrDbChannel[0].BufDepth = CSL_AIF2_DB_FIFO_DEPTH_QW128; //Set DB FIFO depth for channel 0 
       IngrDbSetup.IngrDbChannel[0].DataSwap = CSL_AIF2_DB_WORD_SWAP; //DL
       IngrDbSetup.IngrDbChannel[0].IQOrder = CSL_AIF2_DB_IQ_NO_SWAP; //No Order change
       IngrDbSetup.IngrDbChannel[0].bEnablePsData = FALSE; //Enable 4 bytes PS data
       IngrDbSetup.IngrDbChannel[0].PacketType = 0; //User data
       
       //Egress DB setup
       EgrDbSetup.bEnableEgrDb = TRUE; //Enable Ingress DB
       EgrDbSetup.PmControl = CSL_AIF2_DB_AXC_TOKEN_FIFO;//to enhance CPRI packet performance
       EgrDbSetup.bEnableChannel[0] = TRUE; //Enable Egress DB channel 0
       EgrDbSetup.EgrDbChannel[0].BaseAddress = AIF2_DB_BASE_ADDR_E_FIFO_0; //Set DB FIFO base address for channel 0
       EgrDbSetup.EgrDbChannel[0].BufDepth = CSL_AIF2_DB_FIFO_DEPTH_QW128; //Set DB FIFO depth for channel 0
       EgrDbSetup.EgrDbChannel[0].DataSwap = CSL_AIF2_DB_WORD_SWAP; //DL
       EgrDbSetup.EgrDbChannel[0].IQOrder = CSL_AIF2_DB_IQ_NO_SWAP; //No Order change
       
       //AD Common setup
       AdCommonSetup.IngrGlobalEnable = TRUE;
       AdCommonSetup.EgrGlobalEnable = TRUE;
       AdCommonSetup.FailMode = CSL_AIF2_AD_DROP;//drop fail packet
       AdCommonSetup.IngrPriority = CSL_AIF2_AD_PKT_PRI;
       AdCommonSetup.EgrPriority = CSL_AIF2_AD_NON_AXC_PRI;
       AdCommonSetup.Tx_QueNum = AIF2_BASE_TX_QUE_NUM;//base egress queue number setup to 512
       
       //AT Common setup
       AtCommonSetup.PhySyncSel = CSL_AIF2_SW_SYNC;//Select SW sync for Phy timer trigger
       AtCommonSetup.RadSyncSel = CSL_AIF2_SW_SYNC;//Select SW sync for Rad timer trigger
       AtCommonSetup.SyncMode = CSL_AIF2_NON_RP1_MODE;
       AtCommonSetup.AutoResyncMode = CSL_AIF2_AUTO_RESYNC_MODE;
       AtCommonSetup.CrcMode = CSL_AIF2_AT_CRC_DONT_USE;//Do not use RP1 CRC in this test
       AtCommonSetup.PhytCompValue = 0;
       
       AtCommonSetup.AtInit.pPhyTimerInit = &PhyTimerInit;
       AtCommonSetup.AtInit.pRadTimerInit = &RadTimerInit;
       PhyTimerInit.ClockNum = 0;
       PhyTimerInit.FrameLsbNum = 0;
       PhyTimerInit.FrameMsbNum = 0;
       RadTimerInit.ClockNum = 0;
       RadTimerInit.SymbolNum = 0;
       RadTimerInit.FrameLsbNum = 0;
       RadTimerInit.FrameMsbNum = 0;
       AtCommonSetup.AtTerminalCount.pPhyTimerTc = &PhyTimerTc;
       AtCommonSetup.AtTerminalCount.pRadTimerTc = &RadTimerTc;
       PhyTimerTc.FrameLsbNum = FRAME_COUNT_TC_PHY_TIMER;//set phy Frame TC to 4095
       PhyTimerTc.ClockNum = CLOCK_COUNT_TC_PHY_TIMER_CPRI; //set phy clock TC for CPRI
       RadTimerTc.FrameLsbNum = FRAME_COUNT_TC_LTE_FDD;//set Frame TC to 4095
       RadTimerTc.SymbolNum = SYMBOL_COUNT_TC_LTE_FDD; //set Symbol TC to 9
       RadTimerTc.LutIndexNum = 0; //set LutIndex TC to 0
       AtCommonSetup.AtTerminalCount.RadClockCountTc[0] = CLOCK_COUNT_TC_LTE_FDD_CPRI;//set Clock count TC for CPRI
      
       //AT Event setup (Event 7)
       AtEventSetup.AtRadEvent[7].EventSelect = CSL_AIF2_EVENT_7;//Select Event 7 
       AtEventSetup.AtRadEvent[7].EventOffset = 400; 
       AtEventSetup.AtRadEvent[7].EvtStrobeSel = CSL_AIF2_RADT_FRAME; 
       AtEventSetup.AtRadEvent[7].EventModulo = 2457599; 
       AtEventSetup.AtRadEvent[7].EventMaskLsb = 0xFFFFFFFF; 
       AtEventSetup.AtRadEvent[7].EventMaskMsb = 0xFFFFFFFF; 
       AtEventSetup.bEnableRadEvent[7] = TRUE;//Enable Event 7
       
       /****** Do AIF2 HW setup (set all MMRs above) **********************************************************************/
       CSL_aif2HwSetup(hAif2, &aif2Setup);
    
       ctrlArg = TRUE;
       hAif2->arg_link = CSL_AIF2_LINK_0;//Select link num
       
       //Enable Serdes loopback for link 0
       CSL_aif2HwControl(hAif2, CSL_AIF2_CMD_ENABLE_DISABLE_LINK_LOOPBACK, (void *)&ctrlArg);
       //Enable Tx/Rx of link 0
       CSL_aif2HwControl(hAif2, CSL_AIF2_CMD_ENABLE_DISABLE_TX_LINK, (void *)&ctrlArg);
       CSL_aif2HwControl(hAif2, CSL_AIF2_CMD_ENABLE_DISABLE_RX_LINK, (void *)&ctrlArg);
       for(i=0;i<100;i++)asm (" NOP 9 ");//insert time delay for aif2 configuration completion 
       
       //AT Arm timer
       CSL_aif2HwControl(hAif2, CSL_AIF2_CMD_AT_ARM_TIMER, (void *)&ctrlArg);
       
       //Trigger the SW debug frame sync
       CSL_aif2HwControl(hAif2, CSL_AIF2_CMD_AT_DEBUG_SYNC, (void *)&ctrlArg);
    
    }
    
    void main(void)
    {
        Uint32  hostRxCount;
        Uint16  testpass;
        Uint32 *temp;
        Uint32  idx, idx2, rx_count, value;
        MNAV_HostPacketDescriptor *host_pkt;
       
        printf("Beginning AIF2 CPRI Generic packet  test:\n\n");
        for(idx=0;idx<1000;idx++)asm (" NOP 9 ");//delay for printf not to block ISR execution
    
        enable_module(aif_pdctl, aif_mdctl);//Enable AIF2 module power
    
        int4_result = 0;
        
        Intc_config();
        
        MNavigator_config();//multicore navigator configuration for LTE
        
        for(idx =0; idx < 8; idx++){  //push 8 host linked packets into Tx queue for test
    
        //Create Host packet Tx descriptor #2 with 2 linked Host Buf desc.
        tmp0[idx] = pop_queue(HOST_TX_COMPLETE_Q);
        tmp0[idx] &= 0xFFFFFFF0;//set DESC_SIZE field to zero
        tmp1[idx] = pop_queue(HOST_TX_COMPLETE_Q);
        tmp1[idx] &= 0xFFFFFFF0;//set DESC_SIZE field to zero
        
        host_pkt = (MNAV_HostPacketDescriptor *)tmp0[idx];
    
        host_pkt->ps_reg_loc = 1;
        host_pkt->return_policy = 1; 
        host_pkt->psv_word_count = 0;
        host_pkt->buffer_len = 256;
        host_pkt->packet_length = 256 * 2 ;
        host_pkt->next_desc_ptr = tmp1[idx];
        host_pkt->src_tag_lo = 0; //should be matched with Rx flow id
    
        temp = (Uint32 *)host_pkt->buffer_ptr;
        for (idx2 = 0; idx2 < 64; idx2 ++) temp[idx2] = idx2 + 0x10000;
    
        host_pkt = (MNAV_HostPacketDescriptor *)tmp1[idx];
        host_pkt->buffer_len = 256;
        host_pkt->next_desc_ptr = NULL;
    
        temp = (Uint32 *)host_pkt->buffer_ptr;
        for (idx2 = 0; idx2 < 64; idx2 ++) temp[idx2] = idx2 + 0x20000;
       
        tmp0[idx] |= 0x00000003;//set DESC_SIZE to 3 for 64 byte host descriptors
        tmp1[idx] |= 0x00000003;//set DESC_SIZE to 3 for 64 byte host descriptors
        //Tx decriptors will be pushed in ISR for this example
        }
        
        Aif2_MNAV_Cpri_config();//Aif2 configuration for M Navigator mode
    
         /*****************************************************************
        * Enable AIF2 and wait for completion.
        */
        while(1)
        {
            asm (" NOP 9 ");
            asm (" NOP 9 ");
            if(int4_result == 3)//Wait two phy frame time
            {
                //AT disable all events and halt timer
                ctrlArg = TRUE;
    	     CSL_aif2HwControl(hAif2, CSL_AIF2_CMD_AT_DISABLE_ALL_EVENTS, (void *)&ctrlArg);
                CSL_aif2HwControl(hAif2, CSL_AIF2_CMD_AT_HALT_TIMER, (void *)&ctrlArg);
    	     ctrlArg = FALSE;//disable AD scheduler and Rx, Tx Link
    	     CSL_aif2HwControl(hAif2, CSL_AIF2_CMD_AD_E_ENABLE_DISABLE_GLOBAL, (void *)&ctrlArg);
                CSL_aif2HwControl(hAif2, CSL_AIF2_CMD_AD_IN_ENABLE_DISABLE_GLOBAL, (void *)&ctrlArg);
    	     CSL_aif2HwControl(hAif2, CSL_AIF2_CMD_ENABLE_DISABLE_TX_LINK, (void *)&ctrlArg);
                CSL_aif2HwControl(hAif2, CSL_AIF2_CMD_ENABLE_DISABLE_RX_LINK, (void *)&ctrlArg);
                CSL_aif2Reset(hAif2);//reset all aif2 modules 
                break;
            }
        }
    
        hostRxCount = 0;  // descriptor count for host RX queue
        while (hostRxCount < 8)
        {
            // Get current descriptor count for host RX queue
            hostRxCount = get_descriptor_count(HOST_RX_Q);
            if (hostRxCount != 0)
            printf(" Number of monolithic packets received in RX queue: %d\n", hostRxCount);
        }
    
       /*****************************************************************
        * Compare the data in the destination buffers.
        */
    
        /* Compare the Monolithic packet data */
        testpass = 1;
        rx_count = get_descriptor_count(HOST_RX_Q);
    
        for (idx = 0; idx < rx_count; idx ++)
        {
          tmp0[idx] = pop_queue(HOST_RX_Q);
          host_pkt = (MNAV_HostPacketDescriptor *)tmp0[idx];
          temp = (Uint32 *)host_pkt->buffer_ptr;
          for (idx2 = 0; idx2 < 64; idx2 ++)if (temp[idx2] != (idx2 + 0x10000)) testpass = 0;
    	  
          tmp1[idx] = host_pkt->next_desc_ptr;
          host_pkt = (MNAV_HostPacketDescriptor *)tmp1[idx];
          temp = (Uint32 *)host_pkt->buffer_ptr;
          for (idx2 = 0; idx2 < 64; idx2 ++)if (temp[idx2] != (idx2 + 0x20000)) testpass = 0;
    	  
          push_queue(HOST_RX_FDQ, 1, 0, tmp0[idx]);
          push_queue(HOST_RX_FDQ, 1, 0, tmp1[idx]);
        }
    
        if (testpass == 1)
          printf(" Test a) Host Packet Data Send/Recv: PASS\n");
        else
          printf(" Test a) Host Packet Data Send/Recv: FAIL\n");
    
    
        /* read the descriptor counts of the Host queues. */
        value = get_descriptor_count(HOST_TX_Q);
        if (value != 0) printf(" Test b1) Host Packet Tx Descriptor Counts:%d FAIL\n",value);
        else printf(" Test b1) Host Packet Tx Descriptor Counts:%d PASS\n",value);
    
        value = get_descriptor_count(HOST_TX_COMPLETE_Q);
        if (value != 16) printf(" Test b2) Host Packet Tx Complete Descriptor Counts:%d FAIL\n",value);
        else printf(" Test b2) Host Packet Tx Complete Descriptor Counts:%d PASS\n",value);
    
        value = get_descriptor_count(HOST_RX_Q);
        if (value != 0) printf(" Test b3) Host Packet Rx Descriptor Counts:%d FAIL\n",value);
        else printf(" Test b3) Host Packet Rx Descriptor Counts:%d PASS\n",value);
        
        value = get_descriptor_count(HOST_RX_FDQ);
        if (value != 16) printf(" Test b4) Host Packet Rx Free Descriptor Counts:%d FAIL\n",value);
        else printf(" Test b4) Host Packet Rx Free Descriptor Counts:%d PASS\n",value);
    
        printf("\nEnding AIF2 CPRI Generic packet  test\n");
        
    }
    

     In case of AIF2, the loopback mode is supported by SERDES. AIF2 UG SERDES register map shows this loopback mode field. AIF2 core doesn't have its own digital internal loopback.

    Regards,

    Albert  

  • Hi

    Thanks a lot for your response. I got replies to all by above queries.

    Kindly answer the following queries as well:

    For DSP- FPGA interaction, I shall be using CPRI Generic mode with Packet DMA at 8x link rate for 1 link. 

    Through this link, I wish to READ and WRITE data on FPGA of varied length from DSP.

    Hence, DSP is Source and FPGA is destination for the READ and WRITE transactions.

     

    Though, I have been able to find how to  transfer various size of packet with flexible packing. But, now I wish to extend this send and receive of packets to READ and WRITE data from DSP on FPGA.

     

    Kindly suggest how I can do the same through AIF2.

     

    Regards

    Anuj Agarwal

  • AIF2 interface supports WRITE process and that means you can send packet from DSP to FPGA.

    but it doesn't support READ process which menas DSP send request to FPGA and FPGA respond with packet.

    AIF2 can only send request packet to FPGA and FPGA master should control this request to send back requested data. It totally depends on your application in DSP and FPGA.

    Regards,

    Albert 

  • Hi Albert

    Thanks a lot for your quick response.

    Also, can you please elaborate on the following statement: (How can we achieve the same)

    AIF2 can only send request packet to FPGA and FPGA master should control this request to send back requested data. It totally depends on your application in DSP and FPGA.


    To support READ (in addition to WRITE) operation, one might distinguish the request packet using a particular data and data size in the packet. Is the method correct?

    Or is there any other way/configuration/parameter through which I can distinguish the request packet from a normal WRITE transaction packet?


    Thanks a lot for the support

    Regards

    Anuj

  • To support READ (in addition to WRITE) operation, one might distinguish the request packet using a particular data and data size in the packet. Is the method correct?
     [Albert] yes, you need to have your own way to distinguish the packet. HW doesn't support that feature.

    Regards,

    Albert

     

  • Dear Albert

    Thanks a lot for your response and help.

    There is a change in my requirements. I now need to support continuous transfer (send and receive) of IQ data at 1.2 Mbps between corepac and FPGA (CPRI supported) through AIF2. 

    To elaborate further, I need to support the following:

    1) CPRI protocol on AIF2

    2) continuous data send and receive of IQ data at 1.2 Mbps

    3) Communication between DSP and FPGA through AIF2

    4) Each core preferably uses 1 AxC internally and all cores to use 1 physical link 

     

    Please let me know which mode would be best suited for the same.

    Thanks

     

    Regards

    Anuj Agarwal

  • Hi,

    What you are trying to do now is the normal use case of AIF2 with CPRI protocol.

    you can get more information from AIF2 UG and also see AIF2 CSL and LLD in your latest PDK or MCSDK SW package. (it has example code inside)

    and you need to choose which Radio standard (WCDMA, LTE) you will use for the AIF2. you can find something that matched with 1.2 Mbps data rate.

    Regards,

    Albert 

  • Dear Mr Albert

    Thanks a lot for your guidance.

    I am confused over using AIF2 in LTE mode because of following and similar statements I read at different places from which it is inferred that for inter device communication, generic packet is the only mode supported:

    1) AIF2 UG: AIF2 marks the LTE symbol with the received AIF2 channel number and the LTE symbol index (count value starting at 0 on the radio frame boundary). The packet is then transferred to FFTc; The whole transfer of the LTE symbol from AIF2 to L2 and finally to FFTc is performed with no interrupts of real time action by any of the CorePac cores. (packet exchanges between AIF2 and PA occur in much the same way).

    Inference: LTE mode is used for data transfer between radio head and co-processors.
    Question: Can LTE mode be used for data transfer between FPGA and DSP core and not radio head/ coprocessors?

     

    2) AIF2 LLD: The AIF2 has a special mode called generic packet for inter-device communication. It allows to used the AIF2 to transfer general digital packets betweens DSPs or between a DSP and a FPGA.

    Inference: Generic packet mode is used for inter-device communication.

    Question: Our use case is to send/receive IQ data between FPGA and DSP core which matches inter device communication mode. But data cannot be sent/received continuously in this mode. Hence, even though generic mode supports inter device communication, it is not best suitable for our use case as it doesnt transfer IQ data continuously? 

     

    3) AIF2 LLD: The AIF2 LLD works together with CPPI and QMSS LLDs to support the transport of LTE antenna samples between the radio equipment and the Keystone FFTC accelerators.

    Inference: In LTE mode, LTE antenna samples are transferred between radio equipment and FFTC accelators and not between FPGA and DSP core.

     

    Kindly guide if LTE mode can be used for 'Inter device communication : Send/receive IQ sample data between FPGA and DSP core on LTE sample rate (1.2 Mbps)'

     

    Thanks

  • Hi

    I am eagerly waiting for the response.

    Kindly suggest the replies to above queries.

     

    Regards

     

  • Hi,

    Your case looks special. you want to transfer original LTE5 AxC IQ steam continuously but you also want to transfer this data from your FPGA to the DSP core.

    From my thinking, you'd better use LTE AxC mode for this rather using generic packet mode, becasue generic mode has smaller BW and other limitation of transferring continuous IQ stream. in your case, you don't need to directly deliver the received IQ samples to FFTC but just store it on L2 or MSMC memory and DSP core can handle those data in run time. AIF2 fully support flexible DMA for your case. your FPGA can generate full CPRI frame with LTE5 MHz symbols and it will be delivered to DSP local memory by AIF2 DMA machine. you can use TI LLD CPPI and QMSS library to setup DMA for this transfer.

    Regards,

    Albert 

  • Dear Albert

    Thanks a lot for the information. Please guide on the below queries as well:

    1) As LTE AxC mode is also not the obvious mode for above mentioned requirements, can you also list the limitations of LTE mode for my use case?

    2) Please elaborate on how to transfer 'continuous' stream of IQ data in LTE mode?

    3) In multicore environment, data shall be received on 1 physical link for all cores. So how can a core be mapped in AIF2 so as to deliver the received packets on 1 link to specific cores?  e.g. In SRIO, we do it with the help of LSU registers and in ethernet, we do it with the help of PDSP and LUT.    So, how core mapping can be achieved in AIF2 and how the decision can be taken that a particular sample/packet is meant for specific core?

    4)  How are AxCs mapped? The numPeAxC (number of AxC on egress side) and numPdAxC (number of AxC on ingress side) are different variables in example code. Does this mean that AxC is not bidirectional? Is it feasible to use 4 AxC (1 per core) against 1 AxC (for all cores)? If yes, how would this mapping be done? And what would be the benefits?

    I am really thankful to you for your guidance and support.

    Thanks

  • here is the answer.

    1) Generic packet mode consumes additional BW by delimiter (4B5B encoding or NULL encoding) and generic mode doesn't support correct timing for LTE. you can generate some general event from AT but you can not guarantee that your LTE symbol receiving time is matched with that AT event timing. AxC mode always support correct symbol streaming timing for both PD,PE and AT and doesn't consume any unnecessary BW for LTE data transfer. AxC mode operation is exactly matched with what your Radio head digital part is doing and it is our original intention of designing AIF2

    2)It is in many of our TI documents and Radio spec. you may get useful information from AIF2 UG, MNavigator UG, CPRI spec 4.1 and LTE spec. Also study AIF2 LTE example code in our PDK or MCSDK (AIF2 LLD)

    3) AIF2 and SRIO is totally different interface. Most AIF2 packet data is AxC symbol and the destination is always monolithic descriptors in the memory (DDR, MSMC, L2). if you use L2 as a destination, specific core program can handle that. if you used DDR or MSMC as a destination, your application should know which core program need to handle which AxC symbol data and how it can be pushed in FFTC input queue. it cannot be handled by AIF2 HW

    4) this question doesn't make sense to me. please read other answers and think about this again. in real case, Egress is used for DL and Ingress is used for UL, so we don't; need to use symmetrical setup for both sides, but it can be symmetrical if user wants to test it with loopback mode.

    Regards,

    Albert

  • Hi,

    I also need to transfer the original IQ stream to DSP memory and process it from there.  Can you provide example code on how to do this?  I need to: (1) how to initiate transfer, (2) how to define destination starting and ending addresses in DSP memory, (3) how to reset starting address after reaching end, (4) get an interrupt after buffer is half full or full.

    Thanks,

    John