This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

bootargs for android am37x

Hi,

I'm referring to the Developers Guide for TI-Android-ICS:
(http://processors.wiki.ti.com/index.php/TI-Android-ICS-4.0.3-DevKit-3.0.0_DevelopersGuide).

On that page it says the bootargs for the beagleboard-xm should be:

setenv bootargs 'console=ttyO2,115200n8 androidboot.console=ttyO2 mem=256M root=/dev/mmcblk0p2 rw rootfstype=ext4 rootdelay=1 init=/init
ip=off omap_vout.vid1_static_vrfb_alloc=y vram=8M omapfb.vram=0:8M omapdss.def_disp=dvi omapfb.mode=dvi:1024x768-16'

If the xm has 512MB RAM.  Why is mem=256M passed to the kernel?

My custom board will not boot unless I pass mem=256M.  But my board has also has 512M, like the xM.