Hi,
We're using the OMAP-L138 SOM with WinCE6.0 and DSPLINK. I've looked everywhere for example code compatible with DSPLINK that will help us get started with DSP capture of data from the on-board AIC3106 on the LogicPD EVM. Changes would need to be made in the OSD and possibly the BSP, but beyond that, I have no idea where to begin. I've found an example in Linux that writes gpp data to the codec, but it's not CE, and it doesn't read the codec. Could anyone please point me to some relevant code using CE?
Thanks much. D.M.