I have found and used the register settings spreadsheet here. I have a query over one of the default values though.
All the default values seem to match exactly those found in the Elpida DDR3 datasheet for the part shown on the Sitara Evaluation board with the exception of one field.
The value provided in the spreadsheet for tFAW is 40nS where the datasheet gives 30nS for 8 bit DRAM at 800MHz clock speed. Is there any reason for this discrepancy? The datasheet value for the Micron part I am using is also 30nS, should I also be using 40nS instead?