Hello,
I tried to create a CCS project for SysLink samples as described in the following link:
http://processors.wiki.ti.com/index.php/Creating_CCS_Project_for_SysLink_samples
I'm using CCS v5 under Linux with the following packages:
syslink_2_20_02_20
xdctools_3_24_06_63
ipc_1_24_02_27
bios_6_34_02_18
I receive the following error message when I try to rebuild the project after making the changes mentioned in above wiki page:
Cannot read property "base" from undefined MessageApp_common.cfg.xs /messageQ_DSP Configuration Validation XDCTools Configuration Marker
Cannot read property "base" from undefined MessageQ_ti81xx_dsp.cfg /messageQ_DSP Configuration Validation XDCTools Configuration Marker
Cannot read property "base" from undefined SysLinkSamples_common.cfg.xs /messageQ_DSP 91 C/C++ Problem
Cannot read property "base" from undefined SysLinkSamples_common.cfg.xs /messageQ_DSP Configuration Validation XDCTools Configuration Marker
I appreciate any advice regarding this problem.
Regards,
Mohammad