What revision of the SGX544 is used in OMAP5432 ES1 and ES2? I dont' see this in the TRM.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
What revision of the SGX544 is used in OMAP5432 ES1 and ES2? I dont' see this in the TRM.
Hi,
Can I use the same SGX drivers (user and kernel )for ES2.0 which I used for the ES1.0? or Is there any changes from SGX core revision 105 to 116 that I need to update to drivers too?
Thanks & Regards,
Vikas
I'm not a graphics expert, but I know that the GPU revision is specified in the underlying DDK build process. In other words, IMG's microcode is tailored to comprehend differences between the core revisions. I think it would certainly be recommended to get newer code! Furthermore ES1.0 is years old so you would be missing a lot of patches that were added since then by staying with the old code.
If it's a big deal to move to the proper code then you might give it a try and see how it goes, but if any issues pop up I don't expect you'll be able to find anyone to help you work through the issues!