Although we don't seem to have any example code for muxing in and out different audio channels and combining them, has anything like this been done on another DSP, or would someone have an idea about how to go about this from scratch?
-Reagan
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Although we don't seem to have any example code for muxing in and out different audio channels and combining them, has anything like this been done on another DSP, or would someone have an idea about how to go about this from scratch?
-Reagan
You might want to post to other DSP forum?
We've done a 6 in to 2 out mixer/switch on a 5000 dsp for an interior cabin communication system operating on voice signals, this is kind of a special case of a mixer.
A more generalized case is to define a N x C mixing matrix M, where N is number of inputs and C is number of output channels. Then at time k, given a [1 x N] input vector XIN of the N inputs, use the mixing matrix to create the [1 x C] vector of outputs, YOUT
YOUT(k) = XIN(k) * M
where * implies a matrix multiplication.
That's the general concept. For example to mix 4 inputs to a stereo output, with say the 3rd input channel muted on the LEFT, the mixing matrix would look like:
| 1 1 |
| 1 1 |
| 0 1 |
| 1 1 |
So the implementation in a general sense is a matrix multiply operation. (note the above example doesn't take in consideration scaling to prevent overflow)
-S