Other Parts Discussed in Thread: TVP5158
Hi all,
I am using DVRRDK3.0 with DM8168EVM. I have run a link_api_demo in the board,but it failed with error below. I don't know why happens this error. Please give me some help. Thanks a lot. The Error was :
root@dm816x:~# ./dvr_rdk_demo_link_api.out
0: SYSTEM: System Common Init in progress !!!
0: SYSTEM: IPC init in progress !!!
13: SYSTEM: Opening MsgQ Heap [IPC_MSGQ_MSG_HEAP] ...
14: SYSTEM: Creating MsgQ [HOST_MSGQ] ...
16: SYSTEM: Creating MsgQ [HOST_ACK_MSGQ] ...
17: SYSTEM: Opening MsgQ [DSP_MSGQ] ...
18: SYSTEM: Opening MsgQ [VIDEO-M3_MSGQ] ...
18: SYSTEM: Opening MsgQ [VPSS-M3_MSGQ] ...
19: SYSTEM: Notify register to [DSP] line 0, event 15 ...
20: SYSTEM: Notify register to [VIDEO-M3] line 0, event 15 ...
20: SYSTEM: Notify register to [VPSS-M3] line 0, event 15 ...
21: SYSTEM: IPC init DONE !!!
22: SYSTEM: Creating ListMP [HOST_IPC_OUT_24] in region 0 ...
24: SYSTEM: Creating ListMP [HOST_IPC_IN_24] in region 0 ...
26: SYSTEM: ListElem Shared Addr = 0x2b129080
27: SYSTEM: Creating ListMP [HOST_IPC_OUT_25] in region 0 ...
29: SYSTEM: Creating ListMP [HOST_IPC_IN_25] in region 0 ...
31: SYSTEM: ListElem Shared Addr = 0x2b146b80
32: SYSTEM: Creating ListMP [HOST_IPC_OUT_19] in region 0 ...
34: SYSTEM: Creating ListMP [HOST_IPC_IN_19] in region 0 ...
36: SYSTEM: ListElem Shared Addr = 0x2b164680
37: SYSTEM: Creating ListMP [HOST_IPC_OUT_20] in region 0 ...
40: SYSTEM: Creating ListMP [HOST_IPC_IN_20] in region 0 ...
41: SYSTEM: ListElem Shared Addr = 0x2b184080
42: SYSTEM: Creating ListMP [HOST_IPC_OUT_21] in region 0 ...
44: SYSTEM: Creating ListMP [HOST_IPC_IN_21] in region 0 ...
46: SYSTEM: ListElem Shared Addr = 0x2b1a3a80
65: SYSTEM: System Common Init Done !!!
yinxr TEST, 05-09-am.
============
Chain Select
============
Current System Settings,
NSF Mode : SNF + TNF
1: Multi CH Capture + NSF + DEI + Display (16CH 4x TVP5158, NTSC, YUV422I )
2: Multi CH Src + Enc + Dec + Snk (VideoM3 chain) (VideoM3 local loopBack)
3: Multi CH Cap + NF + Enc + Dec + SW (DEI/H,SC5) + Disp (16CH Cap+Enc+Dec+Disp, Interlace Enc/Dec)
4: Multi CH Cap + NF + DEI/H + Enc + Dec + SW (SC5) + Disp (16CH Cap+Enc+Dec+Disp, Progressive Enc/Dec)
s: System Settings
x: Exit
Enter Choice: 1
11595: CHAINS : CPU Revision [ES1.1] !!!
11595: CHAINS : Detected [1x SII9233A, 1x SII9134 CZ] Board !!!
11595: CHAINS : Base Board Revision [DVR] !!!
11595: CHAINS : Daughter Card Revision [DVR] !!!
[host] Set auto detecting video standard mode (y/n): n
[host] Select video standard:
1: 1920x1080P60
2: 1920x1080P50
3: 1920x1080P30
4: 1920x1080P25
5: 1920x1080P24
6: 1920x1080I60
7: 1920x1080I50
8: 1280x720P60
9: 1280x720P50
10: 1280x720P30
11: 1280x720P25
12: 1280x720P24
13: 720x576P50
14: 720x576I50
15: 720x480P60
16: 720x480I60
17: WUXGA(1920x1200)60
18: UXGA+(1600*1200)60
19: SXGA+(1400*1050)60
20: WXGA(1360*768)60
21: SXGA(1280*1024)60
22: WXGA(1280*768)60
23: XGA(1024*768)60
24: SVGA(800*600)60
25: VGA(640*480)60
1
Display 0: Layout: CHAINS_LAYOUT_2X2_PLUS_4CH
[m3vpss ] 33629: CAPTURE: Create in progress !!!
[m3vpss ] 33658: CAPTURE: VIP0 PortA capture mode is [ 8-bit, Pixel-mux Embedded Sync] !!!
19054:!!!SLAVE CORE [VPSS-M3] DOWN!!!
SystemLink_copySlaveCoreExceptionContext:146
[m3vpss ] 33744: CAPTURE: VIP0 PortA capture mode is [16-bit, Non-mux Embedded Sync] !!!
[m3vpss ] Unhandled Exception:
[m3vpss ] Exception occurred in ThreadType_Task
[m3vpss ] handle: 0x3eecf928.
[m3vpss ] stack base: 0x3ef462a0.
[m3vpss ] stack size: 0x8000.
[m3vpss ] R0 = 0x4409ad80 R8 = 0x3e8151cc
[m3vpss ] R1 = 0x3e76d724 R9 = 0x00000000
[m3vpss ] R2 = 0x00000000 R10 = 0x4409ad88
[m3vpss ] R3 = 0x4409abcc R11 = 0x3e730edc
[m3vpss ] R4 = 0x3e769c40 R12 = 0x00000000
[m3vpss ] R5 = 0x3e769c44 SP(R13) = 0x3ef4e148
[m3vpss ] R6 = 0x3e72e170 LR(R14) = 0x00000001
[m3vpss ] R7 = 0x00000000 PC(R15) = 0x0042e810
[m3vpss ] PSR = 0x61000000
[m3vpss ] ICSR = 0x00400803
[m3vpss ] MMFSR = 0x00
[m3vpss ] BFSR = 0x04
[m3vpss ] UFSR = 0x0000
[m3vpss ] HFSR = 0x40000000
[m3vpss ] DFSR = 0x00000000
[m3vpss ] MMAR = 0xe000ed34
[m3vpss ] BFAR = 0xe000ed38
[m3vpss ] AFSR = 0x00000000
[m3vpss ] Terminating Execution...
mmap of [0xbe9e0000:36864]
mmap virt addresss:0x2ab62000
munmap of [0x2ab62000:36864]
SystemLink_copySlaveCoreExceptionContext:153
Regards,
XueRui