This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

the problem when migrate to RDK4.0

Hi,

    I use rdk2.8 and EVM before, and now migrate to RDK4.0.

    When I run ./init.sh and ./load, the log showed bellow.

    Could you tell me how to fix it?

Thanks!

Best regards!

 

root@vt8168:~# cd /opt/dvr_rdk/ti816x/
root@vt8168:/opt/dvr_rdk/ti816x# ./init.sh
*** Bootargs Validated for mem param ***
*** Bootargs Validated for notifyk.vpssm3 params ***
*** Kernel Base address validated ***
Kernel bootargs validated
amixer: Cannot find the given element from control default

amixer: Cannot find the given element from control default

 [c6xdsp ] Remote Debug Shared Memory @ 0xbf000000
 [m3video] Remote Debug Shared Memory @ 0xbf010820
 [m3vpss ] Remote Debug Shared Memory @ 0xbf021040
 Setting DMM priority for [DUCATI  ] to [0] ( 0x4e000624 = 0x08000000 )
 Setting DMM priority for [HDVICP0 ] to [2] ( 0x4e000634 = 0x0000000a )
 Setting DMM priority for [HDVICP1 ] to [2] ( 0x4e000634 = 0x000a0000 )
 Setting DMM priority for [HDVICP2 ] to [2] ( 0x4e000634 = 0x00a00000 )
/opt/dvr_rdk/ti816x
root@vt8168:/opt/dvr_rdk/ti816x# ./load.sh
Attached to slave procId 2.
Loaded file ../firmware/dvr_rdk_fw_m3vpss_1024M_256M.xem3 on slave procId 2.
Started slave procId 2.
After Ipc_loadcallback status [0x00000000]
 [m3vpss ] ***** VPSS Firmware build time 10:34:13 May  8 2013  EDG gcc 3.0 mode
 [m3vpss ] ***** SYSTEM  : Frequency <ORG> - 250000000, <NEW> - 274909088
 [m3vpss ] notify_attach  rtnVal  0
 [m3vpss ] initProxyServer  rtnVal  0
 [m3vpss ] 
 [m3vpss ]  *** UTILS: CPU KHz = 549818 Khz ***
 [m3vpss ] 
 [m3vpss ]  35: SYSTEM  : System Common Init in progress !!!
 [m3vpss ]  35: SYSTEM: IPC init in progress !!!
 [m3vpss ]  35: SYSTEM: Attaching to [HOST] ...
 [m3vpss ]  38: SYSTEM: Attaching to [HOST] ... SUCCESS !!!
After Ipc_startcallback status [0x00000000]
Attached to slave procId 1.
 [m3vpss ] Unhandled Exception:
 [m3vpss ] Exception occurred in ThreadType_SWI
 [m3vpss ] handle: 0x0.
 [m3vpss ] stack base: 0x9dc5ada4.
 [m3vpss ] stack size: 0x4000.
 [m3vpss ] R0 = 0xd1042800  R8  = 0x9da343a8
 [m3vpss ] R1 = 0xe020f8df  R9  = 0x9da343a0
 [m3vpss ] R2 = 0x68004808  R10 = 0x9da343a4
 [m3vpss ] R3 = 0x00000001  R11 = 0x9da345d4
 [m3vpss ] R4 = 0x00000000  R12 = 0x9da33f3c
 [m3vpss ] R5 = 0x9da33f44  SP(R13) = 0x9dc5ecc8
 [m3vpss ] R6 = 0x9dc56df0  LR(R14) = 0x9d9fe7cf
 [m3vpss ] R7 = 0x00000000  PC(R15) = 0x68004808
 [m3vpss ] PSR = 0x60000000
 [m3vpss ] ICSR = 0x00400803
 [m3vpss ] MMFSR = 0x00
 [m3vpss ] BFSR = 0x01
 [m3vpss ] UFSR = 0x0000
 [m3vpss ] HFSR = 0x40000000
 [m3vpss ] DFSR = 0x00000000
 [m3vpss ] MMAR = 0xe000ed34
 [m3vpss ] BFAR = 0xe000ed38
 [m3vpss ] AFSR = 0x00000000
 [m3vpss ] Terminating Execution...
Loaded file ../firmware/dvr_rdk_fw_m3video_1024M_256M.xem3 on slave procId 1.
Started slave procId 1.
After Ipc_loadcallback status [0x00000000]
Error in Ipc_control Ipc_CONTROLCMD_STARTCALLBACK [0xffffffff]
Attached to slave procId 0.
Loaded file ../firmware/dvr_rdk_fw_c6xdsp_1024M_256M.xe674 on slave procId 0.
Started slave procId 0.
After Ipc_loadcallback status [0x00000000]
 [c6xdsp ] ***** VIDEO Firmware build time 10:31:58 May  8 2013  EDG gcc 3.0 mode
 [c6xdsp ] ***** SYSTEM  : Frequency <ORG> - 800000000, <NEW> - 1000000000
 [c6xdsp ] 
 [c6xdsp ]  *** UTILS: CPU KHz = 1000000 Khz ***
 [c6xdsp ] 
 [c6xdsp ]  5: SYSTEM  : System Common Init in progress !!!
 [c6xdsp ]  5: SYSTEM: IPC init in progress !!!
 [c6xdsp ]  5: SYSTEM: Attaching to [HOST] ...
 [c6xdsp ]  10: SYSTEM: Attaching to [HOST] ... SUCCESS !!!
After Ipc_startcallback status [0x00000000]
 [c6xdsp ] Remote Debug Shared Memory @ 0xbf000000
 [m3video] Remote Debug Shared Memory @ 0xbf010820
 [m3vpss ] Remote Debug Shared Memory @ 0xbf021040

 [c6xdsp ]  1015: SYSTEM: Attaching to [VIDEO-M3] ...
 [c6xdsp ]  2022: SYSTEM: Attaching to [VIDEO-M3] ...
 [c6xdsp ]  3029: SYSTEM: Attaching to [VIDEO-M3] ...
 [c6xdsp ]  4036: SYSTEM: Attaching to [VIDEO-M3] ...
 [c6xdsp ]  5043: SYSTEM: Attaching to [VIDEO-M3] ...
 [c6xdsp ]  6051: SYSTEM: Attaching to [VIDEO-M3] ...
 [c6xdsp ]  7058: SYSTEM: Attaching to [VIDEO-M3] ...

  • Pls share the full logs from kernel boot onwards. Which EVM revision are you using ? Are you using uboot,uImage,and filesystem that is included as part of RDK 4.0 release ?

    Also are you compiling with the arm-arago-Linux-gnueabi toolchain that is included as part of the release. Are you seeing the issue with the prebuilt binaries that are part of the release ?

  • U-Boot 2010.06-svn2 (May 09 2013 - 18:46:26)
    
    I2C:   ready
    DRAM:  2 GiB
    NAND:  HW ECC BCH8 Selected
    256 MiB
    MMC:   OMAP SD/MMC: 0
    Net:   Detected MACID:84:7e:40:d0:79:62
    Ethernet PHY: GENERIC @ 0x00
    DaVinci EMAC
    write 0x55aa, readback 0x0000
    Hit any key to stop autoboot:  0 
    
    NAND read: device 0 offset 0x580000, size 0x440000
     4456448 bytes read: OK
    ## Booting kernel from Legacy Image at 80009000 ...
       Image Name:   Linux-2.6.37+
       Image Type:   ARM Linux Kernel Image (uncompressed)
       Data Size:    2290540 Bytes = 2.2 MiB
       Load Address: 80008000
       Entry Point:  80008000
       Verifying Checksum ... OK
       Loading Kernel Image ... OK
    OK
    
    Starting kernel ...
    
    Uncompressing Linux... done, booting the kernel.
    [    0.000000] Linux version 2.6.37+ (root@ubuntu) (gcc version 4.5.3 20110311 (prerelease) (GCC) ) #1 Thu May 9 11:30:23 CST 2013
    [    0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c53c7f
    [    0.000000] CPU: VIPT nonaliasing data cache, VIPT aliasing instruction cache
    [    0.000000] Machine: ti8168evm
    [    0.000000] vram size = 20971520 at 0x0
    [    0.000000] ti81xx_reserve: ### Reserved DDR region @8ff00000
    [    0.000000] reserved size = 20971520 at 0x0
    [    0.000000] FB: Reserving 20971520 bytes SDRAM for VRAM
    [    0.000000] Memory policy: ECC disabled, Data cache writeback
    [    0.000000] OMAP chip is TI8168 2.0
    [    0.000000] Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 59648
    [    0.000000] Kernel command line: console=ttyO2,115200n8 root=/dev/nfs rw nfsroot=10.1.10.75:/opt/RDK4_0/dvrrdk/DVRRDK_04.00.00.03/target/rM
    [    0.000000] PID hash table entries: 1024 (order: 0, 4096 bytes)
    [    0.000000] Dentry cache hash table entries: 32768 (order: 5, 131072 bytes)
    [    0.000000] Inode-cache hash table entries: 16384 (order: 4, 65536 bytes)
    [    0.000000] Memory: 234MB 1MB = 235MB total
    [    0.000000] Memory: 233404k/233404k available, 28740k reserved, 0K highmem
    [    0.000000] Virtual kernel memory layout:
    [    0.000000]     vector  : 0xffff0000 - 0xffff1000   (   4 kB)
    [    0.000000]     fixmap  : 0xfff00000 - 0xfffe0000   ( 896 kB)
    [    0.000000]     DMA     : 0xffc00000 - 0xffe00000   (   2 MB)
    [    0.000000]     vmalloc : 0xd0800000 - 0xf8000000   ( 632 MB)
    [    0.000000]     lowmem  : 0xc0000000 - 0xd0000000   ( 256 MB)
    [    0.000000]     pkmap   : 0xbfe00000 - 0xc0000000   (   2 MB)
    [    0.000000]     modules : 0xbf000000 - 0xbfe00000   (  14 MB)
    [    0.000000]       .init : 0xc0008000 - 0xc003f000   ( 220 kB)
    [    0.000000]       .text : 0xc003f000 - 0xc045d000   (4216 kB)
    [    0.000000]       .data : 0xc045e000 - 0xc049bd00   ( 248 kB)
    [    0.000000] SLUB: Genslabs=11, HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
    [    0.000000] NR_IRQS:375
    [    0.000000] IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts
    [    0.000000] Total of 128 interrupts on 1 active controller
    [    0.000000] GPMC revision 6.0
    [    0.000000] Trying to install interrupt handler for IRQ368
    [    0.000000] Trying to install interrupt handler for IRQ369
    [    0.000000] Trying to install interrupt handler for IRQ370
    [    0.000000] Trying to install interrupt handler for IRQ371
    [    0.000000] Trying to install interrupt handler for IRQ372
    [    0.000000] Trying to install interrupt handler for IRQ373
    [    0.000000] Trying to install interrupt handler for IRQ374
    [    0.000000] Trying to install type control for IRQ375
    [    0.000000] Trying to set irq flags for IRQ375
    [    0.000000] OMAP clockevent source: GPTIMER1 at 27000000 Hz
    [    0.000000] Console: colour dummy device 80x30
    [    0.000000] Calibrating delay loop... 1199.30 BogoMIPS (lpj=5996544)
    [    0.230000] pid_max: default: 32768 minimum: 301
    [    0.230000] Security Framework initialized
    [    0.230000] Mount-cache hash table entries: 512
    [    0.230000] CPU: Testing write buffer coherency: ok
    [    0.230000] devtmpfs: initialized
    [    0.230000] TI81XX: Map 0x8ff00000 to 0xfe500000 for dram barrier
    [    0.230000] TI81XX: Map 0x40300000 to 0xfe600000 for sram barrier
    [    0.230000] omap_voltage_early_init: voltage driver support not added
    [    0.230000] regulator: core version 0.5
    [    0.230000] regulator: dummy: 
    [    0.230000] NET: Registered protocol family 16
    [    0.230000] omap_voltage_domain_lookup: Voltage driver init not yet happened.Faulting!
    [    0.230000] omap_voltage_add_dev: VDD specified does not exist!
    [    0.230000] OMAP GPIO hardware version 0.1
    [    0.230000] OMAP GPIO hardware version 0.1
    [    0.230000] omap_mux_init: Add partition: #1: core, flags: 0
    [    0.230000] registered ti816x_gpio_vr device
    [    0.230000] registered ti816x_sr device
    [    0.230000] Cannot clk_get ck_32
    [    0.230000] pm_dbg_init: only OMAP3 supported
    [    0.230000] registered ti81xx_vpss device
    [    0.230000] registered ti81xx_vidout device
    [    0.230000] registered ti81xx on-chip HDMI device
    [    0.230000] registered ti81xx_fb device
    [    0.230000] registered ti81xx_vin device
    [    0.240000] bio: create slab <bio-0> at 0
    [    0.240000] regulator: VFB: 800 <--> 1025 mV at 800 mV 
    [    0.240000] SCSI subsystem initialized
    [    0.240000] Advanced Linux Sound Architecture Driver Version 1.0.23.
    [    0.240000] Switching to clocksource gp timer
    [    0.240000] NET: Registered protocol family 2
    [    0.240000] IP route cache hash table entries: 2048 (order: 1, 8192 bytes)
    [    0.240000] TCP established hash table entries: 8192 (order: 4, 65536 bytes)
    [    0.240000] TCP bind hash table entries: 8192 (order: 3, 32768 bytes)
    [    0.240000] TCP: Hash tables configured (established 8192 bind 8192)
    [    0.240000] TCP reno registered
    [    0.240000] UDP hash table entries: 256 (order: 0, 4096 bytes)
    [    0.240000] UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
    [    0.240000] NET: Registered protocol family 1
    [    0.240000] RPC: Registered udp transport module.
    [    0.240000] RPC: Registered tcp transport module.
    [    0.240000] RPC: Registered tcp NFSv4.1 backchannel transport module.
    [    0.240000] NetWinder Floating Point Emulator V0.97 (double precision)
    [    0.240000] PMU: registered new PMU device of type 0
    [    0.240000] omap-iommu omap-iommu.0: ducati registered
    [    0.240000] omap-iommu omap-iommu.1: sys registered
    [    0.300000] JFFS2 version 2.2. (NAND) © 2001-2006 Red Hat, Inc.
    [    0.300000] msgmni has been set to 455
    [    0.300000] io scheduler noop registered
    [    0.300000] io scheduler deadline registered
    [    0.300000] io scheduler cfq registered (default)
    [    0.300000] Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled
    [    0.300000] omap_uart.0: ttyO0 at MMIO 0x48020000 (irq = 72) is a OMAP UART0
    [    0.300000] omap_uart.1: ttyO1 at MMIO 0x48022000 (irq = 73) is a OMAP UART1
    [    0.300000] omap_uart.2: ttyO2 at MMIO 0x48024000 (irq = 74) is a OMAP UART2
    [    0.870000] console [ttyO2] enabled
    [    0.880000] brd: module loaded
    [    0.880000] loop: module loaded
    [    0.880000] ahci probe: devid name is ahci
    [    0.890000] ahci CAP register dump =0x6726ff81
    [    0.890000] Modified ahci CAP register dump =0x6f26ff81
    [    0.900000] ahci ahci.0: forcing PORTS_IMPL to 0x3
    [    0.900000] ahci: SSS flag set, parallel bus scan disabled
    [    0.910000] ahci ahci.0: AHCI 0001.0100 32 slots 2 ports 3 Gbps 0x3 impl platform mode
    [    0.920000] ahci ahci.0: flags: ncq sntf stag pm led clo only pmp pio slum part ccc 
    [    0.930000] scsi0 : ahci_platform
    [    0.930000] scsi1 : ahci_platform
    [    0.930000] ata1: SATA max UDMA/133 mmio [mem 0x4a140000-0x4a150fff] port 0x100 irq 16
    [    0.940000] ata2: SATA max UDMA/133 mmio [mem 0x4a140000-0x4a150fff] port 0x180 irq 16
    [    0.950000] omap2-nand driver initializing
    [    0.960000] ONFI param page 0 valid
    [    0.960000] ONFI flash detected
    [    0.960000] NAND device: Maf ID: 0x2c, Chip ID: 0xca (Micron, NAND 256MiB 3,3V 16-bit)
    [    0.960000]  erasesize: 0x20000, writesize: 2048, oobsize: 64
    [    0.980000] omap2-nand: detected x16 NAND flash 
    [    0.980000] Creating 6 MTD partitions on "omap2-nand.0":
    [    0.990000] 0x000000000000-0x000000260000 : "U-Boot"
    [    0.990000] 0x000000260000-0x000000280000 : "U-Boot Env"
    [    1.000000] 0x000000280000-0x000000580000 : "U-Boot Logo"
    [    1.010000] 0x000000580000-0x0000009c0000 : "Kernel"
    [    1.010000] 0x0000009c0000-0x00000d1e0000 : "File System"
    [    1.100000] 0x00000d1e0000-0x000010000000 : "Reserved"
    [    1.180000] davinci_mdio davinci_mdio.0: davinci mdio revision 1.6
    [    1.180000] davinci_mdio davinci_mdio.0: detected phy mask fffffffe
    [    1.190000] davinci_mdio.0: probed
    [    1.190000] davinci_mdio davinci_mdio.0: phy[0]: device 0:00, driver unknown
    [    1.200000] mice: PS/2 mouse device common for all mice
    [    1.210000] omap_rtc omap_rtc: rtc core: registered omap_rtc as rtc0
    [    1.210000] i2c /dev entries driver
    [    1.220000] Linux video capture interface: v2.00
    [    1.220000] OMAP Watchdog Timer Rev 0x00: initial timeout 60 sec
    [    1.230000] notify_init : notify drivercreated  for  remote proc id 2 at physical Address 0xbee00000
    [    1.240000] asoc: HDMI-DAI-CODEC <-> hdmi-dai mapping ok
    [    1.240000] ALSA device list:
    [    1.250000]   #0: TI81XX SOUND1
    [    1.250000] TCP cubic registered
    [    1.250000] NET: Registered protocol family 17
    [    1.260000] VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3
    [    1.270000] omap_voltage_late_init: Voltage driver support not added
    [    1.270000] Power Management for TI81XX.
    [    1.280000] smartreflex smartreflex: Driver initialized
    [    1.290000] omap_rtc omap_rtc: setting system clock to 2000-01-01 00:00:01 UTC (946684801)
    [    1.410000] ata1: SATA link down (SStatus 0 SControl 300)
    [    1.760000] ata2: SATA link down (SStatus 0 SControl 300)
    [    1.800000] davinci_mdio davinci_mdio.0: resetting idled controller
    [    1.800000] net eth0: attached PHY driver [Generic PHY] (mii_bus:phy_addr=0:00, id=4061e4)
    [    2.820000] Sending DHCP requests .
    [    3.800000] PHY: 0:00 - Link is Up - 100/Full
    [    5.600000] ., OK
    [    5.620000] IP-Config: Got DHCP answer from 10.1.3.162, my address is 10.1.10.103
    [    5.620000] IP-Config: Complete:
    [    5.630000]      device=eth0, addr=10.1.10.103, mask=255.255.255.0, gw=10.1.10.254,
    [    5.630000]      host=10.1.10.103, domain=, nis-domain=(none),
    [    5.640000]      bootserver=10.1.3.162, rootserver=10.1.10.75, rootpath=
    [    5.690000] VFS: Mounted root (nfs filesystem) on device 0:14.
    [    5.700000] devtmpfs: mounted
    [    5.700000] Freeing init memory: 220K
    INIT: version 2.88 booting
     Mounting /dev/shm              :  Mounting /dev/pts          :  Mounting other filesystems : mount: mounting usbfs on /proc/bus/usb failed: y
     Mounting /dev/sda1              :  Mounting /dev/sda2              : mkdir: can't create directory '/media': File exists
    mkdir: can't create directory '/media/sda2': File exists
    Sync command ...Error opening /dev/fb0: No such file or directory
    Starting udev
    [    6.560000] udev[67]: starting version 164
    Starting Bootlog daemon: bootlogd.
    Applying sync command
    
    
    HDCard 2.0 (2012.12)
    
    vt8168 login: root
    Password: 
    root@vt8168:~# 
    root@vt8168:~# 
    root@vt8168:~# 
    root@vt8168:~# cd /opt/dvr_rdk/ti816x/
    root@vt8168:/opt/dvr_rdk/ti816x# ./init.sh 
    *** Bootargs Validated for mem param ***
    *** Bootargs Validated for notifyk.vpssm3 params ***
    *** Kernel Base address validated ***
    Kernel bootargs validated
    amixer: Cannot find the given element from control default
    
    amixer: Cannot find the given element from control default
    
     [c6xdsp ] Remote Debug Shared Memory @ 0xbf000000
     [m3video] Remote Debug Shared Memory @ 0xbf010820
     [m3vpss ] Remote Debug Shared Memory @ 0xbf021040
     Setting DMM priority for [DUCATI  ] to [0] ( 0x4e000624 = 0x08000000 )
     Setting DMM priority for [HDVICP0 ] to [2] ( 0x4e000634 = 0x0000000a )
     Setting DMM priority for [HDVICP1 ] to [2] ( 0x4e000634 = 0x000a0000 )
     Setting DMM priority for [HDVICP2 ] to [2] ( 0x4e000634 = 0x00a00000 )
    /opt/dvr_rdk/ti816x
    root@vt8168:/opt/dvr_rdk/ti816x# ./load.sh 
    Attached to slave procId 2.
    Loaded file ../firmware/dvr_rdk_fw_m3vpss_1024M_256M.xem3 on slave procId 2.
    Started slave procId 2.
    After Ipc_loadcallback status [0x00000000]
     [m3vpss ] ***** VPSS Firmware build time 10:34:13 May  8 2013  EDG gcc 3.0 mode
     [m3vpss ] ***** SYSTEM  : Frequency <ORG> - 250000000, <NEW> - 274909088
     [m3vpss ] notify_attach  rtnVal  0
     [m3vpss ] initProxyServer  rtnVal  0
     [m3vpss ]  
     [m3vpss ]  *** UTILS: CPU KHz = 549818 Khz ***
     [m3vpss ]  
     [m3vpss ]  35: SYSTEM  : System Common Init in progress !!!
     [m3vpss ]  35: SYSTEM: IPC init in progress !!!
     [m3vpss ]  35: SYSTEM: Attaching to [HOST] ... 
     [m3vpss ]  38: SYSTEM: Attaching to [HOST] ... SUCCESS !!!
    After Ipc_startcallback status [0x00000000]
    Attached to slave procId 1.
     [m3vpss ] Unhandled Exception:
     [m3vpss ] Exception occurred in ThreadType_SWI
     [m3vpss ] handle: 0x0.
     [m3vpss ] stack base: 0x9dc5ada4.
     [m3vpss ] stack size: 0x4000.
     [m3vpss ] R0 = 0xd1042800  R8  = 0x9da343a8
     [m3vpss ] R1 = 0xe020f8df  R9  = 0x9da343a0
     [m3vpss ] R2 = 0x68004808  R10 = 0x9da343a4
     [m3vpss ] R3 = 0x00000001  R11 = 0x9da345d4
     [m3vpss ] R4 = 0x00000000  R12 = 0x9da33f3c
     [m3vpss ] R5 = 0x9da33f44  SP(R13) = 0x9dc5ecc8
     [m3vpss ] R6 = 0x9dc56df0  LR(R14) = 0x9d9fe7cf
     [m3vpss ] R7 = 0x00000000  PC(R15) = 0x68004808
     [m3vpss ] PSR = 0x60000000
     [m3vpss ] ICSR = 0x00400803
     [m3vpss ] MMFSR = 0x00
     [m3vpss ] BFSR = 0x01
     [m3vpss ] UFSR = 0x0000
     [m3vpss ] HFSR = 0x40000000
     [m3vpss ] DFSR = 0x00000000
     [m3vpss ] MMAR = 0xe000ed34
     [m3vpss ] BFAR = 0xe000ed38
     [m3vpss ] AFSR = 0x00000000
     [m3vpss ] Terminating Execution...
    Loaded file ../firmware/dvr_rdk_fw_m3video_1024M_256M.xem3 on slave procId 1.
    Started slave procId 1.
    After Ipc_loadcallback status [0x00000000]
    Error in Ipc_control Ipc_CONTROLCMD_STARTCALLBACK [0xffffffff]
    Attached to slave procId 0.
    Loaded file ../firmware/dvr_rdk_fw_c6xdsp_1024M_256M.xe674 on slave procId 0.
    Started slave procId 0.
    After Ipc_loadcallback status [0x00000000]
     [c6xdsp ] ***** VIDEO Firmware build time 10:31:58 May  8 2013  EDG gcc 3.0 mode
     [c6xdsp ] ***** SYSTEM  : Frequency <ORG> - 800000000, <NEW> - 1000000000
     [c6xdsp ]  
     [c6xdsp ]  *** UTILS: CPU KHz = 1000000 Khz ***
     [c6xdsp ]  
     [c6xdsp ]  5: SYSTEM  : System Common Init in progress !!!
     [c6xdsp ]  5: SYSTEM: IPC init in progress !!!
     [c6xdsp ]  5: SYSTEM: Attaching to [HOST] ... 
     [c6xdsp ]  10: SYSTEM: Attaching to [HOST] ... SUCCESS !!!
    After Ipc_startcallback status [0x00000000]
     [c6xdsp ] Remote Debug Shared Memory @ 0xbf000000
     [m3video] Remote Debug Shared Memory @ 0xbf010820
     [m3vpss ] Remote Debug Shared Memory @ 0xbf021040
    
     [c6xdsp ]  1015: SYSTEM: Attaching to [VIDEO-M3] ... 
     [c6xdsp ]  2022: SYSTEM: Attaching to [VIDEO-M3] ... 
     [c6xdsp ]  3029: SYSTEM: Attaching to [VIDEO-M3] ... 
     [c6xdsp ]  4036: SYSTEM: Attaching to [VIDEO-M3] ... 
     [c6xdsp ]  5043: SYSTEM: Attaching to [VIDEO-M3] ... 
     [c6xdsp ]  6051: SYSTEM: Attaching to [VIDEO-M3] ... 
     [c6xdsp ]  7058: SYSTEM: Attaching to [VIDEO-M3] ...
    
    
    

  • The logs shows you have not migrated to the uboot that is part of DVR RDK 4.0. Pls use uboot that is part of RDK 4.0. Also I dont see syslink being insmod-ed. Can you check if your filesystem is updated with the correct binaries and you are using the filesystem that is part of RDK 4.0 release and not an older release.Also have your tried the pre built binaries ? Is this TI EVM or your custom board . Pls mention the EVM revision if you are using EVM.

  • Hi Badri,

        Thank you for your reply!

       I am using my own board and rdk4.0!

        The problem has been solved! That is because the DDR timing. Changing DDR3_SW_LEVELING is OK !

        But now I meet another problem.Could you move to http://e2e.ti.com/support/dsp/davinci_digital_media_processors/f/717/t/264273.aspx ,and give me some advices?

    Thank you !

    Best regards!