Good afternoon,
We have just got a OMAP35x EVM board to evaluate. I have it running in CCSv5 using a XDS510 USB with the omap3530 gel files.
I have a couple of questions fistly in the Gel files it sets the system clock as 19.2MHz but the clock on the board is 26MHz so is this incorrect in the Gel file? I have changed it and it does not effect the small bench mark program I am running therefor I assume it aslso does not change the clock speed of the processor so what is it doing?
Secondly by decault the processor clock seems to be set as 330MHz. I want to run it at 720MHz. So I started by halfing the DPLL_DIV_VALUE divider and then doubling the nL3Div divider to keep the L3 clock at at 166MHz. This stops it working, the program is loaded but with this error in the console
"Cortex_A8_0: Trouble Setting Breakpoint with the Action "Finish Auto Run" at 0x8005baf4: Error 0x20000008/-1066 Severe Error during: Break Point, Cannot set/verify breakpoint at 0x8005BAF4"
it does not jump to main as usual and seems to be disconnected from the device ("disconect from device" in run menu is grayed out), when I click connect it gives the following error
"Error connecting to the target: Error 0x80000244/-1178 Fatal Error during: Register, Initialization, OCS, The target does not have a CPU clock. ".
This is the info printed when the modified Gel file is loaded:
Can anybody suggest what I am doing wrong in changing the CPU frequency of the ARM and why changing he clock from 19.2MHz (which I belive is wrong) to 26MHz has no effect?
Many thanks
Sean