Hi,
The XGCONF tool is not displaying any of the information from the .cfg file in both the instance as well as 'Properties' tab. I created a new example project (SYSBIOS-> Static Example). I opened the .cfg file as is and see the problem. When I try to add a new instance of say a task the cfg file gets updated correctly but if I close and re-open the file I can no longer see the properties.
I am using the following versions
CCS - 5.3.0.00090
SYSBIOS - 6.34.2.18
XDCTools - 3.24.6.63
Regards,
Sudhanand.