Hi, is just that i am working with a Pandaboard ES, with Android 4.0 and kernel 3.0.8, and i'm using the parallel display option with an LVDS converter and a 14'' LCD (also a 15.6'' LCD), but the resolution is not the right one, so i modified the /drivers/video/omap2/displays/panel-generic-dpi.c and the max resolution that i could get was 1330x770 but is not the right one for the LCDs, i still have a black strip because the resolution is not being adjusted to the LCD, is there a way to change it in Android, for it to be adjusted complete to the LCD??? , because when i try a bigger resolution, the system UI stops working. i really need some help on this, thanks in advanced.