Other Parts Discussed in Thread: TMS320C5535
Hi all,
I want to use TMS320C5535 in a timing critical project. But I am not familiar with TMS320C5535.
First I have looked that TMS320C5535 does not have external clock input for the timers module.
So I decide to provide 2.5ppm (maybe 1 ppm) 12Mhz clock signal to TMS320C5535.
But I could not able to find any data regarding the PLL unit and internal timing accuracy.
Required speed is 100Mhz and accuracy is 5ppm. (Including temperature, aging, supply etc.)
Is it possible for TMS320C5535 ? (10ns tcy with 5ppm accuracy)
Is CLKOUT pin frequency exactly same with the system clock ?
Best regards.