Hello,
Can any one tell if the new v03.03.00.051 dated 15-Apr-2013 is compatible with the C5535 ?
Can any one also give more info about the C5517 ?
Thanks,
Nicolas
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
Can any one tell if the new v03.03.00.051 dated 15-Apr-2013 is compatible with the C5535 ?
Can any one also give more info about the C5517 ?
Thanks,
Nicolas
I give answer to my post : YES.
In the Installation guide, the following is written :
CSL has been tested on Code Composer StudioTM Ver5.2. The following platforms have been used for
testing:
• C5515 EVM
• C5535 eZdsp
• C5517 EVM
Nicolas
Hello Nicolas,
Yes , " CSL v03.03.00.051" supports C5535 eZDSP aswell.
On the other question that you had asked on C5517:
C5517 is not yet in mass production. So if you need more information this, please contact local TI FAE.
Hope this helps.
Regards
Vasanth
Keep in mind you have to specify the correct device and platform in csl_general.h. It looks like "out of the box", the csl as delivered will build for the 05/15/35 on the 5515 EVM platform. See section 3 of the installation guide for more details.
-S