Hi,
I Just got this new DM385 IPNC.
It can boot properly to the Linux prompt with its original Linux Kernel
Image Name: Linux-2.6.37_DM385_IPNC_3.50.00
Created: 2012-12-21 11:57:15 UTC
But when I tried to use it's Web inrterface, it always pop up an error box "Windows has found a problem" with this file"
Name: IPNCWebDlls.CAB
Publisher: unkown publisher
This file was blocked because it does not have a valid digital signature.
I already changed my IE's security level options to prompt when downloading unsigned Activex control, but it still have this error.
and when I tried to use RTSP stream by adding "rtsp://192.168.1.168:8556/PSIA/Streaming/channels/2?videoCodecType=H.264" to my VLC network setting, it did not work and no error was returned.
Is there any setting wrong ?
Please help me with this issue.
Thank you very much!
Ivy