This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OMAP3530/DM3730 DPLL4 Settings

Hi, 

I work on DM3730 processor and DPLL clock settings for uart3 module. Some values about my boards are:

OSC_SYS_CLK                         = 26 MHz

SYS_CLK = OSC_SYS_CLK / 2 = 13 MHz

According to Figure 3-61. Common CM Source-Clock Controls on DM3730 Technical Referance Manual:

Setup CM_CLKSEL2_PLL, which sets up M and N for DPLL4. =  M = 576, N = 6 

Setup CM_CLKSEL3_PLL, which sets up M2 for DPLL4          = M2 = 13 

So my PER_48M_FCLK is 48 MHz. Then with "Baud rate = (functional clock/16)/N" formula, my divisor value is 26 for 115200 baudrate. But this setup only works 57600 baud rate with upper PLL settings. 

My other question: I use external oscillator (TPS65950) with 26 MHz and selected sys_boot[6] is 1(for using of an external square clock source). It doesn't work correctly(upper problem occurs). Then I selected sys_boot[6] is 0. But it also doesn't work correctly. Moreover, these 2 setup configurations show same behavior(57600 baud problem).

What do you think about my problems?

Regards,

Emre