This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

wifi problem

Hi

A) From where i should get the firmware for OMAP4 ICS ??

git clone git://git.kernel.org/pub/scm/linux/kernel/git/firmware/linux-firmware.git   (Showing :read error:connection reset by peer)

B) Actually while booting the TI blaze Tablet it showing Error could not get firmware:2

Help me to resolve these two.

Regards

Mukesh

  • Can you check in next links?

    http://omappedia.org/wiki/Android_Mac80211#WLAN_Driver_build_instruction
    http://omappedia.org/wiki/Android_Mac80211#WLAN_Calibration_Instruction

    by the information stored in

    /4ai17/mydroid/hardware/ti/wlan/.git/config

    [remote "omap-mirror"]
        url = git://git.omapzoom.org/platform/hardware/ti/wlan

  • Hi Mukesh.

    According to http://www.omappedia.com/wiki/4AI.1.7_OMAP4_Icecream_Sandwich_Release_Notes#WLAN_Firmware_files, you should find the firmware in the repo.

    I use Jelly Bean instead of ICS, but in the case of JB, the firmware is in device/ti/proprietary-open/wl12xx/wlan/wlan.tgz.

    Regards,

        Steve

  • I didn't see that exact error but if you have a wilink7 and are trying to use the 2.5 build it won't work because 2.5 is building wilink8 driver.   However, you if you build the wilink7 drivers but you either need to rename one of the kernel modules or you can patch device/ti/blaze_tablet/BoardConfig.mk like so:

    diff --git a/BoardConfig.mk b/BoardConfig.mk
    index 5bc63b3..652072d 100644
    --- a/BoardConfig.mk
    +++ b/BoardConfig.mk
    @@ -75,8 +75,8 @@ WPA_SUPPLICANT_VERSION           := VER_0_8_X_TI
     BOARD_HOSTAPD_DRIVER             := NL80211
     BOARD_WLAN_DEVICE                := wl12xx_mac80211
     BOARD_SOFTAP_DEVICE              := wl12xx_mac80211
    -WIFI_DRIVER_MODULE_PATH          := "/system/lib/modules/wlcore_sdio.ko"
    -WIFI_DRIVER_MODULE_NAME          := "wlcore_sdio"
    +WIFI_DRIVER_MODULE_PATH          := "/system/lib/modules/wl12xx_sdio.ko"
    +WIFI_DRIVER_MODULE_NAME          := "wl12xx_sdio"

    jeff