This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
In our custom board, we are using AM335x module.
We want to connect a Ethernet switch(RGMII) directly to AM335x RGMII port without using PHY.
Can anybody give some ideas how to achieve this at u-boot and kernel level?
Thanks & Regards,
Praveen
Hello Prav,
Direct MAC-to-MAC connections are not supported from a HW perspective. There are several threads in this forum discussing the issue, but this is a good one to start with:
http://e2e.ti.com/support/arm/sitara_arm/f/791/t/262120.aspx
Some Ethernet switches do provide a PHY-like interface on one or more ports which would allow you to connect the AM335x MAC directly to the switch.