Other Parts Discussed in Thread: CCSTUDIO
hello,
i'am newbie...
i want to ask about comm_intr() for interrupt in C6713...
it's my code :
interrupt void c_int11()
{
DSK6713_LED_toggle(0);
DSK6713_waitusec(200000);
}
void main(void)
{
DSK6713_init();
DSK6713_LED_init();
comm_intr();
while(1)
{
DSK6713_LED_toggle(1);
DSK6713_waitusec(200000);
}
}
there are 2 error...
**** Build of configuration Debug for project bis1 ****
C:\ti\ccsv5\utils\bin\gmake -k all
'Building file: ../main.c'
'Invoking: C6000 Compiler'
"C:/ti/ccsv5/tools/compiler/c6000_7.3.4/bin/cl6x" -mv6700 -g --define=c6713 --define=CHIP_6713 --include_path="C:/ti/ccsv5/tools/compiler/c6000_7.3.4/include" --include_path="C:/CCStudio_v3.1/C6000/dsk6713/include" --include_path="C:/CCStudio_v3.1/C6000/csl/include" --include_path="E:/Data Danny/Program/CCS5 anyar/bis1/Debug" --include_path="C:/ti/bios_5_41_13_42/packages/ti/bios/include" --include_path="C:/ti/bios_5_41_13_42/packages/ti/rtdx/include/c6000" --display_error_number --diag_warning=225 --abi=coffabi --preproc_with_compile --preproc_dependency="main.pp" "../main.c"
"../main.c", line 49: warning #225-D: function declared implicitly
"../main.c", line 53: warning #112-D: statement is unreachable
'Finished building: ../main.c'
' '
'Building target: bis1.out'
'Invoking: C6000 Linker'
"C:/ti/ccsv5/tools/compiler/c6000_7.3.4/bin/cl6x" -mv6700 -g --define=c6713 --define=CHIP_6713 --display_error_number --diag_warning=225 --abi=coffabi -z -m"bis1.map" --stack_size=0x800 --heap_size=0x800 --warn_sections --display_error_number -i"C:/ti/ccsv5/tools/compiler/c6000_7.3.4/lib" -i"C:/ti/ccsv5/tools/compiler/c6000_7.3.4/include" -i"C:/ti/bios_5_41_13_42/packages/ti/rtdx/lib/c6000" -i"C:/ti/bios_5_41_13_42/packages/ti/bios/lib" --reread_libs --rom_model -o "bis1.out" -l"./bis1cfg.cmd" "./main.obj" "./bis1cfg_c.obj" "./bis1cfg.obj" -l"libc.a" -l"C:\CCStudio_v3.1\C6000\csl\lib\csl6713.lib" -l"C:\CCStudio_v3.1\C6000\dsk6713\lib\dsk6713bsl.lib"
<Linking>
undefined first referenced
symbol in file
--------- ----------------
_comm_intr ./main.obj
error #10234-D: unresolved symbols remain
error #10010: errors encountered during linking; "bis1.out" not built
>> Compilation failure
gmake: *** [bis1.out] Error 1
gmake: Target `all' not remade because of errors.
**** Build Finished ****
anyone can help me...??
thanks a lot...