This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Beagleboard xm camera support

Hai

I'm Sekra

I'm using Omnivision 2 megapixel camera (SOC camera supported CMOS sensor) ans im using 3.2.44 mainline kernel.

I want to write the drivers for the camera working on my beagleboard xm board.

In kernel, the V4L2 camera support for CONFIG_VIDEO_XXX and CONFIG_SOC_CAMERA_SUPPORT.

How can i start this stuff with the camera?How can i write the drivers?

For VIDEO support,it needs .c & .h file of the particular source code

For SOC CAMERA SUPPORT .c is only they were using then along with soc_camera.h file also used.

How could i learn this stuff,Can i write this driver for video support also??

Clarify me.

Thanks in advance........