Hi all,
When I measured the throughput performance of PCIe Memory Write through a PCIe switch, in some case, I obtain a throughput value better than the old measurements when using the BOC between two DSPs C6678!!
it looks non normal non ???
Some details:
- using EDMA: the throughput using PCIe switch is likely less than using the BOC (it looks normal-OK)
- using CPU:
1 - for data nearly <1KB: the throughput using PCIe switch is better than using the BOC (it looks non normal, there is an explaination of that??)
2- for data >1KB: the throughput using PCIe switch is likely less than using the BOC (it looks normal-OK)
PS: the throughput is measured with TSCL/TSCH counter.