Hi
My customer is designing with AM3357, there is a load switch TPS2051 for his USB port.
When there is a hot plug of a USB device, there is a transient voltage drop of and a current surge of 375mA, this is acceptable to the load switch.
In essence, during a hot plug, the USB module in the AM3357 hangs up, the only way to recover the USB port is by resetting the system.
Like to check if; Without changing the hardware, is there a way to disable and enable the USB module via software?