Other Parts Discussed in Thread: TMS320C5515, TLV320AIC34
Hello all
We are developing our application using the TMS320C5515 DSP Evaluation Module and the TLV320AIC34 (Codec) Evaluation Module. We created a breadboard for interconnecting the boards.
We have problems using dlms( ) function of Dsplib 2.4 library. When the code runs from ram using Code Composer 5.3.0 there is a noise of about 100 hz no matter there are not voices (or any sound) at the microphones.
When the dlms () function is not called in the application, there is not that 100 Hz noise and the voices are heard normally at the output of the codec.
On the other hand, when running the code from flash there is only noise at the output of the codec.
Does anyone have idea what is happening? What could be missing when calling the dlms () function?
Best Regards
Nacuri