Hi all,
I downloaded from the page of the TI G726 Encoder and Decoder c55xx, but there are questions.
http://software-dl.ti.com/dsps/dsps_public_sw/codecs/C55X_Speech/index_FDS.html
G726 Encoder and Decoder, Version 2.00.00.012
Appendix B Table B-1 and Appendix A Table A-1 of g726_api_ref_xdais.doc
How to specify is unknown about CompandingLaw of No. 3 in.
the comments of ig726dec.h and ig726enc.h
CONST_COMP_ALAW_8
CONST_COMP_MULAW_8
CONST_COMP_LINEAR_8 (no companding)
It is written above and can be used, but I do not know the value because there is no # define.
Regards.