This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

g726DecoderMain.c of TI sample G.726 Decoder / Encoder

Hi all,

I downloaded from the page of the TI G726 Encoder and Decoder c55xx, but there are questions.

http://software-dl.ti.com/dsps/dsps_public_sw/codecs/C55X_Speech/index_FDS.html
 G726 Encoder and Decoder, Version 2.00.00.012

・g726DecoderMain.c ([install folder]\G726_3X_REL200_ROOTDIR\g726\tstsrc\c55x)

line 121 to 123
        tablesPtr [0] = (void *) G726_TII_g726itbl40;
        tablesPtr [1] = (void *) G726_TII_adpcmalaw;
        tablesPtr [2] = (void *) G726_TII_adpcmmulaw;
It has been an assignment, but can I do? Describe this three lines without thinking?

I think to try to linear PCM format of the PCM, but it is sufficient to describe the three rows in that case?

G726_TII_g726itbl40 is like the encoder table but can not find it.
Please tell me the meaning for the above process.

Regards.