This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PLL doesn't lock

Previous version of our DM8148 board worked ok; recently we made some minor changes to the PCB, now the new PCB doesn't boot. Uboot is stuck at prcm_init()->pll_config(), the PLL status register read back never shows the PLL is locked. this happens on the configuration of audio PLL; if I comment out audio PLL configuration, it will get stuck on the next one.

the oscillator waveform looks normal. I also tried using crystal instead, still same problem.

I would appreciate everyone's input.

  • Hi,

    What is the list of changes? Is anything related to PLL? Have you check JTAG load program and run it?

    Regards,

    Hyun

  • Thanks for the reply.

    The changes:

    1. changed DDR3 from EMIF0 32bit to EMIF0 16bit+EMIF1 16 bit. total capacity doubled to 1GB
    This is an effort to get rid of resizer overflow issue.
    The PLL issue happens before DDR initialization, so I double this is the cause. 

    2. changed main clock from crystal to oscillator.
    But I tried changing it back, no difference. 

    I am using CCS5 to debug it, the rom boot loader loads uboot in MMC without any problem, but it always hangs at pll_config().
    As I mentioned, previous board works fine. 

     

  • update: I found the POR input was not right. I am checking the circuit right now.

  • Fixed POR issue, which is caused by power supply, right now it stucks on ddr_pll_config(),

    the PLL status register reads back 0xC00001E9, so that means "Reference input loss", what could cause this?

    Input oscillator is 20Mhz, DDR is running at 400Mhz.

  • I also tried slowing down the DDR to 200Mhz, same thing.

    anybody? please~

  • Hi Hongfeng,

    Did you perform the DDR leveling? See below for more info:

    http://processors.wiki.ti.com/index.php/TI814x-DDR3-Init-U-Boot

    http://processors.wiki.ti.com/index.php/TI814x-DDR3-Init-U-Boot_Wordwise_SWleveling

    Can you also run memory test from u-boot: http://processors.wiki.ti.com/index.php/DM816x_C6A816x_AM389x_DDR3_Init#Run_mtest

    target# mtest 0x80800000 0xA0000000 0xaa55aa55 3 (referred as Test A)
    target# mtest 0xA0000000 0xC0000000 0xaa55aa55 3 (referred as Test B)

    Regards,
    Pavel

  • Pavel:

    At this point, I don't think it's related to SW leveling. because it's stuck at prcm_init(), which is before function config_ti814x_ddr().

    The DDR won't work anyway if the PLL doesn't even work.

  • Hongfeng,

    Does you flow stuck at the below line?

    ../board/ti/ti8148/evm.c

    prcm_init() -> ddr_pll_config -> pll_config()

    /*
     * configure individual ADPLLJ
     */
    static void pll_config(u32 base, u32 n, u32 m, u32 m2, u32 clkctrl_val)
    {
        u32 m2nval, mn2val, read_clkctrl = 0;

        m2nval = (m2 << 16) | n;
        mn2val = m;

        /* by-pass pll */
        read_clkctrl = __raw_readl(base + ADPLLJ_CLKCTRL);
        __raw_writel((read_clkctrl | 0x00800000), (base + ADPLLJ_CLKCTRL));
        while ((__raw_readl(base + ADPLLJ_STATUS) & 0x101) != 0x101);       ----> stuck here?
        read_clkctrl = __raw_readl(base + ADPLLJ_CLKCTRL);
        __raw_writel((read_clkctrl & 0xfffffffe), (base + ADPLLJ_CLKCTRL));

    Are you on EZSDK 5.05.02.00?

    What is the revision of the DM814x device (PG2.x or 3.x)? http://e2e.ti.com/support/dsp/davinci_digital_media_processors/f/716/t/243814.aspx

    Regards,
    Pavel

  • Thanks for your reply.

    1. the code was stuck at last line of pll_config()

    while ((__raw_readl(base + ADPLLJ_STATUS) & 0x600) != 0x600);

    2. I am using RDK3.2

    3. If I change the boot loader to skip ddr_pll_config(), and let it run entirely from SRAM, then uboot will boot up ok.

    4. Since other PLLs appear normal, and we did change the DDR part, I suspect the hardware is causing the problem, I am working with our PCB engineer trying to figure this out.

    Regards,

    Hongfeng

  • Yes, I also suspect that this is entirely hardware problem. Some pointers for hardware check:

    http://processors.wiki.ti.com/index.php/DM814x_Hardware_Design_Guide

    Regards,
    Pavel

  • I found out what's triggering the problem, but it just makes things more confusing.

    Previously, I lowered the DDR frequency to 200Mhz to rule out other possible causes, now I found that if I change it back to 400Mhz, the PLL works just fine. I tried other values: 300Mhz, 533Mhz, both are working fine. I don't know what's special about this 200Mhz?

  • Hongfeng,

    I can not say for RDK, but for EZSDK DDR3 supports by default 400MHz and 533MHz.

    ti-ezsdk_dm814x-evm_5_05_02_00/board-support/u-boot-2010.06-psp04.04.00.01/include/asm/arch-ti81xx/clocks_ti814x.h

    #define DDR_PLL_400     /* Values supported 400,533 */

    Regards,
    Pavel


  • If its RDK, the DDR parameters (timing, latency etc) set in uboot are not applicable to 200 MHz.