Hello everyone.
We are trying to stream video from FPGA to dm8168evm via vip0. By default vip0 uses embedded sync from tvp7002. Our fpga can do hsync and vsync, has no i2c.
So FPGA gives
- HSYNC
- VSYNC
- DATA_CLK
- DATA[D0-D15]
In file ti81xx_vpss.c i redefined hdvpss_info struct by using this topic http://processors.wiki.ti.com/index.php/DM81xx_AM38xx_Adding_External_Decoders_to_V4L2_Capture_Driver
In file ti81xxvin_main.c
Commented all subdev_call and a part of probe function to let nodes appear.
So, from saLoopBack everything looks fine. ioctls lands in right place, but...In file ti81xxvin_main.c i found a spot where application hangs, videobuf_streamon(&buf_obj->buffer_queue) in vidioc_streamon method.
/*
*
* Framebuffer device registration for TI TI816x platforms
*
* Copyright (C) 2009 Texas Instruments Inc.
* Author: Yihe Hu <yihehu@ti.com>
*
* Some code and ideas taken from TI OMAP2 Platforms
* by Tomi Valkeinen.
*
* This program is free software; you can redistribute it and/or modify it
* under the terms of the GNU General Public License as published by the
* Free Software Foundation; either version 2 of the License, or (at your
* option) any later version.
*
* This program is distributed in the hope that it will be useful, but
* WITHOUT ANY WARRANTY; without even the implied warranty of
* MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the GNU
* General Public License for more details.
*
* You should have received a copy of the GNU General Public License along
* with this program; if not, write to the Free Software Foundation, Inc.,
* 59 Temple Place - Suite 330, Boston, MA 02111-1307, USA.
*/
#include <linux/module.h>
#include <linux/kernel.h>
#include <linux/mm.h>
#include <linux/init.h>
#include <linux/platform_device.h>
#include <linux/bootmem.h>
#include <linux/io.h>
#include <linux/vps_capture.h>
#include <linux/ti81xxfb.h>
#include <linux/ti81xx.h>
#include <mach/hardware.h>
#include <mach/board-ti814x.h>
#include <mach/board-ti816x.h>
#include <asm/mach/map.h>
#if defined(CONFIG_TI81XX_VPSS) || defined(CONFIG_TI81XX_VPSS_MODULE)
static u64 ti81xx_dma_mask = ~(u32)0;
static struct platform_device vpss_device = {
.name = "vpss",
.id = -1,
.dev = {
.platform_data = NULL,
},
};
static struct vps_platform_data vps_pdata;
static int __init ti81xx_vpss_init(void)
{
/*FIXME add platform data here*/
int r;
if (cpu_is_ti816x() || cpu_is_dm385()) {
if (cpu_is_dm385())
vps_pdata.cpu = CPU_DM813X;
else
vps_pdata.cpu = CPU_DM816X;
vps_pdata.numvencs = 4;
vps_pdata.vencmask = (1 << VPS_DC_MAX_VENC) - 1;
} else if (cpu_is_ti814x()) {
vps_pdata.cpu = CPU_DM814X;
vps_pdata.numvencs = 3;
vps_pdata.vencmask = (1 << VPS_DC_MAX_VENC) - 1 \
- VPS_DC_VENC_HDCOMP;
}
vpss_device.dev.platform_data = &vps_pdata;
r = platform_device_register(&vpss_device);
if (r)
printk(KERN_ERR "unable to register ti81xx_vpss device\n");
else
printk(KERN_INFO "registered ti81xx_vpss device\n");
return r;
}
#if defined(CONFIG_TI81XX_HDMI_MODULE) || defined(CONFIG_TI81XX_HDMI)
static struct platform_device ti81xx_hdmi_plat_device = {
.name = "TI81XX_HDMI",
.id = -1,
.num_resources = 0,
.dev = {
/*.release = ti81xx_hdmi_platform_release,*/
.platform_data = NULL,
}
};
static int __init ti81xx_hdmi_init(void)
{
int r;
/*FIXME add platform data here*/
r = platform_device_register(&ti81xx_hdmi_plat_device);
if (r)
printk(KERN_ERR "Unable to register ti81xx onchip-HDMI device\n");
else
printk(KERN_INFO "registered ti81xx on-chip HDMI device\n");
return r;
}
#else
static int __init ti81xx_hdmi_init(void)
{
return 0;
}
#endif
#if defined(CONFIG_VIDEO_TI81XX_VIDIN_MODULE) || \
defined(CONFIG_VIDEO_TI81XX_VIDIN)
#define HDVPSS_CAPTURE_INST0_BASE 0x48105500
#define HDVPSS_CAPTURE_INST0_SIZE 1024u
#define HDVPSS_CAPTURE_INST2_BASE 0x48105A00
#define HDVPSS_CAPTURE_INST2_SIZE 1024u
u8 ti81xx_card_name[] = "TI81xx_catalogue";
struct ti81xxvin_interface tvp7002_pdata = {
.clk_polarity = 0,
.hs_polarity = 0,
.vs_polarity = 1,
.fid_polarity = 0,
.sog_polarity = 0,
};
static struct ti81xxvin_subdev_info hdvpss_capture_sdev_info[] = {
{
.name = TVP7002_INST0,
.board_info = {
/* TODO Find the correct address
of the TVP7002 connected */
I2C_BOARD_INFO("tvp7002", 0x5d),
.platform_data = &tvp7002_pdata,
},
.vip_port_cfg = {
.ctrlChanSel = VPS_VIP_CTRL_CHAN_SEL_15_8,
.ancChSel8b = VPS_VIP_ANC_CH_SEL_DONT_CARE,
.pixClkEdgePol = VPS_VIP_PIX_CLK_EDGE_POL_RISING,
.invertFidPol = 0,
.embConfig = {
.errCorrEnable = 1,
.srcNumPos = VPS_VIP_SRC_NUM_POS_DONT_CARE,
.isMaxChan3Bits = 0,
},
.disConfig = {
.fidSkewPostCnt = 0,
.fidSkewPreCnt = 0,
//.lineCaptureStyle =
//VPS_VIP_LINE_CAPTURE_STYLE_DONT_CARE,
.lineCaptureStyle =
VPS_VIP_LINE_CAPTURE_STYLE_HSYNC,
//.fidDetectMode =
//VPS_VIP_FID_DETECT_MODE_DONT_CARE,
//.fidDetectMode =
//VPS_VIP_FID_DETECT_MODE_PIN,
.fidDetectMode =
VPS_VIP_FID_DETECT_MODE_VSYNC,
.actvidPol = VPS_VIP_POLARITY_DONT_CARE,
.vsyncPol = VPS_VIP_POLARITY_DONT_CARE,
.hsyncPol = VPS_VIP_POLARITY_DONT_CARE,
}
},
.video_capture_mode = VPS_CAPT_VIDEO_CAPTURE_MODE_SINGLE_CH_NON_MUX_DISCRETE_SYNC_HSYNC_VSYNC,
//.video_capture_mode =
//VPS_CAPT_VIDEO_CAPTURE_MODE_SINGLE_CH_NON_MUX_EMBEDDED_SYNC,
.video_if_mode = VPS_CAPT_VIDEO_IF_MODE_16BIT,
//.video_if_mode = VPS_CAPT_VIDEO_IF_MODE_24BIT,
.input_data_format = FVID2_DF_YUV422P,
//.input_data_format = FVID2_DF_RGB24_888,
},
{
.name = TVP7002_INST1,
.board_info = {
I2C_BOARD_INFO("tvp7002", 0x5c),
.platform_data = &tvp7002_pdata,
},
.vip_port_cfg = {
.ctrlChanSel = VPS_VIP_CTRL_CHAN_SEL_15_8,
.ancChSel8b = VPS_VIP_ANC_CH_SEL_DONT_CARE,
.pixClkEdgePol = VPS_VIP_PIX_CLK_EDGE_POL_RISING,
.invertFidPol = 0,
.embConfig = {
.errCorrEnable = 1,
.srcNumPos = VPS_VIP_SRC_NUM_POS_DONT_CARE,
.isMaxChan3Bits = 0,
},
.disConfig = {
.fidSkewPostCnt = 0,
.fidSkewPreCnt = 0,
.lineCaptureStyle =
VPS_VIP_LINE_CAPTURE_STYLE_DONT_CARE,
.fidDetectMode =
VPS_VIP_FID_DETECT_MODE_DONT_CARE,
.actvidPol = VPS_VIP_POLARITY_DONT_CARE,
.vsyncPol = VPS_VIP_POLARITY_DONT_CARE,
.hsyncPol = VPS_VIP_POLARITY_DONT_CARE,
}
},
.video_capture_mode =
VPS_CAPT_VIDEO_CAPTURE_MODE_SINGLE_CH_NON_MUX_EMBEDDED_SYNC,
.video_if_mode = VPS_CAPT_VIDEO_IF_MODE_16BIT,
.input_data_format = FVID2_DF_YUV422P,
},
};
static const struct v4l2_dv_preset hdvpss_inst0_inp0_presets[] = {
{
.preset = V4L2_DV_720P60,
},
{
.preset = V4L2_DV_1080I60,
},
{
.preset = V4L2_DV_1080P60,
},
{
.preset = V4L2_DV_1080P30,
},
};
static const struct v4l2_dv_preset hdvpss_inst2_inp0_presets[] = {
{
.preset = V4L2_DV_720P60,
},
{
.preset = V4L2_DV_1080I60,
},
{
.preset = V4L2_DV_1080P60,
},
{
.preset = V4L2_DV_1080P30,
},
};
static const struct ti81xxvin_input hdvpss_inst0_inputs[] = {
{
.input = {
.index = 0,
.name = "Component",
.type = V4L2_INPUT_TYPE_CAMERA,
.std = V4L2_STD_UNKNOWN,
.capabilities = V4L2_OUT_CAP_PRESETS,
},
.subdev_name = TVP7002_INST0,
.dv_presets = hdvpss_inst0_inp0_presets,
.num_dv_presets = ARRAY_SIZE(hdvpss_inst0_inp0_presets),
},
};
static const struct ti81xxvin_input hdvpss_inst1_inputs[] = {
{
.input = {
.index = 0,
.name = "Component",
.type = V4L2_INPUT_TYPE_CAMERA,
.std = V4L2_STD_UNKNOWN,
.capabilities = V4L2_OUT_CAP_PRESETS,
},
.subdev_name = TVP7002_INST1,
.dv_presets = hdvpss_inst2_inp0_presets,
.num_dv_presets = ARRAY_SIZE(hdvpss_inst2_inp0_presets),
},
};
/* 16 bit decoders are present on the Port A of VIP0 and VIP1 instances. Which
represents the VIP0 and VIP2 instances in software. While Port B of VIP0 and
VIP1 are represented by VIP1 and VIP3 instances. On these two instances no
decoders are present.
*/
static struct ti81xxvin_config ti81xx_hsvpss_capture_cfg = {
.subdev_info = hdvpss_capture_sdev_info,
.subdev_count = ARRAY_SIZE(hdvpss_capture_sdev_info),
.card_name = ti81xx_card_name,
.inst_config[0] = {
.inputs = hdvpss_inst0_inputs,
.input_count = ARRAY_SIZE(hdvpss_inst0_inputs),
},
.inst_config[1] = {
.inputs = hdvpss_inst0_inputs,
.input_count = 0,
},
.inst_config[2] = {
.inputs = hdvpss_inst1_inputs,
.input_count = ARRAY_SIZE(hdvpss_inst1_inputs),
},
.inst_config[3] = {
.inputs = hdvpss_inst1_inputs,
.input_count = 0,
},
};
static struct resource ti81xx_hdvpss_capture_resource[] = {
[0] = {
.start = HDVPSS_CAPTURE_INST0_BASE,
.end = (HDVPSS_CAPTURE_INST0_BASE +
HDVPSS_CAPTURE_INST0_SIZE - 1),
.flags = IORESOURCE_MEM,
},
[1] = {
.start = HDVPSS_CAPTURE_INST2_BASE,
.end = (HDVPSS_CAPTURE_INST2_BASE +
HDVPSS_CAPTURE_INST2_SIZE - 1),
.flags = IORESOURCE_MEM,
},
};
static struct platform_device hdvpss_capture_dev = {
.name = "ti81xxvin",
.id = -1,
.dev = {
.dma_mask = &ti81xx_dma_mask,
.coherent_dma_mask = ~(u32)0,
},
.num_resources = 2,
.resource = ti81xx_hdvpss_capture_resource,
};
static int __init ti81xx_vin_init(void)
{
int r;
hdvpss_capture_dev.dev.platform_data = &ti81xx_hsvpss_capture_cfg;
if (cpu_is_ti814x()) {
hdvpss_capture_sdev_info[0].ti81xxvin_select_decoder =
vps_ti814x_select_video_decoder;
hdvpss_capture_sdev_info[0].ti81xxvin_set_mode =
vps_ti814x_set_tvp7002_filter;
hdvpss_capture_sdev_info[0].decoder_id = 0;
hdvpss_capture_sdev_info[1].ti81xxvin_select_decoder =
NULL;
hdvpss_capture_sdev_info[1].ti81xxvin_set_mode =
NULL;
hdvpss_capture_sdev_info[1].decoder_id = 0;
} else {
hdvpss_capture_sdev_info[0].ti81xxvin_select_decoder =
vps_ti816x_select_video_decoder;
hdvpss_capture_sdev_info[0].ti81xxvin_set_mode =
vps_ti816x_set_tvp7002_filter;
hdvpss_capture_sdev_info[0].decoder_id = 0;
hdvpss_capture_sdev_info[1].ti81xxvin_select_decoder =
NULL;
hdvpss_capture_sdev_info[1].ti81xxvin_set_mode =
NULL;
hdvpss_capture_sdev_info[1].decoder_id = 0;
}
r = platform_device_register(&hdvpss_capture_dev);
if (r)
printk(KERN_ERR "unable to register ti81xx_vin device\n");
else
printk(KERN_INFO "registered ti81xx_vin device\n");
return r;
}
#else
static int __init ti81xx_vin_init(void)
{
return 0;
}
#endif
#if defined(CONFIG_FB_TI81XX_MODULE) || defined(CONFIG_FB_TI81XX)
static struct ti81xxfb_platform_data ti81xxfb_config;
static struct platform_device ti81xx_fb_device = {
.name = "ti81xxfb",
.id = -1,
.dev = {
.dma_mask = &ti81xx_dma_mask,
.coherent_dma_mask = ~(u32)0,
.platform_data = &ti81xxfb_config,
},
.num_resources = 0,
};
void ti81xxfb_set_platform_data(struct ti81xxfb_platform_data *data)
{
ti81xxfb_config = *data;
}
static int __init ti81xx_fb_init(void)
{
int r;
r = platform_device_register(&ti81xx_fb_device);
if (r)
printk(KERN_ERR "unable to register ti81xx_fb device\n");
else
printk(KERN_INFO "registered ti81xx_fb device\n");
return r;
}
#else
static int __init ti81xx_fb_init(void)
{
return 0;
}
void ti81xxfb_set_platform_data(struct ti81xxfb_platform_data *data)
{
}
#endif
#if defined(CONFIG_VIDEO_TI81XX_VIDOUT_MODULE) || \
defined(CONFIG_VIDEO_TI81XX_VIDOUT)
static struct resource ti81xx_vidout_resource[VPS_DISPLAY_INST_MAX] = {
};
static struct platform_device ti81xx_vidout_device = {
.name = "t81xx_vidout",
.num_resources = ARRAY_SIZE(ti81xx_vidout_resource),
.resource = &ti81xx_vidout_resource[0],
.id = -1,
};
static int __init ti81xx_init_vout(void)
{
int r;
r = platform_device_register(&ti81xx_vidout_device);
if (r)
printk(KERN_ERR "Unable to register ti81xx_vidout device\n");
else
printk(KERN_INFO "registered ti81xx_vidout device\n");
return r;
}
#else
static int __init ti81xx_init_vout(void)
{
return 0;
}
#endif
static int __init ti81xx_init_vpss(void)
{
int retval = 0;
/*if vpss failed to register, none of the below could works*/
if (ti81xx_vpss_init())
return -1;
retval = ti81xx_init_vout();
retval += ti81xx_hdmi_init();
retval += ti81xx_fb_init();
retval += ti81xx_vin_init();
return retval;
}
arch_initcall(ti81xx_init_vpss);
#endif
By the way one more question. In file ti81xxvin_main.c there is a structure named cparams that partially duplicates the fields from hdvpss_info struct what is the point of that?