Hi,
it is said that the QM uses 4*512KB memory if a total of 512K descriptors are supported. And Up to 4*16KB of this memory can be in the internal linking RAM for keystone I in QMSS LLD SDS. My questions are
1. is 4B here the entry size for every descritpors?
2. for KeystoneII, is it true that up to 4*32KB memory can be in internal linking RAM?
3. In chapter 11.2 of this document, it said that each entry must be 64bit wide. it is comflict with my understanding on 1. is this requirement only for external linking RAM? is it still 4B for internal linking RAM?
Thank you.