This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Intermittent 3874 PCIe Controller Failures

After one or two days of operation, the PCIe Controller seems to fail with the following symptoms:

  • From the PC side, all memory, including configuration space, reads all ones.
  • From the Sitara side, attempts to read PCIe registers result in address faults.  However, we can still read PRCM registers.

Description of our use:

  • We use an I7 based PC to send video frames to a 3874 Sitara over PCIE.
  • Thirty frames are sent per second. Each frame is approximately 700 KB.
  • Frame transfers take around 2 ms. at 5.0 Gts and 4 ms. at 2.5 Gts.
  • The Sitara uses DMA to read the frames from PC memory to RAM.
  • The PC reads/write Sitara memory to control the transfers. This is around 1000 transactions per second.
  • Our 3874's are rev 2.1 (3874BCYE80)
Questions:
  1. Have others seen the PCIe Controller Failures?
  2. If so, is there a work around?
  3. Is the problem in the 3.0 revision of the chip?
  4. Does the 8148 have the same problem?
  5. Is it possible to recover from the problem by resetting the PCIe subsystem?
  6. Would a PCIe analyzer help? Which one do you recommend?
  7. Will it help to reduce the transfer rate from 5.0 Gts to 2.5 Gts?
  8. Will it help to disable Active State Power Management?
  9. The errata (3.0.6) says that mis-aligned burst transfers cause corruption.  Is it possible that we're making burst transfers with I7 CPU instructions?
Help will be greatly appreciated.
Thanks,
Michael