Other Parts Discussed in Thread: TPS65910, PMP
My goal is to use gstreamer and V4L2 to capture input HDMI video and display this on the LCD screen of the EVM8148.
I have been trying to follow the steps from the VPSS Video Driver user guide and turns out that I needed to download the latest platform support package. Here is what I have now:
- EZSDK 5.05
- PSP package 04.04.00.02
- HDVPSS 1_00_01_44
The pre-built uImage inside of PSP release package supports the pre-built V4L2 capture module, so I have decided to just use this and not rebuild.
I copied to the SD card uImage, MLO and u-boot.bin
The boot.cmd file on the SD card contains the following:
setenv bootargs 'console=ttyO0,115200n8 rootwait root=/dev/nfs nfsroot=192.168.1.73:/home/mike/targetfs rw mem=256M earlyprintk notifyk.vpssm3_sva=0xBF900000 vram=50M ti814xfb.vram=0:16M,1:16M,2:6M ip=dhcp'
When I power cycle the EVM 8148 I let uboot count down without interrupting and I don't do anything else. I assume that the bootargs are being passed from the file.
My target file system doens't seem to be loading via NFS. What am I doing wrong here?
<snip>
regulator: VIO: 1500 mV
regulator: VDD1: 600 <--> 1500 mV at 1200 mV
regulator: VDD2: 600 <--> 1500 mV at 1200 mV
regulator: VDDCTRL: 600 <--> 1400 mV at 1200 mV
regulator: LDO1: 1100 <--> 3300 mV at 1800 mV
regulator: LDO2: 1100 <--> 3300 mV at 1800 mV
regulator: LDO3: 1100 <--> 3300 mV at 3300 mV
regulator: LDO4: 1100 <--> 3300 mV at 1800 mV
regulator: LDO5: 1100 <--> 3300 mV at 3300 mV
regulator: LDO6: 1100 <--> 3300 mV at 3300 mV
regulator: LDO7: 1100 <--> 3300 mV at 3300 mV
regulator: LDO8: 1100 <--> 3300 mV at 1800 mV
tps65910 1-002d: No interrupt support, no core IRQ
omap_i2c omap_i2c.3: bus 3 rev4.0 at 100 kHz
Advanced Linux Sound Architecture Driver Version 1.0.23.
Switching to clocksource gp timer
musb-hdrc: version 6.0, host, debug=0
musb-hdrc musb-hdrc.0: dma type: dma-cppi41
MUSB controller-0 revision 4ea20800
usb2phy: computed values rxcalib(15)DACs(25 12 13)
usb2phy: override computed values rxcalib(15)DACs(25 12 13)
usb2phy_config: musb(0) rxcalib done, rxcalib read value 6f6cd96e
musb-hdrc musb-hdrc.0: MUSB HDRC host driver
musb-hdrc musb-hdrc.0: new USB bus registered, assigned bus number 1
usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
usb usb1: Product: MUSB HDRC host driver
usb usb1: Manufacturer: Linux 2.6.37 musb-hcd
usb usb1: SerialNumber: musb-hdrc.0
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
musb-hdrc musb-hdrc.0: USB Host mode controller at d081e000 using DMA, IRQ 18
musb-hdrc musb-hdrc.1: dma type: dma-cppi41
MUSB controller-1 revision 4ea20800
usb2phy: computed values rxcalib(15)DACs(35 15 16)
usb2phy: override computed values rxcalib(15)DACs(35 15 16)
usb2phy_config: musb(1) rxcalib done, rxcalib read value 6f71df86
musb-hdrc musb-hdrc.1: MUSB HDRC host driver
musb-hdrc musb-hdrc.1: new USB bus registered, assigned bus number 2
usb usb2: New USB device found, idVendor=1d6b, idProduct=0002
usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1
usb usb2: Product: MUSB HDRC host driver
usb usb2: Manufacturer: Linux 2.6.37 musb-hcd
usb usb2: SerialNumber: musb-hdrc.1
hub 2-0:1.0: USB hub found
hub 2-0:1.0: 1 port detected
musb-hdrc musb-hdrc.1: USB Host mode controller at d0826800 using DMA, IRQ 19
NET: Registered protocol family 2
IP route cache hash table entries: 2048 (order: 1, 8192 bytes)
TCP established hash table entries: 8192 (order: 4, 65536 bytes)
TCP bind hash table entries: 8192 (order: 3, 32768 bytes)
TCP: Hash tables configured (established 8192 bind 8192)
TCP reno registered
UDP hash table entries: 256 (order: 0, 4096 bytes)
UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
NET: Registered protocol family 1
RPC: Registered udp transport module.
RPC: Registered tcp transport module.
RPC: Registered tcp NFSv4.1 backchannel transport module.
NetWinder Floating Point Emulator V0.97 (double precision)
PMU: registered new PMU device of type 0
omap-iommu omap-iommu.0: ducati registered
omap-iommu omap-iommu.1: sys registered
JFFS2 version 2.2. (NAND) © 2001-2006 Red Hat, Inc.
msgmni has been set to 394
io scheduler noop registered
io scheduler deadline registered
io scheduler cfq registered (default)
Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled
omap_uart.0: ttyO0 at MMIO 0x48020000 (irq = 72) is a OMAP UART0
console [ttyO0] enabled, bootconsole disabled
console [ttyO0] enabled, bootconsole disabled
omap_uart.1: ttyO1 at MMIO 0x48022000 (irq = 73) is a OMAP UART1
omap_uart.2: ttyO2 at MMIO 0x48024000 (irq = 74) is a OMAP UART2
omap_uart.3: ttyO3 at MMIO 0x481a6000 (irq = 44) is a OMAP UART3
omap_uart.4: ttyO4 at MMIO 0x481a8000 (irq = 45) is a OMAP UART4
omap_uart.5: ttyO5 at MMIO 0x481aa000 (irq = 46) is a OMAP UART5
brd: module loaded
loop: module loaded
ahci ahci.0: forcing PORTS_IMPL to 0x1
ahci ahci.0: AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl platform mode
ahci ahci.0: flags: ncq sntf pm led clo only pmp pio slum part ccc apst
scsi0 : ahci_platform
ata1: SATA max UDMA/133 mmio [mem 0x4a140000-0x4a150fff] port 0x100 irq 16
omap2-nand driver initializing
ONFI flash detected
ONFI param page 0 valid
NAND device: Manufacturer ID: 0x2c, Chip ID: 0xca (Micron NAND 256MiB 3,3V 16-bit)
Creating 6 MTD partitions on "omap2-nand.0":
0x000000000000-0x000000020000 : "U-Boot-min"
0x000000020000-0x000000260000 : "U-Boot"
0x000000260000-0x000000280000 : "U-Boot Env"
0x000000280000-0x0000006c0000 : "Kernel"
0x0000006c0000-0x00000cee0000 : "File System"
0x00000cee0000-0x000010000000 : "Reserved"
davinci_mdio davinci_mdio.0: davinci mdio revision 1.6
davinci_mdio davinci_mdio.0: detected phy mask fffffffc
davinci_mdio.0: probed
davinci_mdio davinci_mdio.0: phy[0]: device 0:00, driver unknown
davinci_mdio davinci_mdio.0: phy[1]: device 0:01, driver unknown
CAN device driver interface
CAN bus driver for Bosch D_CAN controller 1.0
d_can d_can: d_can device registered (irq=52, irq_obj=53)
usbcore: registered new interface driver cdc_ether
usbcore: registered new interface driver dm9601
usbcore: registered new interface driver cdc_acm
cdc_acm: v0.26:USB Abstract Control Model driver for USB modems and ISDN adapters
Initializing USB Mass Storage driver...
usbcore: registered new interface driver usb-storage
USB Mass Storage support registered.
mice: PS/2 mouse device common for all mice
ata1: SATA link down (SStatus 0 SControl 300)
usb 1-1: new low speed USB device using musb-hdrc and address 2
qt602240_ts 1-004a: Family ID: 128 Variant ID: 1 Version: 22 Build: 171
qt602240_ts 1-004a: Matrix X Size: 18 Matrix Y Size: 12 Object Num: 17
input: AT42QT602240/ATMXT224 Touchscreen as /devices/platform/omap/omap_i2c.1/i2c-1/1-004a/input/input0
omap_rtc omap_rtc: rtc core: registered omap_rtc as rtc0
i2c /dev entries driver
Linux video capture interface: v2.00
usbcore: registered new interface driver uvcvideo
USB Video Class driver (v1.0.0)
OMAP Watchdog Timer Rev 0x00: initial timeout 60 sec
usbcore: registered new interface driver usbhid
usbhid: USB HID core driver
notify_init : notify drivercreated for remote proc id 2 at physical Address 0xbf900000
usbcore: registered new interface driver snd-usb-audio
asoc: tlv320aic3x-hifi <-> davinci-mcasp.2 mapping ok
ALSA device list:
#0: TI81XX EVM
TCP cubic registered
NET: Registered protocol family 17
can: controller area network core (rev 20090105 abi 8)
NET: Registered protocol family 29
can: raw protocol (rev 20090105)
can: broadcast manager protocol (rev 20090105 t)
Registering the dns_resolver key type
VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3
omap_voltage_late_init: Voltage driver support not added
Power Management for TI81XX.
Detected MACID=40:5f:c2:67:22:a5
omap_rtc omap_rtc: setting system clock to 2000-01-01 00:00:00 UTC (946684800)
Waiting for root device /dev/mmcblk0p2...
usb 1-1: New USB device found, idVendor=04f3, idProduct=0234
usb 1-1: New USB device strings: Mfr=0, Product=2, SerialNumber=0
usb 1-1: Product: OM
input: OM as /devices/platform/omap/ti81xx-usbss/musb-hdrc.0/usb1/1-1/1-1:1.0/input/input1
generic-usb 0003:04F3:0234.0001: input: USB HID v1.11 Mouse [OM] on usb-musb-hdrc.0-1/input0
mmc0: host does not support reading read-only switch. assuming write-enable.
mmc0: new high speed SDHC card at address e624
mmcblk0: mmc0:e624 SD08G 7.40 GiB
mmcblk0: p1 p2 p3
EXT3-fs: barriers not enabled
kjournald starting. Commit interval 5 seconds
EXT3-fs (mmcblk0p2): warning: maximal mount count reached, running e2fsck is recommended
EXT3-fs (mmcblk0p2): using internal journal
EXT3-fs (mmcblk0p2): recovery complete
EXT3-fs (mmcblk0p2): mounted filesystem with writeback data mode
VFS: Mounted root (ext3 filesystem) on device 179:2.
devtmpfs: mounted
Freeing init memory: 228K
INIT: version 2.86 booting
Please wait: booting...
Error opening /dev/fb0: No such file or directory
Starting udev
udevd (82): /proc/82/oom_adj is deprecated, please use /proc/82/oom_score_adj instead.
EXT3-fs: barriers not enabled
kjournald starting. Commit interval 5 seconds
EXT3-fs (mmcblk0p3): warning: maximal mount count reached, running e2fsck is recommended
EXT3-fs (mmcblk0p3): using internal journal
EXT3-fs (mmcblk0p3): recovery complete
EXT3-fs (mmcblk0p3): mounted filesystem with writeback data mode
Remounting root file system...
Caching udev devnodes
ipv6: disagrees about version of symbol module_layout
ALSA: Restoring mixer settings...
Configuring network interfaces... ifconfig: SIOCGIFFLAGS: No such device
CPSW phy found : id is : 0x4dd074
CPSW phy found : id is : 0x4dd074
done.
Setting up IP spoofing protection: rp_filter.
Fri Nov 11 01:36:00 UTC 2011
INIT: Entering runlevel: 5
Loading HDVICP2 Firmware
DM814X prcm_config_app version: 2.0.0.1
Doing PRCM settings...
PRCM for IVHD0 is in Progress, Please wait.....
BW Phy Addr : 0x48180600 Data : 0x00000001
AW Phy Addr : 0x48180600 Data : 0x00000002
Phy Addr : 0x48180c04 Data : 0x00000037
BW Phy Addr : 0x48180620 Data : 0x00070000
AW Phy Addr : 0x48180620 Data : 0x00070002
BW Phy Addr : 0x48180624 Data : 0x00030000
AW Phy Addr : 0x48180624 Data : 0x00010002
Phy Addr : 0x48180600 Data : 0x00000102
BW Phy Addr : 0x48180c10 Data : 0x00000007
AW Phy Addr : 0x48180c10 Data : 0x00000003
Phy Addr : 0x48180c14 Data : 0x00000004
BW Phy Addr : 0x58088000 Data : 0xc77611cb
AW Phy Addr : 0x58088000 Data : 0xeafffffe
BW Phy Addr : 0x58098000 Data : 0xf3468d81
AW Phy Addr : 0x58098000 Data : 0xeafffffe
BW Phy Addr : 0x48180c10 Data : 0x00000003
AW Phy Addr : 0x48180c10 Data : 0x00000000
Phy Addr : 0x48180c14 Data : 0x00000007
PRCM for IVHD0 is Done Successfully
PRCM Initialization completed
syslink: disagrees about version of symbol module_layout
FATAL: Error inserting syslink (/lib/modules/2.6.37/kernel/drivers/dsp/syslink.ko): Invalid module format
PHY: 0:01 - Link is Up - 0/Half
PHY: 0:01 - Link is Down
PHY: 0:00 - Link is Up - 100/Full
(hangs here)
Thank you for any information.
-Mike