This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Run error in Qt 2.4.1 in Linux Ubuntu 10.04.....

Dear Mr. Dave,

I installed Qt 2.4.1 in Ubuntu 10.04 as per describe in Sitara Linux Training Hands on with QT and Run from the compile on terminal.

I created New Project,,,,, Qt Widget Project/Qt Gui Application ….. in following path.

/home/rd/test/

I put one “lable” in widget.ui page and I successfully build this project.

But when I run this project the following error generate:

starting /home/rd/test/test….
Failed to start program. Path or Permission wrong?
/home/rd/test/test exited with code -1

Please help.

Regards,
Dharmendra

  • Hello,

    It seems you are building the application for the target Sitara platform, so you will not be able to run it on your host PC. You can copy it to your device and then run it.

    Regards,

    Dave

  • Hi,

    Thanks for support, I was done. I was done as per following.

    I was changed in program of button shifting in /ti-sdk-am335x-evm-05.07.00.00/targetNFS/usr/bin/qtopia/examples/animation/animatedtiles/main.c file and successfully build it and run in our device and effect of this change in shown TFT(button shifted) and its done.

    Now I want to put my company home page (comapny home.jpg) instead of Texas matrix application launcher home page (texas home.jpg), so please let us know about it and suggest for go in write direction,,,

    How can I change??

    Its files path??

    What and Where to change??

    Is there any tools for this changes???

    For your information my TFT is 5.7 inch (320 x 240 pixel resolution).

    Please help for further progress...

    Thanks and Regards,

    Dharmendra

    Dharmendra

  • Dear All,

    Anybody please reply.

    Regards,

    Dharmendra