With God’s help
When we are streaming video from our DM6446 encoder in mpeg4 format to VLC it is work good but to our DM6446 decoder we receive from the VIDDEC2_process function:
Frame status = 0
Extended error codes = 0x408 / 0x 801 / 0x 81d
The 2 codec’s are of TI.
The encoder parameters:
Image Size = 352x240
Frame Rate = 30
GOP Size = 30
Rate Control Mode = CBR
Constant Bitrate = 4000000
Q Initial = 8
The decoder parameters:
Image Size = 352x240
Frame Rate = 30
GOP Size = 30
Rate Control Mode = CBR
Bitrate = 4000000
Q Min = 4
Q Max = 51
Q Initial = 8
What cause to the problem?
What the code errors mean?
All the Best
Aba Abuchatzira